4.11. CDD UART Module
4.11.1. Acronyms and Definitions
Abbreviation/Term |
Explanation |
|---|---|
AUTOSAR |
Automotive Open System Architecture |
BSW |
Basic Software |
DET |
Default Error Tracer |
CDD |
Complex Device Driver |
DMA |
Direct Memory Access |
ISR |
Interrupt Service Routine |
INT |
Interrupt |
HW |
Hardware |
SW |
Software |
MCU |
Micro Controller Unit |
OS |
Operating System |
API |
Application Programming Interface |
UART |
Universal Asynchronous Receiver Transmitter |
4.11.2. Introduction
This document describes the functionality and configuration of the Cdd_Uart module.
Supported AUTOSAR Release |
4.3.1 |
|---|---|
Supported Configuration Variants |
Pre-Compile, Post-Build |
Vendor ID |
UART_VENDOR_ID (44) |
Module ID |
UART_MODULE_ID (255) |
Supported Platform |
AM261x |
The UART complex device driver provides data read and write transfer using the module unit channels in the device board.
4.11.3. Functional Overview
The driver is configurable for parameters such as baud rate, word length, parity, stop bits, IO mode, clock frequency, transmission and reception buffer threshold, and operating mode. Depending upon the IO Mode selected, the driver allows for both synchronous as well as asynchronous mode of data transfer.
The UART Driver provides services for reading and writing to/from
UART Channels
UART Ports / Serial Device
4.11.3.1. Driver Architecture
The UART driver has architecture as shown in below figure from the AM261 Technical Reference Manual
Fig. 4.51 UART interface
UART comes under the Complex Driver Design section under the AUTOSAR Classic Platform Architecture
Fig. 4.52 AUTOSAR CDDs
4.11.3.2. Initialization
Cdd_Uart_Init() is the function responsible for initializing driver peripheral and opening its configured instances for transmission
4.11.3.3. States
UART driver maintains these below states as per the driver source condition:
CDD_UART_UNINIT
CDD_UART_INIT
4.11.3.4. Assumptions
For using DMA feature, driver assumes that cache initialization is done in application only and not done by the driver.
4.11.3.5. Limitations
None
4.11.3.6. Main Functions
Cdd_Uart_Read() - This API is used for reading data using a given channel ID upto a specified length
Cdd_Uart_Write() - This API is used for writing data using a given channel ID upto a specified data count
Cdd_Uart_Cancel() - This API is used for cancelling an ongoing data transfer using a given channel ID in the given direction
Cdd_Uart_GetRemainingWords() - This API is used for checking the remaining words count for an ongoing Interrupt or DMA mode data transfer
Note: Timeout Value parameter in Cdd_Uart_Read() and Cdd_Uart_Write() should be passed as number of ticks according to clock frequency. The clock source have changed from RTI timers which used 200MHz clock frequency to R5f timers which uses 400MHz clock frequency, so the timeout values need to be passed accordingly.
4.11.3.7. Design overview
Will be updated in future release
4.11.4. Hardware Features
4.11.4.1. IP Supported Features
Interrupt, Polling And DMA Mode. For DMA mode, only trigger level 1 is supported
Write, Read and Cancel Operation.
Read Return Full & Partial Mode.
Receiver line error status like overrun, framing.
4.11.4.2. Not supported Features
MODEM control functions.
Hardware Flow Control.
Partial Mode is only supported in interrupt mode and returns FIFO level chars.
IrDA and CIR Features.
4.11.4.3. Non compliance
4.11.4.3.1. Deviations to requirements (Requirement Traceability)
4.11.4.3.1.1. Deviation of requirements against AUTOSAR specification requirements
None
4.11.5. Source files
The files structure for the UART driver is similar to other drivers. The source is divided into headers under include/ and driver source within src/ directory under Uart driver path in MCAL. Cdd_Uart.c and Cdd_Uart.h are the 2 files that contain the provided driver API’s.
Static source C Files are defined below
📦AM261x
┣ 📂build
┣ 📂mcal
┃ ┣ 📂Uart
┃ ┃ ┣ 📂include
┃ ┃ ┃ ┣ 📜Cdd_Uart.h : Shall specify the interface provided by the driver.
┃ ┃ ┃ ┣ 📜Cdd_Uart_Irq.h : contain interrupt service routines.
┃ ┃ ┣ 📂src
┃ ┃ ┃ ┣ 📜Cdd_Uart.c : Shall implement the CDD Uart driver functionality.
┃ ┃ ┃ ┣ 📜Cdd_Uart_Irq.c : contain interrupt service routines.
┃ ┃ ┣ 📂V0
┃ ┃ ┃ ┗ 📜Cdd_Uart_Priv.c : Shall implement the private functions.
┃ ┃ ┃ ┣ 📜Cdd_Uart_Priv.h : Contains device specific function declarations.
┃ ┃ ┃ ┣ 📜uart.c : Contains the UART driver implementations.
┃ ┃ ┃ ┣ 📜Uart.h : Contains Internal functions declarations for Uart driver.
┃ ┃ ┃ ┗ 📜uart_dma.h : Contains DMA related function declarations.
┃ ┃ ┃ ┣ 📜uart_dma_edma.c : Contains functions that support the Enhanced DMA mode
for use with UART channels in DMA mode as IO mode.
┃ ┃ ┗ 📜Makefile
┃ 📂mcal_config
┃ 📂mcal_docs
┃ 📜README.txt
Plugin files are defined below in the table.
Plugin Files |
Description |
|---|---|
Cdd_Uart_Cfg.h |
Contains the Precompile switches and Symbolic names |
Cdd_Uart_Cfg.c |
Contains all Pre-Compile Configured parameters |
Cdd_Uart_PBcfg.c |
Contains all Post-Build Configured parameters |
4.11.6. Module requirements
Will be updated in future release
4.11.6.1. Memory Mapping
Memory Mapping Sections |
CDD_UART_CODE |
CDD_UART_CODE_ISR |
CDD_UART_VAR_NO_INIT |
CDD_UART_VAR_ZERO_INIT |
CDD_UART_PBCFG |
CDD_UART_PBCFG_ROOT |
|---|---|---|---|---|---|---|
CDD_UART_START_SEC_VAR_INIT_UNSPECIFIED(.bss) |
x |
|||||
CDD_UART_STOP_SEC_VAR_INIT_UNSPECIFIED |
x |
|||||
CDD_UART_START_SEC_CODE_APPL(.text) |
x |
|||||
CDD_UART_STOP_SEC_CODE_APPL |
x |
|||||
CDD_UART_START_SEC_VAR_UNSPECIFIED(.data) |
x |
|||||
CDD_UART_STOP_SEC_VAR_UNSPECIFIED |
x |
|||||
CDD_UART_START_SEC_CODE(.text) |
x |
|||||
CDD_UART_STOP_SEC_CODE |
x |
|||||
CDD_UART_START_SEC_PBCFG(.data) |
x |
|||||
CDD_UART_STOP_SEC_PBCFG |
x |
|||||
CDD_UART_START_SEC_PBCFG_ROOT(.const) |
x |
|||||
CDD_UART_STOP_SEC_PBCFG_ROOT |
x |
4.11.6.2. Scheduling
There are no scheduled functions within the CDD UART driver
4.11.6.3. Error handling
4.11.6.3.1. Development Error Reporting (DET)
The Cdd_UartDriver will report development errors on enabling UART_DEV_ERROR_DETECT == STD_ON in Cdd_Uart_Cfg.h
Refer API documentation for list of development errors reported by UART Driver
4.11.6.3.2. Parameter checking
AUTOSAR requires that API functions check the validity of their parameters. The checks are described in spec and are done as internal parameter checks of the API functions. These checks are for development error reporting and can be en-/disabled separately. Refer to the configuration chapter where the en-/disabling of the checks is described. En-/disabling of single checks is an addition to the AUTOSAR standard which requires to en-/disable the complete parameter checking via the parameter UART_DEV_ERROR_DETECT.
4.11.6.3.3. Production Code Error Reporting
By default, production code related errors are reported to the DEM using the service DEM_ReportErrorStatus().
4.11.7. Used resources
4.11.7.1. Interrupt Handling
Following Interrupt Service Routines are present in UART:
Cdd_Uart_ChannelIsr - The Channel-based Interrupt Subroutine calls handler function based on the selected channel.
CDD_EDMA_lld_transferCompletionMasterIsrFxn - The common-channel DMA-based Interrupt Subroutine calls handler function available for transfer completion.
4.11.8. Integration description
4.11.8.1. Dependent modules
4.11.8.1.1. DET
The module UART depends on the DET (by default) in order to report development errors. Detection and reporting of development errors, DET shall be enabled or disabled by the switch CDD_UART_DEV_ERROR_DETECT = STD_ON in Cdd_Uart_Cfg.h, generated by using appropriate option check within the configurator plugin. The DET can be replaced optionally by an equivalent component which is responsible to recognize development errors, if no DET component is available.
4.11.8.1.2. MCU
The Cdd_Uart Modules expects the MCU modules to enable the GPIO registers used by configuring the PRCM correctly. MCU module is responsible for setting up clock configuration for the driver, the hardware clock available on the board.
4.11.8.1.3. PORT
The Cdd_Uart Modules expects that PinMux is set correctly to configure the GPIO pins for appropriate UART channel ports. The pin direction shall also be set by the PORT driver
4.11.8.1.4. Callback Functions
The UART driver provides read, write and error call back functions supported for all channels targeted from UART Configurator Plugin
4.11.8.1.5. SchM (Optional)
If multiple AUTOSAR runnables have access to the same Data Store Memory block, the exported AUTOSAR specification enforces data consistency by using an AUTOSAR exclusive area. With this specification, the runnables have mutually exclusive access to the per-instance memory global data, which prevents data corruption. Beside the OS, the BSW Scheduler provides functions that UART module calls at begin and end of critical sections. This implementation requires 1 level of exclusive access to guard critical sections.
The data consistency mechanism that has to be applied to an ExclusiveArea might be domain, ECU or even project specific. The decision which mechanism has to be applied by RTE / Basic Software Scheduler is taken during ECU integration by setting the Exclusive Area configuration parameter RteExclusiveAreaImplMechanism. This parameter is an input for RTE generator. For UART Module, data consistency and exclusive access to critical sections are required for the following sections as shown in the table below:
Exclusive Area Functions used |
UART Function calling Exclusive Area |
Need for Exclusive Area |
Recommended Exclusive Area Mapping |
|---|---|---|---|
UART_EXCLUSIVE_AREA_0 |
UART_writeCancelNoCB |
To protect against multiple access for shared resources |
ALL_INTERRUPT_BLOCKING : All interrupts should be blocked as this API’s can be called in the interrupts |
4.11.8.2. Multi-core support
Not supported
4.11.9. Configuration
4.11.9.1. CddUartDriver
This container contains the configuration parameters and sub containers of the AUTOSAR Complex device driver (CDD) module.
4.11.9.1.1. CddUartChannel
Configuration of an individual UART channel.
4.11.9.1.1.1. CddUartHwID
Item |
|
|---|---|
Name |
CddUartHwID |
Description |
This parameter contains the Channel ID of UART port in the device. |
Origin |
Texas Instruments |
Post-build-variant-multiplicity |
false |
Post-Build-Variant-Value |
false |
Value-Configuration-Class |
– |
Post-Build-Time |
VARIANT-POST-BUILD |
Pre-Compile-Time |
VARIANT-PRE-COMPILE |
Default-value |
CDD_UART_CHANNEL_ID_0 |
Range |
CDD_UART_CHANNEL_ID_0 |
4.11.9.1.1.2. CddUartClockFrequency
Item |
|
|---|---|
Name |
CddUartClockFrequency |
Description |
This parameter indicates the input clock frequency from the device. |
Origin |
Texas Instruments |
Post-build-variant-multiplicity |
false |
Post-Build-Variant-Value |
false |
Value-Configuration-Class |
– |
Post-Build-Time |
VARIANT-POST-BUILD |
Pre-Compile-Time |
VARIANT-PRE-COMPILE |
Default-value |
48000000 |
Max-value |
1000000000 |
Min-value |
32000 |
4.11.9.1.1.3. CddUartBaudRate
Item |
|
|---|---|
Name |
CddUartBaudRate |
Description |
This parameter contains the desired Baud Rate to be used for transmission of signals. |
Origin |
Texas Instruments |
Post-build-variant-multiplicity |
false |
Post-Build-Variant-Value |
false |
Value-Configuration-Class |
– |
Post-Build-Time |
VARIANT-POST-BUILD |
Pre-Compile-Time |
VARIANT-PRE-COMPILE |
Default-value |
115200 |
Max-value |
12000000 |
Min-value |
2400 |
4.11.9.1.1.4. CddUartIOMode
Item |
|
|---|---|
Name |
CddUartIOMode |
Description |
This parameter identifies the UART operational mode for the configured IP. |
Origin |
Texas Instruments |
Post-build-variant-multiplicity |
false |
Post-Build-Variant-Value |
false |
Value-Configuration-Class |
– |
Post-Build-Time |
VARIANT-POST-BUILD |
Pre-Compile-Time |
VARIANT-PRE-COMPILE |
Default-value |
CDD_UART_MODE_INTERRUPT |
Range |
CDD_UART_MODE_POLLING |
4.11.9.1.1.5. CddUartTXTriggerLevel
Item |
|
|---|---|
Name |
CddUartTXTriggerLevel |
Description |
This parameter identifies the UART transmission trigger level threshold for the configured UART. |
Origin |
Texas Instruments |
Post-build-variant-multiplicity |
false |
Post-Build-Variant-Value |
false |
Value-Configuration-Class |
– |
Post-Build-Time |
VARIANT-POST-BUILD |
Pre-Compile-Time |
VARIANT-PRE-COMPILE |
Default-value |
CDD_UART_TRIGGER_LEVEL_16 |
Range |
CDD_UART_TRIGGER_LEVEL_1 |
4.11.9.1.1.6. CddUartRXTriggerLevel
Item |
|
|---|---|
Name |
CddUartRXTriggerLevel |
Description |
This parameter identifies the UART trigger level threshold during receival for the configured UART. |
Origin |
Texas Instruments |
Post-build-variant-multiplicity |
false |
Post-Build-Variant-Value |
false |
Value-Configuration-Class |
– |
Post-Build-Time |
VARIANT-POST-BUILD |
Pre-Compile-Time |
VARIANT-PRE-COMPILE |
Default-value |
CDD_UART_TRIGGER_LEVEL_16 |
Range |
CDD_UART_TRIGGER_LEVEL_1 |
4.11.9.1.1.7. CddUartWordLength
Item |
|
|---|---|
Name |
CddUartWordLength |
Description |
This parameter identifies the word length for the packets used in data transmission with UART. |
Origin |
Texas Instruments |
Post-build-variant-multiplicity |
false |
Post-Build-Variant-Value |
false |
Value-Configuration-Class |
– |
Post-Build-Time |
VARIANT-POST-BUILD |
Pre-Compile-Time |
VARIANT-PRE-COMPILE |
Default-value |
CDD_UART_WORD_LENGTH_8 |
Range |
CDD_UART_WORD_LENGTH_5 |
4.11.9.1.1.8. CddUartParity
Item |
|
|---|---|
Name |
CddUartParity |
Description |
This parameter specifies the parity of the bits transferred. |
Origin |
Texas Instruments |
Post-build-variant-multiplicity |
false |
Post-Build-Variant-Value |
false |
Value-Configuration-Class |
– |
Post-Build-Time |
VARIANT-POST-BUILD |
Pre-Compile-Time |
VARIANT-PRE-COMPILE |
Default-value |
CDD_UART_PARITY_NONE |
Range |
CDD_UART_PARITY_NONE |
4.11.9.1.1.9. CddUartReadReturnModes
Item |
|
|---|---|
Name |
CddUartReadReturnModes |
Description |
This parameter identifies the UART read return modes. |
Origin |
Texas Instruments |
Post-build-variant-multiplicity |
false |
Post-Build-Variant-Value |
false |
Value-Configuration-Class |
– |
Post-Build-Time |
VARIANT-POST-BUILD |
Pre-Compile-Time |
VARIANT-PRE-COMPILE |
Default-value |
CDD_UART_FULL_READ_RETURN |
Range |
CDD_UART_FULL_READ_RETURN |
4.11.9.1.1.10. CddUartOperatingModes
Item |
|
|---|---|
Name |
CddUartOperatingModes |
Description |
This parameter identifies the UART operational mode for the configured channels. |
Origin |
Texas Instruments |
Post-build-variant-multiplicity |
false |
Post-Build-Variant-Value |
false |
Value-Configuration-Class |
– |
Post-Build-Time |
VARIANT-POST-BUILD |
Pre-Compile-Time |
VARIANT-PRE-COMPILE |
Default-value |
CDD_UART_16x_OPER |
Range |
CDD_UART_13x_OPER |
4.11.9.1.1.11. CddUartStopBits
Item |
|
|---|---|
Name |
CddUartStopBits |
Description |
This parameter specifies the size of stop bits to use in data packets. |
Origin |
Texas Instruments |
Post-build-variant-multiplicity |
false |
Post-Build-Variant-Value |
false |
Value-Configuration-Class |
– |
Post-Build-Time |
VARIANT-POST-BUILD |
Pre-Compile-Time |
VARIANT-PRE-COMPILE |
Default-value |
CDD_UART_STOP_BIT_1 |
Range |
CDD_UART_STOP_BIT_1 |
4.11.9.1.1.12. CddUartReadNotificationHandler
Item |
|
|---|---|
Name |
CddUartReadNotificationHandler |
Description |
This parameter is a read notification handler function. |
Origin |
Texas Instruments |
Post-build-variant-multiplicity |
false |
Post-Build-Variant-Value |
false |
Value-Configuration-Class |
– |
Post-Build-Time |
VARIANT-POST-BUILD |
Pre-Compile-Time |
VARIANT-PRE-COMPILE |
Default-value |
CddUart_CallbackReadNotify |
4.11.9.1.1.13. CddUartWriteNotificationHandler
Item |
|
|---|---|
Name |
CddUartWriteNotificationHandler |
Description |
This parameter is a write notification handler function. |
Origin |
Texas Instruments |
Post-build-variant-multiplicity |
false |
Post-Build-Variant-Value |
false |
Value-Configuration-Class |
– |
Post-Build-Time |
VARIANT-POST-BUILD |
Pre-Compile-Time |
VARIANT-PRE-COMPILE |
Default-value |
CddUart_CallbackWriteNotify |
4.11.9.1.1.14. CddUartErrorNotificationHandler
Item |
|
|---|---|
Name |
CddUartErrorNotificationHandler |
Description |
This parameter is a error notification handler function. |
Origin |
Texas Instruments |
Post-build-variant-multiplicity |
false |
Post-Build-Variant-Value |
false |
Value-Configuration-Class |
– |
Post-Build-Time |
VARIANT-POST-BUILD |
Pre-Compile-Time |
VARIANT-PRE-COMPILE |
Default-value |
CddUart_CallbackErrorNotify |
4.11.9.1.1.15. CddUartHwUnitCddDmaTxHandler
Item |
|
|---|---|
Name |
CddUartHwUnitCddDmaTxHandler |
Description |
References the CDD DMA handler used for CDD UART transmission |
Multiplicity-Configuration-Class |
– |
Post-Build Time |
VARIANT-POST-BUILD |
Pre-Compile Time |
VARIANT-PRE-COMPILE |
Origin |
Texas Instruments |
Post-build-variant-multiplicity |
false |
Post-Build-Variant-Value |
false |
Value-Configuration-Class |
– |
Post-Build-Time |
VARIANT-POST-BUILD |
Pre-Compile-Time |
VARIANT-PRE-COMPILE |
4.11.9.1.1.16. CddUartHwUnitCddDmaRxHandler
Item |
|
|---|---|
Name |
CddUartHwUnitCddDmaRxHandler |
Description |
References the CDD DMA handler used for CDD UART reception |
Multiplicity-Configuration-Class |
– |
Post-Build Time |
VARIANT-POST-BUILD |
Pre-Compile Time |
VARIANT-PRE-COMPILE |
Origin |
Texas Instruments |
Post-build-variant-multiplicity |
false |
Post-Build-Variant-Value |
false |
Value-Configuration-Class |
– |
Post-Build-Time |
VARIANT-POST-BUILD |
Pre-Compile-Time |
VARIANT-PRE-COMPILE |
4.11.9.2. CddUartGeneral
Item |
|
|---|---|
Name |
CddUartGeneral |
Description |
Switches the Cdd_Uart_GetVersionInfo function ON or OFF. |
Post-build-variant-multiplicity |
false |
Origin |
Texas Instruments |
Post-Build-Variant-Value |
false |
Value-Configuration-Class |
– |
Post-Build-Time |
VARIANT-POST-BUILD |
Pre-Compile-Time |
VARIANT-PRE-COMPILE |
Default-value |
true |
4.11.9.2.1. CddUartRegisterReadbackApi
Item |
|
|---|---|
Name |
CddUartRegisterReadbackApi |
Description |
Switches the Cdd_Uart_RegisterReadback function ON or OFF. |
Origin |
Texas Instruments |
Post-build-variant-multiplicity |
false |
Post-Build-Variant-Value |
false |
Value-Configuration-Class |
– |
Post-Build-Time |
VARIANT-POST-BUILD |
Pre-Compile-Time |
VARIANT-PRE-COMPILE |
Default-value |
true |
4.11.9.2.2. CddUartDeinitApi
Item |
|
|---|---|
Name |
CddUartDeinitApi |
Description |
Switches the Cdd_Uart_DeInit function ON or OFF. |
Origin |
Texas Instruments |
Post-build-variant-multiplicity |
false |
Post-Build-Variant-Value |
false |
Value-Configuration-Class |
– |
Post-Build-Time |
VARIANT-POST-BUILD |
Pre-Compile-Time |
VARIANT-PRE-COMPILE |
Default-value |
true |
4.11.9.2.3. CddUartWriteApi
Item |
|
|---|---|
Name |
CddUartWriteApi |
Description |
Switches the Cdd_Uart_Write function ON or OFF. |
Origin |
Texas Instruments |
Post-build-variant-multiplicity |
false |
Post-Build-Variant-Value |
false |
Value-Configuration-Class |
– |
Post-Build-Time |
VARIANT-POST-BUILD |
Pre-Compile-Time |
VARIANT-PRE-COMPILE |
Default-value |
true |
4.11.9.2.4. CddUartReadApi
Item |
|
|---|---|
Name |
CddUartReadApi |
Description |
Switches the Cdd_Uart_Read function ON or OFF. |
Origin |
Texas Instruments |
Post-build-variant-multiplicity |
false |
Post-Build-Variant-Value |
false |
Value-Configuration-Class |
– |
Post-Build-Time |
VARIANT-POST-BUILD |
Pre-Compile-Time |
VARIANT-PRE-COMPILE |
Default-value |
true |
4.11.9.2.5. CddUartCancelApi
Item |
|
|---|---|
Name |
CddUartCancelApi |
Description |
Switches the Cdd_Uart_Cancel function ON or OFF. |
Origin |
Texas Instruments |
Post-build-variant-multiplicity |
false |
Post-Build-Variant-Value |
false |
Value-Configuration-Class |
– |
Post-Build-Time |
VARIANT-POST-BUILD |
Pre-Compile-Time |
VARIANT-PRE-COMPILE |
Default-value |
true |
4.11.9.2.6. CddUartGetRemainingWordsApi
Item |
|
|---|---|
Name |
CddUartGetRemainingWordsApi |
Description |
Switches the Cdd_Uart_GetRemainingWords API which returns the remaining words to be transferred from the active device UART instance. |
Origin |
Texas Instruments |
Post-build-variant-multiplicity |
false |
Post-Build-Variant-Value |
false |
Value-Configuration-Class |
– |
Post-Build-Time |
VARIANT-POST-BUILD |
Pre-Compile-Time |
VARIANT-PRE-COMPILE |
Default-value |
true |
4.11.9.2.7. CddUartDevErrorDetect
Item |
|
|---|---|
Name |
CddUartDevErrorDetect |
Description |
Switches the Development Error Detection and Notification ON or OFF. |
Origin |
Texas Instruments |
Post-build-variant-multiplicity |
false |
Post-Build-Variant-Value |
false |
Value-Configuration-Class |
– |
Post-Build-Time |
VARIANT-POST-BUILD |
Pre-Compile-Time |
VARIANT-PRE-COMPILE |
Default-value |
true |
4.11.9.2.8. CddUartIrqType
Item |
|
|---|---|
Name |
CddUartIrqType |
Description |
This parameter contains a reference to the OsCounter, which is used by the UART driver. |
Origin |
Texas Instruments |
Post-build-variant-multiplicity |
false |
Post-Build-Variant-Value |
false |
Value-Configuration-Class |
– |
Post-Build-Time |
VARIANT-POST-BUILD |
Pre-Compile-Time |
VARIANT-PRE-COMPILE |
Default-value |
0 |
Range |
CDD_UART_ISR_VOID |
Multiplicity-Configuration-Class |
– |
Post-Build Time |
VARIANT-POST-BUILD |
Pre-Compile Time |
VARIANT-PRE-COMPILE |
Max-value |
16 |
Min-value |
0 |
For using UART with DMA mode, take additional care with these configuration value with CDD DMA configuration:
separate DMA configuration shall be done for Tx and/or Rx of each UART instance configured for DMA IO mode using the CDD DMA configurator plugin. Make sure to set CddDmaInterruptEnable option provided there as UART peripheral shall make use of enhanced DMA with interrupt enabled.
UART Tx makes use of two parameters for Tx and Dummy param sets to service a dummy transfer request at the end as expected from HW IP. So make sure to have corresponding two parameter sets registered in a channel group on configurator plugin.
4.11.10. Examples
4.11.10.1. Overview
Initialize MCU and Port using Mcu_Init() and Port_Init()
Configure the interrupt using Cdd_Uart_InterruptConfiguration()
Initialize the UART peripheral using API Cdd_Uart_Init()
Select the channel and buffer pointers for read and write
Write the sample message to the terminal
Write the message from Write buffer to the terminal to input the characters using Cdd_Uart_Write()
Read the input message using Cdd_Uart_Read() and store it in the Read buffer
Again write the message back which is read to echo the read message to the terminal
Write the message to inform the echo has been completed using interrupt mode
4.11.10.2. Hardware Software Setup and Tools
None
4.11.10.3. Steps to build and run example
CDD UART Interrupt example application demonstrating the CDD UART driver features is present in Uart/uart_interrupt_app under /examples folder.
The UART example app used to verify the data transmission and reception through a selected channel ID 0 of the available UART Hardware Units.
This application can be built from the build folder by running gmake –s uart_interrupt_app PLATFORM=am261x.
The details of running the application and the setup required is part of the MCAL User Guide.
4.11.10.4. Example Logs
Please input 8 characters:
qwertyui
Echo has been completed.
All tests have passed!
4.11.10.5. File Structure
📦AM261x
┣ 📂build
┣ 📂mcal
┃ ┣ 📂examples
┃ ┃ ┣ 📂Uart
┃ ┃ ┃ ┣ 📂uart_interrupt_app
┃ ┃ ┃ ┃ ┣ 📂soc
┃ ┃ ┃ ┃ ┣ 📜Makefile
┃ ┃ ┃ ┃ ┣ 📜UartInterruptApp.c : Contains UART interrupt app test example.
┃ ┃ ┃ ┃ ┣ 📜UartInterruptApp.h : Contains UART interrupt app test example header.
┃ ┣ 📂examples_config
┃ ┃ ┣ 📂Uart_Demo_Cfg
┃ ┃ ┃ ┣ 📂soc
┃ ┃ ┃ ┃ ┣ 📂am261
┃ ┃ ┃ ┃ ┃ ┣ 📂r5f0_0
┃ ┃ ┃ ┃ ┃ ┃ ┣ 📂include
┃ ┃ ┃ ┃ ┃ ┃ ┃ ┣ 📜Cdd_Uart_Cfg.h : Contains the Precompile switches, Symbolic names.
┃ ┃ ┃ ┃ ┃ ┃ ┣ 📂src
┃ ┃ ┃ ┃ ┃ ┃ ┃ ┣ 📜Cdd_Uart_Cfg.c : Contains all Pre-Compile Configured parameters
┃ ┃ ┃ ┃ ┃ ┃ ┃ ┣ 📜Cdd_Uart_PBcfg.c : Contains all Post-Build Configured parameters
┃ 📂mcal_config
┃ 📂mcal_docs
┣ 📜README.txt
4.11.11. FAQ’s
None