4.9. CDD_IPC Module

4.9.1. Acronyms and Definitions

Abbreviation/Term

Explanation

AUTOSAR

Automotive Open System Architecture

BSW

Basic Software

MCAL

Micro Controller Abstraction Layer

API

Application Programming Interface

DET

Default Error Tracer

IPC

Inter Process Communication

SW

Software

MCU

Micro Controller Unit

OS

Operating System

CDD

Complex Device Driver

4.9.2. Introduction

This document describes the functionality, API and configuration of the AUTOSAR BSW module Complex Device driver for IPC on AM261x device.

Supported AUTOSAR Release

4.3.1

Supported Configuration Variants

Post Build

Vendor ID

CDD_IPC_VENDOR_ID (44)

Module ID

CDD_IPC_MODULE_ID (255)

Supported Platform

AM261x

4.9.3. Functional Overview

The main tasks of Complex Device Driver for IPC are the following:

  1. Initialization of the mailbox driver

  2. Simplifies reading and writing to the mailbox peripheral.

4.9.3.1. Complex Device Driver Architecture

The following figure shows where the Complex device driver is located in the AUTOSAR architecture.

CDD in AUTOSAR architecture

Fig. 4.39 CDD in AUTOSAR architecture

4.9.3.2. Initialization

The initialization covers the following steps:

  1. Initialize the mailbox peripheral.

  2. Cdd_Ipc_Init should be called only once during initialization.

  3. No other CDD API can be invoked until this API is called.

4.9.4. Hardware Features

4.9.4.1. Supported Features

  • Open/Close mailbox instance

  • Send/Receive both Notify and RpMsg messages

  • RpMsg Callback functionality supported

4.9.4.2. Not supported Features

  • Multiple mailbox channels between the cores

  • Applications are validated only for the R50_0 core

4.9.5. Source files

Description of static files is provided below:

📦AM261x
┣ 📂build
┣ 📂mcal
┃ ┣ 📂Ipc
┃ ┃ ┣ 📂include
┃ ┃ ┃ ┣ 📜Cdd_Ipc.h : Contains interface header for Complex device driver for IPC
┃ ┃ ┃ ┣ 📜Cdd_Ipc_Irq.h : contains ISR function declaration for Complex Device Driver
┃ ┃ ┃ ┣ 📜ipc_notify_lld_utils.h : Contains Internal functions declaration
┃ ┃ ┃ ┣ 📜ipc_notify_v1_lld.h : Contains Internal functions declaration
┃ ┃ ┃ ┣ 📜ipc_notify_v1_mailbox.h : Contains Internal functions declaration
┃ ┃ ┃ ┣ 📜ipc_rpmsg_linux_resource_table.h : Contains Internal functions declaration
┃ ┃ ┃ ┣ 📜ipc_rpmsg_lld.h : Contains Internal functions declaration
┃ ┃ ┃ ┣ 📜ipc_rpmsg_lld_priv.h : Contains Internal functions declaration
┃ ┃ ┃ ┗ 📜ipc_rpmsg_lld_queue.h : Contains Internal functions declaration
┃ ┃ ┣ 📂src
┃ ┃ ┃ ┣ 📜Cdd_Ipc.c : Contains function definitions for the Complex device driver for IPC and helper functions
┃ ┃ ┃ ┣ 📜Cdd_Ipc_Irq.c : Contains ISR function definitions for Complex Device Driver
┃ ┃ ┃ ┣ 📜ipc_notify_lld_utils.c : Contains Internal functions definition
┃ ┃ ┃ ┣ 📜ipc_notify_v1_lld.c : Contains Internal functions definition
┃ ┃ ┃ ┣ 📜ipc_rpmsg_lld.c : Contains Internal functions definition
┃ ┃ ┃ ┗ 📜ipc_rpmsg_lld_vring.c : Contains Internal functions definition
┃ ┃ ┣ 📂V2
┃ ┃ ┃ ┣ 📜ipc_notify_v1_cfg_lld.c : Contains Internal functions definition
┃ ┃ ┃ ┗ 📜ipc_notify_v1_cfg_lld.h : Contains Internal functions definition
┃ ┃ ┗ 📜Makefile
┣ 📂mcal_config
┣ 📂mcal_docs
┗ 📜README.txt

The below diagram shows the files structure for the CDD driver.

CDD header file include structure

Fig. 4.40 CDD header file include structure

4.9.6. Module requirements

4.9.6.1. Memory Mapping

Memory Mapping Sections

CDD_CODE

CDD_CODE_ISR

CDD_VAR_NO_INIT

CDD_VAR_ZERO_INIT

CDD_IPC_START_SEC_VAR_INIT_UNSPECIFIED (.bss)

x

CDD_IPC_STOP_SEC_VAR_INIT_UNSPECIFIED

x

CDD_IPC_START_SEC_CODE_APPL (.text)

x

CDD_IPC_STOP_SEC_CODE_APPL

x

CDD_IPC_START_SEC_VAR_UNSPECIFIED (.data)

x

CDD_IPC_STOP_SEC_VAR_UNSPECIFIED

x

CDD_IPC_START_SEC_CODE(.rodata)

x

CDD_IPC_START_SEC_CODE

x

4.9.6.2. Scheduling

There is no scheduling functions in CDD IPC.

4.9.6.3. Error handling

4.9.6.3.1. Development Error Reporting

Development errors are reported to the DET using the service Det_ReportError().

4.9.6.4. Error codes

4.9.6.4.1. Development Errors

The errors reported to DET and DEM are described in the following table

Type of Error

Related Error code

Value (Hex)

Error code indicating the IPC is uninitialized

CDD_IPC_E_UNINIT

0x01

Error code indicating register client failed event

CDD_IPC_E_REGISTER_CLIENT_FAILED

0x02

Error code indicating IPC Initialization Failed

CDD_IPC_E_INIT_FAILED

0x03

Error code indicating IPC Deinitialization Failed

CDD_IPC_E_DEINIT_FAILED

0x04

Error code indicating invalid parameter

CDD_IPC_E_PARAM_POINTER

0x05

Error code indicating IPC already initialized

CDD_IPC_E_ALREADY_INITIALIZED

0x06

Error code indicating Service called with wrong param

CDD_IPC_E_PARAM_VALUE

0x07

Error code indicating Service called with invalid length

CDD_IPC_E_PARAM_LENGTH

0x08

Error code indicating invalid IPC Channel

CDD_IPC_E_INVALID_CHANNEL

0x09

Error code indicating invalid IPC configuration

CDD_IPC_E_INVALID_CONFIG

0x0A

Error code indicating IPC Write Failed configuration

CDD_IPC_E_WRITE_FAILED

0x0B

Error code indicating unregister client failed event

CDD_IPC_E_UNREGISTER_CLIENT_FAILED

0x0C

Error code indicating construct failed event

CDD_IPC_E_CONSTRUCT_FAILED

0x0D

Error code indicating RpMsg Write failed event

CDD_IPC_E_RPMSG_WRITE_FAILED

0x0E

Error code indicating Rpmsg read failed event

CDD_IPC_E_RPMSG_READ_FAILED

0x0F

Error code indicating destruct failed event

CDD_IPC_E_DESTRUCT_FAILED

0x10

4.9.6.4.2. Parameter Checking

AUTOSAR requires that API functions check the validity of their parameters. These checks are for development error reporting and can be en-/disabled via the parameter CDD_IPC_DEV_ERROR_DETECT. The following table shows which parameter checks are performed on which services:

Services

CDD_IPC_E_UNINIT

CDD_IPC_E_REGISTER_CLIENT_FAILED

CDD_IPC_E_UNREGISTER_CLIENT_FAILED

CDD_IPC_E_PARAM_POINTER

CDD_IPC_E_ALREADY_INITIALIZED

CDD_IPC_E_PARAM_VALUE

CDD_IPC_E_WRITE_FAILED

CDD_IPC_E_CONSTRUCT_FAILED

CDD_IPC_E_RPMSG_WRITE_FAILED

CDD_IPC_E_RPMSG_READ_FAILED

Cdd_Ipc_Init

x

x

Cdd_Ipc_DeInit

x

x

Cdd_Ipc_Notify_RegisterClient

x

x

x

Cdd_Ipc_Notify_UnregisterClient

x

x

x

Cdd_Ipc_Notify_Write

x

x

x

x

Cdd_Ipc_Construct

x

x

Cdd_Ipc_Destruct

x

x

Cdd_Ipc_RpMsg_SendMsg

x

x

x

Cdd_Ipc_RpMsg_SendMsg

x

x

x

4.9.7. Used resources

4.9.7.1. Interrupt Handling

For interrupt notification, ISR’s are provided in CDD IPC driver.Interrupt Subroutine calls notification function depending on the channel mode.

ISR for IPC Interrupt: Cdd_Ipc_Isr

Interrupt Id for MBox Read Request is 136.

4.9.8. Integration description

4.9.8.1. Dependent modules

4.9.8.1.1. OSEK/AUTOSAR OS (Optional)

An operating system can be used for task scheduling, interrupt handling, global suspend and restore of interrupts and creating of the Interrupt Vector Table. The CDD module may use OSEK/AUTOSAR OS to suspend and restore global interrupts.

4.9.8.1.2. DET (Optional)

The module CDD depends on the DET (by default) in order to report development errors. The mailbox operations like write, read are protected by a critical section.

4.9.8.1.3. Services used by Complex device Driver

The CDD does not provide any call back functions.

4.9.8.1.4. Notifications

At its configurable interfaces the CDD defines notifications that can be mapped to callback functions provided by other modules. The mapping is not statically defined by the CDD but can be performed at configuration time. The function prototypes that can be used for the configuration have to match the appropriate function prototype signatures, which are described in the following.

Cdd_Ipc_notify_msgHandler: This is defined in the Cdd_Ipc_notify_app.c for reference.

4.9.8.2. Multi-core support

Not supported

4.9.9. Configuration

4.9.9.1. CddIpcDriver

This container contains the configuration parameters and sub containers of the AUTOSAR Complex device driver(CDD) module.

4.9.9.1.1. CddIpcLocalCoreId

Item

Name

CddIpcLocalCoreId

Description

This param contains the local coreId on which the IPC instance is running.

Origin

Texas Instruments

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Default-value

CDD_IPC_R5FSS0_0_ID

Range

CDD_IPC_R5FSS0_0_ID
CDD_IPC_R5FSS0_1_ID

4.9.9.1.2. CddIpcRemoteCoreList

Refers to the list of coreId that are valid for the particular platform.

4.9.9.1.2.1. CddIpcRemoteCoreIdIndex

Item

Name

CddIpcRemoteCoreIdIndex

Description

The cores that are participating the IPC message exchange (Exclude the local core from these)

Origin

Texas Instruments

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Default-value

CDD_IPC_R5FSS0_0_ID

Range

CDD_IPC_R5FSS0_0_ID
CDD_IPC_R5FSS0_1_ID

4.9.9.1.2.2. CddIpcSafeIpcCoresEnable

Item

Name

CddIpcSafeIpcCoresEnable

Description

Switch to enable Safe Ipc between local and remote core.

Multiplicity-Configuration-Class

Post-Build Time

VARIANT-POST-BUILD

Origin

Texas Instruments

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Default-value

false

4.9.9.1.3. CddIpcEndPtConfig

This is required only in case of RpMsg is being used. To enable this make sure the CddIpcRpMsgEnable box is enabled.

4.9.9.1.3.1. CddIpcLocalEndPt

Item

Name

CddIpcLocalEndPt

Description

This parameter is used to register a local call back especially for receiving or sending a RPMsg message

Multiplicity-Configuration-Class

Post-Build Time

VARIANT-POST-BUILD

Origin

Texas Instruments

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Default-value

12

Max-value

63

Min-value

0

4.9.9.1.3.2. CddIpcRecvCallBack

Item

Name

CddIpcRecvCallBack

Description

Function pointer to RPMSG callback function

Multiplicity-Configuration-Class

Post-Build Time

VARIANT-POST-BUILD

Origin

Texas Instruments

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Default-value

NULL

4.9.9.1.3.3. CddIpcrecvCallbackArguments

Item

Name

CddIpcrecvCallbackArguments

Description

Function Pointer to recv callback function’s arguments

Multiplicity-Configuration-Class

Post-Build Time

VARIANT-POST-BUILD

Origin

Texas Instruments

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Default-value

NULL

4.9.9.1.3.4. CddIpcrecvNotifyCallback

Item

Name

CddIpcrecvNotifyCallback

Description

Function pointer to IPC notify message Callback function. User can pass a pointer to a custom defined arguments structure and the callback passes this pointer when a notify interrupt is received

Multiplicity-Configuration-Class

Post-Build Time

VARIANT-POST-BUILD

Origin

Texas Instruments

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Default-value

NULL

4.9.9.1.3.5. CddIpcrecvNotifyCallbackArguments

Item

Name

CddIpcrecvNotifyCallbackArguments

Description

Pointer to IPC notify message callback function’s arguments

Multiplicity-Configuration-Class

Post-Build Time

VARIANT-POST-BUILD

Origin

Texas Instruments

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Default-value

NULL

4.9.9.2. CddIpcGeneral

Item

Name

CddIpcGeneral

Description

Switches the Cdd_IpcDeinit function ON or OFF.

Post-build-variant-multiplicity

false

Origin

Texas Instruments

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Default-value

true

4.9.9.2.1. CddIpcWriteApi

Item

Name

CddIpcWriteApi

Description

Switches the Cdd_IpcWrite function ON or OFF.

Origin

Texas Instruments

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Default-value

true

4.9.9.2.2. CddIpcReadApi

Item

Name

CddIpcReadApi

Description

Switches the Cdd_IpcRead function ON or OFF.

Origin

Texas Instruments

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Default-value

true

4.9.9.2.3. CddIpcRpMsgEnable

Item

Name

CddIpcRpMsgEnable

Description

Switch to enable RpMsg API’s to be enabled or not.

Origin

Texas Instruments

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Default-value

true

4.9.9.2.4. CddIpcRecvCallBackEnable

Item

Name

CddIpcRecvCallBackEnable

Description

Switch to Enable RPMsg Recv Callback (This is different from Notify Callback).

Multiplicity-Configuration-Class

Post-Build Time

VARIANT-POST-BUILD

Origin

Texas Instruments

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Default-value

true

4.9.9.2.5. CddIpcRecvNotifyCallbackEnable

Item

Name

CddIpcRecvNotifyCallbackEnable

Description

Switches the Development Error Detection and Notification ON or OFF.

Multiplicity-Configuration-Class

Post-Build Time

VARIANT-POST-BUILD

Origin

Texas Instruments

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Default-value

true

4.9.9.2.6. CddIpcSafeIpcEnable

Item

Name

CddIpcSafeIpcEnable

Description

Switch to enable Safe Ipc to be enabled or not.

Origin

Texas Instruments

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Default-value

false

4.9.9.2.7. CddIpcCrcEnable

Item

Name

CddIpcCrcEnable

Description

Switch to enable Crc to be enabled or not.

Origin

Texas Instruments

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Default-value

false

4.9.9.2.8. CddIpcCrcHookFunc

Item

Name

CddIpcCrcHookFunc

Description

Type of Isr function: void functionname(void) CAT1 : interrupt void func(void) CAT2 : ISR(func)

Multiplicity-Configuration-Class

Post-Build Time

VARIANT-POST-BUILD

Origin

Texas Instruments

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Default-value

CDD_IPC_ISR_VOID

Range

CDD_IPC_ISR_VOID
CDD_IPC_ISR_CAT1
CDD_IPC_ISR_CAT2

4.9.9.2.9. CddIpcTimeout

Item

Name

CddIpcTimeout

Description

Timeout value for send/receive/wait API’s. Unit is in clock ticks

Origin

Texas Instruments

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Default-value

2000000

Max-value

2147483648

Min-value

0

4.9.9.2.10. CddIpcNumOfBuffers

Item

Name

CddIpcNumOfBuffers

Description

This parameter indicates the number of buffers for sending RPMsg

Origin

Texas Instruments

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Default-value

8

Note: In case of CddIpcRecvCallBack , when RPMsg arrive then that is invoked along with the data in the VRING buffer.So now if the msg size is less then what we are transferring between cores then we will send the echo msg back to the core from which we are receiving and will do UNLOCK of core only if complete msg transfer happens.So by this way we are acknowledging the remote core.

4.9.10. Examples

4.9.10.1. Overview

CDD example application demonstrating the Complex device driver features 2 different examples namely ipc_notify_app and ipc_rpmsg_app.

4.9.10.1.1. Ipc_notify_app_working

This application is low payload, low latency message type where user will be able to send a maximum of 28bits of data as the payload. The first 4 bits are used internally by the driver for the client ID. Notify app sends 1000000, to all the other 3 cores and waits for all of them to echo back. To make the example work with lesser cores, edit the following parameters in the example.

  1. #define MAX 2 To the number of cores user needs to reduce.

  2. uint32 gRemoteCoreId[]; Enable only the cores that are required.

  3. uint32 gIpcTransferMutex[MAX] Remove the extra Lock variables (These can be replced with any kind of mutex or semaphore implementation at the user End).

  4. In addition to these please also ensure the Cdd_Ipc_PBCfg.c has the proper cores configured from the XDM file.

The same changes stand valid for the rpmsg_echo_app as well.

4.9.10.1.2. Ipc_rpmsg_app working

  1. RpMsg application uses Vrings as the medium to send larger data whose size and buffer depth can be configured using the parameters CDD_IPC_NUM_OF_BUFFERS and CDD_IPC_MAX_BUFFER_SIZE.

  2. The application exchanges 100000 messages, the payload data is integer value where it gets incremented on every echo back from each core. In order to change the data from the integer to other data i.e., String or characters for command use-cases please change the following line.

snprintf(msgBuf, MAX_MSG_SIZE-1, "%d", msg);

to

snprintf(msgBuf, MAX_MSG_SIZE-1, "%s", Your String Data);

The notify application is present under the path <MCAL_ROOT>/examples/Ipc/Ipc_app_notify. This application can be built from the build folder by giving "gmake -s ipc_notify_app PLATFORM=am261".

The rpmsg application is present under the path <MCAL_ROOT>/examples/Ipc/Ipc_app_rpmsg. This application can be built from the build folder by giving "gmake -s ipc_rpmsg_app PLATFORM=am261".

4.9.10.2. Setup required to run example

None

4.9.10.3. How to run examples

4.9.10.3.1. Ipc_notify_app_working/Ipc_rpmsg_app working

Examples to import from SDK to validate the CDD_IPC(Notify and Rpmsg) example,

  1. Use all the other cores except R50_0 (this is where CDD_IPC app will be run), the path to the examples inside MCU+SDK directory

  2. $(MCU_PLUS_SDK_PATH)/examples/drivers/ipc/ipc_notify_echo/am261x-som

  3. $(MCU_PLUS_SDK_PATH)/examples/drivers/ipc/ipc_rpmsg_echo/am261x-som

  4. After building SDK amd Mcal library, load the Mcal binary in R50_0 and SDK binary in all the other R5 core(R50_1) and execute the binary.

4.9.10.3.2. Notify App Sample Output

../_images/ipc_notifyappsample.png

4.9.10.3.3. RPMsg App Sample Output

../_images/ipc_rpmsgappsample.png

4.9.10.4. Sample Log

Ipc Notify:

CDD_IPC_NOTIFY_APP: Sample IPC Application started!
CDD_IPC_NOTIFY_APP: Sync All Completed
CDD_IPC_NOTIFY_APP: Message exchange started by main core
CDD_IPC_NOTIFY_APP: All echoed messages received by main core from 1 remote cores !!!
CDD_IPC_NOTIFY_APP: Messages sent to each core = 1000000
CDD_IPC_NOTIFY_APP: Number of remote cores = 1
All tests have passed

Ipc Rpmsg:

CDD_IPC_RPMSG_APP: Sample IPC Application started!
CDD_IPC_RPMSG_APP: Sync All Completed
CDD_IPC_RPMSG_APP: RpMsg Message exchange started by main core
CDD_IPC_RPMSG_APP: All echoed messages received by main core from 1 remote cores !!!
CDD_IPC_RPMSG_APP: Messages sent to each core = 100000
CDD_IPC_RPMSG_APP: Number of remote cores = 1
All tests have passed

4.9.10.5. File Structure

📦AM261x
┣ 📂build
┣ 📂mcal
┃ ┣ 📂examples
┃ ┃ ┣ 📂Ipc
┃ ┃ ┃ ┣ 📂soc
┃ ┃ ┃ ┣ 📂Ipc_app_notify
┃ ┃ ┃ ┃ ┣ 📜Cdd_Ipc_app.h : Contains Cdd Ipc example header file
┃ ┃ ┃ ┃ ┣ 📜Cdd_Ipc_notify_app.c : contains the IPC R50 test app for IPC Notify
┃ ┃ ┃ ┃ ┗ 📜Makefile
┃ ┃ ┃ ┣ 📂Ipc_app_rpmsg
┃ ┃ ┃ ┃ ┣ 📜Cdd_Ipc_app.h : Contains Cdd Ipc example header file
┃ ┃ ┃ ┃ ┣ 📜Cdd_Ipc_rpmsg_app.c : Contains IPC R50 test app for RpMsg
┃ ┃ ┃ ┃ ┗ 📜Makefile
┃ ┃ ┃ ┣ 📂Ipc_app_rpmsg_callback_mode
┃ ┃ ┃ ┃ ┣ 📜Cdd_Ipc_app.h : Contains Cdd Ipc example header file
┃ ┃ ┃ ┃ ┣ 📜Cdd_Ipc_rpmsg_callback_app.c : Contains IPC R50 test app for RpMsg
┃ ┃ ┃ ┃ ┗ 📜Makefile
┃ ┣ 📂examples_config
┃ ┃ ┣ 📂Ipc_Demo_Cfg
┃ ┃ ┃ ┗ 📂soc
┃ ┃ ┃ ┃ ┣ 📂am261
┃ ┃ ┃ ┃ ┃ ┗ 📂r5f0_0
┃ ┃ ┃ ┃ ┃ ┃ ┣ 📂include
┃ ┃ ┃ ┃ ┃ ┃ ┃ ┗📜Cdd_Ipc_Cfg.h : Contains the configuration parameters
┃ ┃ ┃ ┃ ┃ ┃ ┗ 📂src
┃ ┃ ┃ ┃ ┃ ┃ ┃ ┣📜Cdd_Ipc_Callback_app_PBCfg.c : Contains all Pre-Compile Configured parameters with Recv CallBack Function
┃ ┃ ┃ ┃ ┃ ┃ ┃ ┗📜Cdd_Ipc_PBCfg.c : Contains all Pre-Compile Configured parameters
┃ 📂mcal_config
┃ 📂mcal_docs
┗ 📜README.txt

4.9.11. References

Technical Reference Manual