4.17. ICU Module

4.17.1. Acronyms and Definitions

Abbreviation/Term

Explanation

AUTOSAR

Automotive Open System Architecture

BSW

Basic Software

MCAL

Micro Controller Abstraction Layer

API

Application Programming Interface

DET

Default Error Tracer

ICU

Input Capture Unit

ECAP

Enhanced Capture

MCU

Micro Controller Unit

4.17.2. Introduction

This document describes the functionality, API and configuration of the AUTOSAR BSW module Icu.

Supported AUTOSAR Release

4.3.1

Supported Configuration Variants

Pre-Compile & Post-Build

Vendor ID

ICU_VENDOR_ID (44)

Module ID

ICU_MODULE_ID (122)

Supported Platform

AM261x

4.17.3. Functional Overview

The ICU module initializes, configures and controls the internal hardware to realize ICU driver as detailed in AUTOSAR BSW ICU Driver Specification. The ICU functionality is realized through the ECAP IP available on the device. Following section highlights key aspects of this implementation, which would be of interest to an integrator.

4.17.3.1. Functional Description

The ICU driver uses ECAP module to capture events. In AM261x we have a total of 8 instances of ICU. The ICU driver provides the following features:

  1. Signal Measurements - High time, Low time, Period time, Duty cycle

  2. Edge Detection - Provide notification for each edge detected

  3. Edge Counting - Measure edge counts

  4. Edge Timestamping - Measure the absolute time when edges occur

Clock Source to timers: Programming of clock source for the ICU module, is beyond the scope of this document. The driver expects that the user of this module has programmed required clock source. The example application demonstrates configuring clock sources for ECAP module

4.17.4. Hardware Features

4.17.4.1. AUTOSAR Supported Features

  • Signal edge notification

  • Periodic signal time measurement

  • Edge time stamping

  • Edge counting

4.17.4.2. Not supported Features

Wakeup functionality is not supported because of the limitation of the hardware.

4.17.5. Source files

Description of static files is provided below:

📦AM261x
┣ 📂build
┣ 📂mcal
┃ ┣ 📂Icu
┃ ┃ ┣ 📂include
┃ ┃ ┃ ┣ 📜Icu.h : Contains the API’s of the ICU driver to be used by upper layers
┃ ┃ ┃ ┗ 📜Icu_Irq.h : Contains ISR function declaration
┃ ┃ ┣ 📂src
┃ ┃ ┃ ┣ 📜Icu.c : Contains the implementation of the API’s for ICU driver
┃ ┃ ┃ ┗ 📜Icu_Irq.c : Contains ISR function definitions
┃ ┃ ┣ 📂V0
┃ ┃ ┃ ┣ 📜ecap.h : Contains Internal functions declaration of ICU driver
┃ ┃ ┃ ┣ 📜ecap.c : Contains Internal Functions definitions
┃ ┃ ┃ ┣ 📜hw_icu.h : Contains Internal functions declaration of ICU driver
┃ ┃ ┃ ┣ 📜Icu_Priv.c : Contains Internal Functions definitions
┃ ┃ ┃ ┗ 📜Icu_Priv.h : Contains Internal Functions declaration
┃ ┃ ┗ 📜Makefile
┣ 📂mcal_config
┣ 📂mcal_docs
┗ 📜README.txt

Description of generated files is provided below:

Plugin Files

Description

Icu_Cfg.h

Contains static configuration of this module

Icu_PBcfg.c

Contain the generated configuration for post-build variant

Icu_Cfg.c

Contain the generated configuration for pre-compile variant

4.17.6. Module requirements

Will be updated in future release:

4.17.6.1. Memory Mapping

Memory Mapping Sections

ICU_CODE

ICU_VAR_INIT

ICU_VAR_NOINIT

ICU_CONST

ICU_CONFIG

ICU_START_SEC_VAR_INIT_UNSPECIFIED (.data)

x

ICU_DATA_INIT_32_SECTION

x

ICU_TEXT_SECTION

x

ICU_DATA_NO_INIT_UNSPECIFIED_SECTION

x

ICU_CONST_32_SECTION

x

ICU_ISR_TEXT_SECTION

x

ICU_CONFIG_SECTION

x

4.17.6.2. Cache

This driver implementation has been validated with cache enabled. For optimal performance it’s recommended to place memmap sections in cache enabled memory area.

4.17.6.3. Scheduling

There is no scheduling functions in Icu.

4.17.6.4. Error handling

4.17.6.4.1. Development Error Reporting

Development errors are reported to the DET using the service Det_ReportError().

4.17.6.5. Error codes

4.17.6.5.1. Development Errors

The errors reported to DET module are described in the following table:

Type of Error

Related Error code

Value (Hex)

API is called with invalid pointer

ICU_E_PARAM_POINTER

0x0A

API service used with an invalid channel identifier or channel was not configured for the functionality of the called API

ICU_E_PARAM_CHANNEL

0x0B

API service used with an invalid or not feasible activation

ICU_E_PARAM_ACTIVATION

0x0C

Init Function Failed

ICU_E_INIT_FAILED

0x0D

API service used with an invalid buffer size

ICU_E_PARAM_BUFFER_SIZE

0x0E

API service Icu_SetMode used with an invalid mode

ICU_E_PARAM_MODE

0x0F

API service used without module initialization

ICU_E_UNINIT

0x14

API service Icu_SetMode is called while in running operation

ICU_E_BUSY_OPERATION

0x16

API Icu_Init service is called and when the ICU driver and the Hardware are already initialized

ICU_E_ALREADY_INITIALIZED

0x17

API Icu_StartTimeStamp is called and the parameter NotifyInterval is Invalid

ICU_E_PARAM_NOTIFY_INTERVAL

0x18

API Icu_GetVersionInfo is called and the parameter versioninfo is invalid

ICU_E_PARAM_VINFO

0x19

4.17.6.5.2. Runtime Errors

Type of Error

Related Error code

Value (Hex)

API service Icu_StopTimestamp called on a channel which was not started or already stopped

ICU_E_NOT_STARTED

0x15

4.17.7. Used resources

4.17.7.1. Interrupt Handling

4.17.7.1.1. Interrupt Configuration

The Driver doesn’t register any interrupts handler (ISR), it’s expected that consumer of this driver registers the required interrupt handler.

For every Icu channel with notification enabled, an ISR requires to be registered. The Interrupt number associated with instance of the ECAP is detailed in TRM (also, please refer the demo application). Please refer IcuApp() in Icu demo application.

Some of the ICU interrupts are not routed/mapped to this core, these interrupts would require additional programming to route these to this core. Please refer IcuApp() in Icu demo application.

4.17.7.1.2. X-Bar Configuration

In AM261x, we have X-Bar support which basically act as a mux and will be used to transmit output signal like of EPWM/GPIO to ECAP(ICU) input. Following steps need to be followed in order to configure Input X-Bar:

1.Input X-Bar for ICU is configured in MCU configuration.

2.In MCU configuration, McuInputXbarChannelTriggerConfiguration container is used to configure different X-Bar with different GPIO.

Input X-Bar is configured for GPIO61 which will be used by ICU

Fig. 4.76 Input X-Bar is configured for GPIO61 which will be used by ICU

3.Now in order to select a particular ECAP instance against that X-Bar which we have configured in MCU, their is a reference to the X-Bar in ICU.

4.XbarSelect parameter in ICU is the reference of the X-Bar which is configured in MCU.

In ICU Input X-Bar is referenced from MCU configuration

Fig. 4.77 In ICU Input X-Bar is referenced from MCU configuration

5.NOTE: When a new X-Bar is configured in MCU then exactly same mapping to be selected for the reference XbarSelect parameter in ICU.

We have a support of Interrupt XBar which act as a mux for interrupts of the peripherals.So in order to provide flexibility to the user since their use cases will be different and our SOC has so many peripherals and a large amount of events like interrupts etc, interrupt XBar is used. Following steps need to be followed in order to configure Interrupt X-Bar:

  1. Interrupt X-Bar for ICU is configured in MCU configuration.

  2. In MCU configuration, McuXbarChannelTriggerConfiguration container is used to configure different X-Bar Interrupt with different peripheral.

  3. Now interrupt registration for the particular X-Bar interrupt, need to be done at the application side of the peripheral.

  4. For example: For ICU, X-Bar Interrupt number 22 is configured in MCU and with the same Interrupt is registered in ICU application.

4.17.8. Integration description

4.17.8.1. Dependent modules

4.17.8.1.1. DET

This implementation depends on the DET in order to report development errors. The detection of development errors is configurable (ON / OFF).

4.17.8.1.2. SchM

If multiple AUTOSAR runnables have access to the same Data Store Memory block, the exported AUTOSAR specification enforces data consistency by using an AUTOSAR exclusive area. With this specification, the runnables have mutually exclusive access to the per-instance memory global data, which prevents data corruption. Beside the OS, the BSW Scheduler provides functions that ICU module calls at begin and end of critical sections. This implementation requires 1 level of exclusive access to guard critical sections.

The data consistency mechanism that has to be applied to an ExclusiveArea might be domain, ECU or even project specific. The decision which mechanism has to be applied by RTE / Basic Software Scheduler is taken during ECU integration by setting the Exclusive Area configuration parameter RteExclusiveAreaImplMechanism. This parameter is an input for RTE generator.

For ICU Module, data consistency and exclusive access to critical sections are required for the following sections as shown in the table below:

Exclusive Area Functions used

ICU Function calling Exclusive Area

Need for Exclusive Area

Recommended Exclusive Area Mapping

ICU_EXCLUSIVE_AREA_0

Icu_DisableNotification
Icu_EnableNotification
Icu_SetActivationCondition
Icu_GetInputState
Icu_EnableEdgeDetection
Icu_DisableEdgeDetection
Icu_StartTimestamp
Icu_StopTimestamp
Icu_GetTimestampIndex
Icu_ResetEdgeCount
Icu_EnableEdgeCount
Icu_DisableEdgeCount
Icu_GetEdgeNumbers
Icu_StartSignalMeasurement
Icu_StopSignalMeasurement
Icu_GetTimeElapsed
Icu_GetDutyCycleValues

To protect against multiple access for shared resources

ALL_INTERRUPT_BLOCKING : All interrupts should be blocked as this API’s can be called in the interrupts

4.17.8.2. Multi-core support

Not Supported

4.17.9. Configuration

4.17.9.1. IcuConfigSet

This container contains the configuration parameters and sub containers of the AUTOSAR Icu module.

4.17.9.1.1. IcuChannel

Configuration of an individual ICU channel.

4.17.9.1.1.1. IcuChannelId

Item

Name

IcuChannelId

Description

Channel Id of the ICU channel. This value will be assigned to the symbolic name derived of the IcuChannel container short name.

Origin

AUTOSAR_ECUC

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Max-value

7

Min-value

0

4.17.9.1.1.2. IcuDefaultStartEdge

Item

Name

IcuDefaultStartEdge

Description

Configures the capture event to enable interupt on that capture event or not

Origin

Texas Instruments

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

true

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

ECAP_INT_ALLCAPS

Range

ECAP_CEVT1_INT
ECAP_CEVT2_INT
ECAP_CEVT3_INT
ECAP_CEVT4_INT
ECAP_CEVT1_CEVT2_INT
ECAP_CEVT1_CEVT3_INT
ECAP_CEVT1_CEVT4_INT
ECAP_CEVT2_CEVT3_INT
ECAP_CEVT2_CEVT4_INT
ECAP_CEVT3_CEVT4_INT
ECAP_CEVT1_CEVT2_CEVT3_INT
ECAP_CEVT1_CEVT2_CEVT4_INT
ECAP_CEVT1_CEVT3_CEVT4_INT
ECAP_CEVT2_CEVT3_CEVT4_INT
ECAP_INT_ALLCAPS

4.17.9.1.1.3. IcuMeasurementMode

Item

Name

IcuMeasurementMode

Description

Configures the measurement mode of this channel.

Origin

AUTOSAR_ECUC

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

true

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

ICU_MODE_SIGNAL_MEASUREMENT

Range

ICU_MODE_EDGE_COUNTER
ICU_MODE_SIGNAL_EDGE_DETECT
ICU_MODE_SIGNAL_MEASUREMENT
ICU_MODE_TIMESTAMP

4.17.9.1.1.4. IcuPrescaler

Item

Name

IcuPrescaler

Description

Time-Base Clock Prescale Bits. Keep value as 0 to by-pass prescaler.

Origin

Texas Instruments

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

0

Max-value

31

Min-value

0

4.17.9.1.1.5. IcuFunctionalClock

Item

Name

IcuFunctionalClock

Description

Value of the System clock frequency in MHz Default frequency is 125MHz for ICU.

Origin

Texas Instruments

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

true

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

200

4.17.9.1.1.6. IcuXbarSelect

Item

Name

IcuXbarSelect

Description

Configures the input select xbar to be used in order to give icu the required input

Origin

Texas Instruments

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

true

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

4.17.9.1.2. IcuSignalEdgeDetection

This container contains the configuration (parameters) in case the measurement mode is “IcuSignalEdgeDetection”

4.17.9.1.2.1. IcuSignalNotification

Item

Name

IcuSignalNotification

Description

Notification function for signal notification.

Multiplicity-Configuration-Class

Post-Build Time

VARIANT-POST-BUILD

Pre-Compile Time

VARIANT-PRE-COMPILE

Origin

AUTOSAR_ECUC

Post-build-variant-multiplicity

true

Post-Build-Variant-Value

true

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

4.17.9.1.3. IcuSignalMeasurement

This container contains the configuration (parameters) in case the measurement mode is “IcuSignalMeasurement”

4.17.9.1.3.1. IcuSignalMeasurementProperty

Item

Name

IcuSignalMeasurementProperty

Description

Configures the property that could be measured in case the mode is “IcuSignalMeasurement”.

Origin

AUTOSAR_ECUC

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

true

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

ICU_PERIOD_TIME

Range

ICU_DUTY_CYCLE
ICU_HIGH_TIME
ICU_LOW_TIME
ICU_PERIOD_TIME

4.17.9.1.4. IcuTimestampMeasurement

This container contains the configuration (parameters) in case the measurement mode is “IcuTimestamp”

4.17.9.1.4.1. IcuTimestampMeasurementProperty

Item

Name

IcuTimestampMeasurementProperty

Description

Configures the handling of the buffer in case the mode is “Timestamp”

Origin

AUTOSAR_ECUC

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

true

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

ICU_LINEAR_BUFFER

Range

ICU_CIRCULAR_BUFFER
ICU_LINEAR_BUFFER

4.17.9.1.4.2. IcuTimestampNotification

Item

Name

IcuTimestampNotification

Description

Notification function if the number of requested timestamps

Multiplicity-Configuration-Class

Post-Build Time

VARIANT-POST-BUILD

Pre-Compile Time

VARIANT-PRE-COMPILE

Origin

AUTOSAR_ECUC

Post-build-variant-multiplicity

true

Post-Build-Variant-Value

true

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

4.17.9.1.5. IcuWakeup

This container contains the configuration (parameters) needed to configure a wakeup capable channel

4.17.9.1.5.1. IcuChannelWakeupInfo

Item

Name

IcuChannelWakeupInfo

Description

If the wakeup-capability is true the wakeup source referenced is transmitted to the ECU State Manager (EcuM) .

Multiplicity-Configuration-Class

Post-Build Time

VARIANT-POST-BUILD

Pre-Compile Time

VARIANT-PRE-COMPILE

Origin

AUTOSAR_ECUC

Post-build-variant-multiplicity

true

Post-Build-Variant-Value

true

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

4.17.9.2. IcuGeneral

Configuration of general ICU parameters.

4.17.9.2.1. IcuDevErrorDetect

Item

Name

IcuDevErrorDetect

Description

Switches the development error detection and notification on or off.

Origin

AUTOSAR_ECUC

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

false

4.17.9.2.2. IcuIrqType

Item

Name

IcuIrqType

Description

ISR Category type:
CAT1 : void func(void)
CAT2 : ISR(func)

Origin

Texas Instruments

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

false

Value-Configuration-Class

Pre-Compile-Time

VARIANT-PRE-COMPILE

Post-Build-Time

VARIANT-POST-BUILD

Default-value

ICU_ISR_CAT1

Range

ICU_ISR_VOID
ICU_ISR_CAT1
ICU_ISR_CAT2

4.17.9.2.3. IcuDeviceVariant

Item

Name

IcuDeviceVariant

Description

Select SOC variant

Origin

Texas Instruments

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

false

Value-Configuration-Class

Pre-Compile-Time

VARIANT-PRE-COMPILE

Post-Build-Time

VARIANT-POST-BUILD

Default-value

AM261x

Range

AM261x

4.17.9.3. IcuOptionalApis

This container contains all configuration switches for configuring optional API services of the ICU driver.

4.17.9.3.1. IcuDeInitApi

Item

Name

IcuDeInitApi

Description

Adds / removes the service Icu_DeInit() from the code.

Origin

AUTOSAR_ECUC

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

false

4.17.9.3.2. IcuDisableWakeupApi

Item

Name

IcuDisableWakeupApi

Description

Adds / removes the service Icu_DisableWakeup() from the code.

Origin

AUTOSAR_ECUC

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

false

4.17.9.3.3. IcuEdgeCountApi

Item

Name

IcuEdgeCountApi

Description

Adds / removes all services related to the edge counting functionality as listed below, from the code: Icu_ResetEdgeCount(), Icu_EnableEdgeCount(), Icu_DisableEdgeCount(), Icu_GetEdgeNumbers().

Origin

AUTOSAR_ECUC

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

false

4.17.9.3.4. IcuEdgeDetectApi

Item

Name

IcuEdgeDetectApi

Description

Adds / removes the services related to the edge detection functionality, from the code:

Origin

AUTOSAR_ECUC

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

false

4.17.9.3.5. IcuEnableWakeupApi

Item

Name

IcuEnableWakeupApi

Description

Adds / removes the service Icu_EnableWakeup() from the code.

Origin

AUTOSAR_ECUC

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

false

4.17.9.3.6. IcuGetDutyCycleValuesApi

Item

Name

IcuGetDutyCycleValuesApi

Description

Adds / removes the service Icu_GetDutyCycleValues() from the code.

Origin

AUTOSAR_ECUC

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

false

4.17.9.3.7. IcuGetInputStateApi

Item

Name

IcuGetInputStateApi

Description

Adds / removes the service Icu_GetInputState() from the code.

Origin

AUTOSAR_ECUC

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

false

4.17.9.3.8. IcuGetTimeElapsedApi

Item

Name

IcuGetTimeElapsedApi

Description

Adds / removes the service Icu_GetTimeElapsed() from the code.

Origin

AUTOSAR_ECUC

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

false

4.17.9.3.9. IcuGetVersionInfoApi

Item

Name

IcuGetVersionInfoApi

Description

Adds / removes the service Icu_GetVersionInfo() from the code.

Origin

AUTOSAR_ECUC

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

false

4.17.9.3.10. IcuSetModeApi

Item

Name

IcuSetModeApi

Description

Adds / removes the service Icu_SetMode() from the code.

Origin

AUTOSAR_ECUC

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

false

4.17.9.3.11. IcuSignalMeasurementApi

Item

Name

IcuSignalMeasurementApi

Description

Adds / removes the services Icu_StartSignalMeasurement() and Icu_StopSignalMeasurement() from the code.

Origin

AUTOSAR_ECUC

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

false

4.17.9.3.12. IcuTimestampApi

Item

Name

IcuTimestampApi

Description

Adds / removes all services related to the timestamping functionality as listed below from the code: Icu_StartTimestamp(), Icu_StopTimestamp(), Icu_GetTimestampIndex().

Origin

AUTOSAR_ECUC

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

false

Value-Configuration-Class

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

false

By default Signal measurement mode is selected but if user want to change it to some other mode so in that case following operation they need to perform:

  1. Change the configuration from the EB tresos tool.

  2. So in case of icu, timestamp mode and edge detection mode also involve interupt callback to be registered. So by default we have given callback name in our application, with that name you can configure callback also in EB tresos.

  3. For Edge detection mode callback name is: Icu_SignalNotification_Channel1.
    For Timestamp mode callback name is : Icu_TimeStampNotification_Channel1

  4. Except this rest of the parameters can be configured as provided in EB plugin.

IsrCallback:

Mode

CallBack

Signal Measurement Mode

NA

Edge Detection Mode

Icu_SignalNotification_Channel1

TimeStamp Mode

Icu_TimeStampNotification_Channel1

Edge Count Mode

NA

The following section details on the un-supported features and additional features added.

4.17.9.4. Variance / Deviation from the specification

APIs (listed below) related to wakeup capability are not supported as the hardware does not support.

  • Controlling Wakeup interrupts

  • Icu_SetMode()

  • Icu_DisableWakeup()

  • Icu_EnableWakeup()

  • Icu_CheckWakeup()

4.17.10. Examples

4.17.10.1. Overview

  • Icu Example

    • Initialize clock using Mcu_Init()

    • Initialize port using Port_Init()

    • Configure Icu interrupt using Icu_InterruptConfig()

    • Initialize Pwm using Pwm_Init()

    • Get Icu Version using Icu_GetVersionInfo()

    • Initialize Icu using Icu_Init()

    • For Signal measurement

      • Start the measurement of signals using Icu_StartSignalMeasurement()

      • Stop the measurement of signals using Icu_StopSignalMeasurement()

      • Read the elapsed Signal Low Time for the given channel using Icu_GetTimeElapsed()

      • Read the active time and period time for the ICU Channel and calculate duty cycle.

4.17.10.2. Setup required to run example

None

4.17.10.3. How to run examples

4.17.10.3.1. Build and Running the Example Application

Please follow steps detailed in section to build library or example.

ECAP based application name - icu_app

This application uses the PWM (Enhanced Pulse Width Module) to provide input to ECAP instance. The ECAP module (with ICU driver) will capture the signals provided as input.

There is one example application provided: icu_app. Please refer to below directory structures.

  • Config files for icu_app are located along with other applications configs at / mcal_sitara_mcu/mcal/examples/config/Icu_Cfg and Icu_PBcfg can also be found as this location.

  • IcuApp.c and IcuApp.h: Shall implement the start-up code sequence and register interrupts and also shall implement the example application that demonstrates the use of the driver.

4.17.10.3.2. Flow of the example application

In the IcuApp.c , following steps are there:

  1. Firstly the pin mux is initialize

  2. UART is enabled.

  3. After that EPWM is enabled , since the output of EPWM is used as an input to our ICU.

  4. After that the ICU is initialize

  5. So by default we have configured ICU in signal measurement mode, but if the user want to change then they need to change the configuration accordingly.

  6. By default we are using EPWM0 for our input to ICU.

  7. And we are taking ECAP0( ICU 0\ :sup:TH instance ) for the demonstration of our example.

  8. So now when we execute our example with default configuration we will be getting active time, period time and duty cycle as part of the signal measurement.

4.17.10.4. Sample Log

IcuApp: Sample Application - STARTS !!!
  
ICU_APP: ICU MCAL Version Info
---------------------
ICU_APP: Vendor ID: 44
ICU_APP: Module ID: 122
ICU_APP: SW Major Version: 10
ICU_APP: SW Minor Version: 1
ICU_APP: SW Patch Version: 0
 
ICU_APP: Variant - Post Build being used !!!
 
ICU_APP: Signal Measurement Mode! 
ICU_APP: elapsed time (Period) is  998 us
ICU_APP: Active Time is 499 
ICU_APP: Period Time is 998 
ICU_APP: Duty Cycle is 0.500000
ICU_APP: elapsed time read is  0 us
ICU_APP: elapsed time (Period) is  998 us
ICU_APP: Active Time is 499 
ICU_APP: Period Time is 998 
ICU_APP: Duty Cycle is 0.500000
All tests have passed

4.17.10.5. File Structure

📦AM261x
┣ 📂build
┣ 📂mcal
┃ ┣ 📂examples
┃ ┃ ┣ 📂Icu
┃ ┃ ┃ ┣ 📂soc
┃ ┃ ┃ ┣ 📜IcuApp.c : Contains Icu test example
┃ ┃ ┃ ┣ 📜IcuApp.h : Contains Icu test example header file
┃ ┃ ┃ ┗ 📜Makefile
┃ ┣ 📂examples_config
┃ ┃ ┣ 📂Icu_Demo_Cfg
┃ ┃ ┃ ┗ 📂soc
┃ ┃ ┃ ┃ ┣ 📂am261
┃ ┃ ┃ ┃ ┃ ┗ 📂r5f0_0
┃ ┃ ┃ ┃ ┃ ┃ ┣ 📂include
┃ ┃ ┃ ┃ ┃ ┃ ┃ ┗📜Icu_Cfg.h : Contains the configuration parameters
┃ ┃ ┃ ┃ ┃ ┃ ┗ 📂src
┃ ┃ ┃ ┃ ┃ ┃ ┃ ┣📜Icu_Cfg.c : Contains all Pre-Compile Configured parameters
┃ ┃ ┃ ┃ ┃ ┃ ┃ ┗ 📜Icu_PBcfg.c : contains all Post build configured parameters
┃ 📂mcal_config
┃ 📂mcal_docs
┗ 📜README.txt

4.17.11. References

AUTOSAR_SWS_ICUDriver
Technical Reference Manual