AM64x MCU+ SDK  12.01.00

Introduction

PCIE Driver API/interface file.

Go to the source code of this file.

Data Structures

struct  Pcie_DeviceCfgBaseAddr
 The Pcie_DeviceCfg is used to specify device level configuration of the driver instance. More...
 
struct  Pcie_ObAtuCfg
 Pcie_ObAtuCfg specifies the Outbound ATU configurations for PCIe. More...
 
struct  Pcie_IbAtuCfg
 Pcie_IbAtuCfg specifies the Inbound ATU configurations for PCIe. More...
 
struct  Pcie_RegisterMsiIsrParams
 Pcie_RegisterMsiIsrParams specifies the parameters to register an ISR for MSI. More...
 
struct  Pcie_RegisterMsixIsrParams
 Pcie_RegisterMsixIsrParams specifies the parameters to register an ISR for MSIX. More...
 
struct  Pcie_MsiIsrCtrl
 PCIe MSI Isr control structure. More...
 
struct  Pcie_MsixIsrCtrl
 ISR and arguement list for MSIx. More...
 
struct  Pcie_MsixTblEntry
 PCIe MSIx table entry. More...
 
struct  Pcie_MsixTbl
 
struct  Pcie_Attrs
 PCIe atributes. More...
 
struct  Pcie_Object
 PCIe driver object. More...
 
struct  Pcie_DeviceCfg
 PCIe device configuration. More...
 
struct  Pcie_InitCfg
 PCIe configuration for initalization. More...
 
struct  Pcie_Config
 PCIE global configuration array. More...
 
struct  Pcie_BarCfg
 PCIe BAR configuration info. More...
 
struct  Pcie_IbTransCfg
 Inbound traslation configuration info The Pcie_IbTransCfg is used to configure the Inbound Translation Registers. More...
 
struct  Pcie_AtuRegionParams
 This Structure defines the ATU region parameters. More...
 

Macros

#define PCIE_MAX_PERIPHS   (4U)
 Maximum PCIe devices supported by the driver. More...
 
#define PCIE_MAX_MSI_IRQ   (32U)
 Maximum PCIe MSI interrupts supported. More...
 
#define PCIE_MAX_MSIX_IRQ   (2048U)
 Maxmium number of MSIx interrupts supported. More...
 
#define PCIE_MAX_NUM_IBATU   (6U)
 Maximum number of configurable Inbound ATUs. More...
 

Typedefs

typedef void * Pcie_Handle
 Driver handle returned by Pcie_open() call. More...
 
typedef void(* Pcie_MsiIsr) (void *arg, uint32_t msiData)
 Function pointer for the PCIe MSI ISR. More...
 
typedef void(* Pcie_MsixIsr) (void *arg, uint32_t msixData)
 Function pointer for the PCIe MSIx ISR. More...
 

Enumerations

enum  Pcie_Mode { PCIE_EP_MODE = 0, PCIE_LEGACY_EP_MODE, PCIE_RC_MODE }
 These are the possible values for PCIe mode. More...
 
enum  Pcie_Gen { PCIE_GEN1 = 1, PCIE_GEN2 = 2, PCIE_GEN3 = 3 }
 Enumeration for PCIE generations. More...
 
enum  Pcie_RefClk_Mode {
  PCIE_REFCLK_MODE_INT_NOSSC_OUTDIS = 1, PCIE_REFCLK_MODE_INT_SSC_OUTDIS = 2, PCIE_REFCLK_MODE_INT_NOSSC_OUTEN = 3, PCIE_REFCLK_MODE_INT_SSC_OUTEN = 4,
  PCIE_REFCLK_MODE_EXT_NOSSC = 5, PCIE_REFCLK_MODE_EXT_SSC = 6
}
 Enumeration for PCIe Reference Clock mode. More...
 
enum  Pcie_SRIS_Mode { PCIE_REFCLK_SRIS_DISABLED = 0, PCIE_REFCLK_SRIS_ENABLED = 1 }
 Enumeration for PCIe SRIS mode. More...
 
enum  Pcie_PwrState { PCIE_PWR_STATE_D0 = 0, PCIE_PWR_STATE_D1 = 1, PCIE_PWR_STATE_D3hot = 2 }
 Enumeration for PCIE Power State. More...
 
enum  Pcie_IntPin {
  PCIE_INT_PINNONE = 0, PCIE_INT_PINA = 1, PCIE_INT_PINB = 2, PCIE_INT_PINC = 3,
  PCIE_INT_PIND = 4
}
 Enumeration for PCIE Legacy Interrupt Pin. More...
 
enum  Pcie_BarPref { PCIE_BAR_NON_PREF = 0, PCIE_BAR_PREF }
 These are the possible values for Prefetch BAR configuration. More...
 
enum  Pcie_BarType { PCIE_BAR_TYPE32 = 0, PCIE_BAR_RSVD, PCIE_BAR_TYPE64 }
 These are the possible values for Type BAR configuration. More...
 
enum  Pcie_BarMem { PCIE_BAR_MEM_MEM = 0, PCIE_BAR_MEM_IO }
 These are the possible values for Memory BAR configuration. More...
 
enum  Pcie_AtuRegionDir { PCIE_ATU_REGION_DIR_OUTBOUND, PCIE_ATU_REGION_DIR_INBOUND }
 Enum to select PCIe ATU(Address translation unit) region direction(Inbound or Outbound). This enum is used while configuring inbound or outbound region. More...
 
enum  Pcie_TlpType { PCIE_TLP_TYPE_MEM, PCIE_TLP_TYPE_IO, PCIE_TLP_TYPE_CFG }
 This enum is used to select PCIe TLP(Transaction layer packet) type while configuring inbound or outbound region. More...
 
enum  Pcie_AtuRegionMatchMode { PCIE_ATU_REGION_MATCH_MODE_ADDR, PCIE_ATU_REGION_MATCH_MODE_BAR }
 Enum to select address or BAR match mode. More...
 
enum  Pcie_Location { PCIE_LOCATION_LOCAL, PCIE_LOCATION_REMOTE }
 Enumeration for PCIe access type remote/local. More...
 
enum  Pcie_LtssmState {
  PCIE_LTSSM_DETECT_QUIET =0, PCIE_LTSSM_DETECT_ACT, PCIE_LTSSM_POLL_ACTIVE, PCIE_LTSSM_POLL_COMPLIANCE,
  PCIE_LTSSM_POLL_CONFIG, PCIE_LTSSM_PRE_DETECT_QUIET, PCIE_LTSSM_DETECT_WAIT, PCIE_LTSSM_CFG_LINKWD_START,
  PCIE_LTSSM_CFG_LINKWD_ACEPT, PCIE_LTSSM_CFG_LANENUM_WAIT, PCIE_LTSSM_CFG_LANENUM_ACEPT, PCIE_LTSSM_CFG_COMPLETE,
  PCIE_LTSSM_CFG_IDLE, PCIE_LTSSM_RCVRY_LOCK, PCIE_LTSSM_RCVRY_SPEED, PCIE_LTSSM_RCVRY_RCVRCFG,
  PCIE_LTSSM_RCVRY_IDLE, PCIE_LTSSM_L0, PCIE_LTSSM_L0S, PCIE_LTSSM_L123_SEND_EIDLE,
  PCIE_LTSSM_L1_IDLE, PCIE_LTSSM_L2_IDLE, PCIE_LTSSM_L2_WAKE, PCIE_LTSSM_DISABLED_ENTRY,
  PCIE_LTSSM_DISABLED_IDLE, PCIE_LTSSM_DISABLED, PCIE_LTSSM_LPBK_ENTRY, PCIE_LTSSM_LPBK_ACTIVE,
  PCIE_LTSSM_LPBK_EXIT, PCIE_LTSSM_LPBK_EXIT_TIMEOUT, PCIE_LTSSM_HOT_RESET_ENTRY, PCIE_LTSSM_HOT_RESET,
  PCIE_LTSSM_RCVRY_EQ0, PCIE_LTSSM_RCVRY_EQ1, PCIE_LTSSM_RCVRY_EQ2, PCIE_LTSSM_RCVRY_EQ3
}
 Enumeration for possible values for encoding LTSSM state. More...
 

Functions

void Pcie_init (void)
 This function initializes the PCIe module. More...
 
Pcie_Handle Pcie_open (uint32_t index)
 This function opens a given PCIe peripheral. More...
 
void Pcie_close (Pcie_Handle handle)
 Function to close PCIe peripheral specified by PCIe handle. More...
 
Pcie_DeviceCfgBaseAddr * Pcie_handleGetBases (Pcie_Handle handle)
 Get the device base address info for the PCIe peripheral. More...
 
int32_t Pcie_setInterfaceMode (Pcie_Handle handle, Pcie_Mode mode, Pcie_Gen gen)
 Set interfac mode (RC/EP) More...
 
int32_t Pcie_getMemSpaceReserved (Pcie_Handle handle, uint32_t *resSize)
 Pcie_getMemSpaceReserved returns amount of reserved space between beginning of hardware's data area and the base returned by Pcie_getMemSpaceRange. More...
 
int32_t Pcie_getMemSpaceRange (Pcie_Handle handle, void **base, uint32_t *size)
 Returns the PCIe Internal Address Range for the memory space. This range is used for accessing memory. More...
 
int32_t Pcie_cfgBar (Pcie_Handle handle, const Pcie_BarCfg *barCfg)
 Configure a BAR Register (32 bits) More...
 
int32_t Pcie_atuRegionConfig (Pcie_Handle handle, Pcie_Location location, uint32_t atuRegionIndex, const Pcie_AtuRegionParams *atuRegionParams)
 Configure address translation registers. More...
 
int32_t Pcie_getVendorId (Pcie_Handle handle, Pcie_Location location, uint32_t *vendorId, uint32_t *deviceId)
 Get vendor ID and device ID of Pcie Device. More...
 
int32_t Pcie_getPwrState (Pcie_Handle handle, Pcie_PwrState *pwrState)
 Get current PCIe Power State. More...
 
int32_t Pcie_getLinkParams (Pcie_Handle handle, Pcie_Gen *gen, uint32_t *numLanes)
 Get current PCIe Link Parameter. More...
 
int32_t Pcie_isLinkUp (Pcie_Handle handle)
 Check if PCIe link training completed. More...
 
int32_t Pcie_waitLinkUp (Pcie_Handle handle)
 Wait for PCIe link training to complete. More...
 
int32_t Pcie_checkLinkParams (Pcie_Handle handle)
 Verify if the link parameters is established as configured. More...
 
int32_t Pcie_LtssmCtrl (Pcie_Handle handle, uint8_t enable)
 Enable/disable PCIe link training. More...
 
int32_t Pcie_setLanes (Pcie_Handle handle)
 Set number of PCIe lanes as configured. More...
 
int32_t Pcie_cfgEP (Pcie_Handle handle)
 Configure Pcie for EP (End Point) operation. PCIe mode setting is NOT done here (Pcie_setInterfaceMode) More...
 
int32_t Pcie_cfgRC (Pcie_Handle handle)
 Configure Pcie for RC (Root Complex) operation. PCIe mode setting is NOT done here (Pcie_setInterfaceMode) More...
 
int32_t Pcie_setCfgEn (Pcie_Handle handle, int enable)
 Set CONFIG_ENABLE to signal RC that the local EP configuration is completed. More...
 
int32_t Pcie_setSlotClockCnfg (Pcie_Handle handle, int enable)
 Set slot clock configuration bit in Link Status Register. More...
 
int32_t Pcie_setDwnStrIrq (Pcie_Handle handle, int enable)
 Enable downstream interrupt in PCIE Controller. More...
 
int32_t Pcie_setLnkDwnStateIrq (Pcie_Handle handle, int enable)
 Enable link down status interrupt in PCIE Controller. More...
 
int32_t Pcie_setPwrStateIrq (Pcie_Handle handle, int enable)
 Enable power management state interrupt in PCIE Controller. More...
 
int32_t Pcie_setHotResetIrq (Pcie_Handle handle, int enable)
 Enable hot reset interrupt in PCIE Controller. More...
 
int32_t Pcie_ackDwnStrIrq (Pcie_Handle handle)
 Acknowledge downstream interrupt. More...
 
int32_t Pcie_ackLnkDwnStateIrq (Pcie_Handle handle)
 Acknowledge link down status interrupt. More...
 
int32_t Pcie_ackPwrStateIrq (Pcie_Handle handle)
 Acknowledge power management state interrupt. More...
 

Variables

Pcie_Config gPcieConfig []
 Externally defined driver configuration array. More...
 
uint32_t gPcieConfigNum
 Externally defined driver configuration array size. More...