AM62Px MCU+ SDK  12.00.00
pmic.h File Reference

Go to the source code of this file.

Data Structures

struct  PMIC_Config
 PMIC driver configuration, these are filled by SysCfg based on the device that is selected. More...
 
struct  PMIC_Params
 Parameters passed during PMIC_open() More...
 

Typedefs

typedef void * PMIC_Handle
 Handle to the PMIC driver returned by PMIC_open() More...
 
typedef struct PMIC_Config_s PMIC_Config
 Forward declaration of PMIC_Config. More...
 
typedef struct PMIC_Params_s PMIC_Params
 Forward declaration of PMIC_Params. More...
 

Functions

void PMIC_init (void)
 This function initializes the PMIC module. More...
 
void PMIC_deinit (void)
 This function de-initializes the PMIC module. More...
 
PMIC_Handle PMIC_open (uint32_t instanceId, const PMIC_Params *params)
 Open PMIC driver. More...
 
PMIC_Handle PMIC_getHandle (uint32_t instanceId)
 Get handle to PMIC driver. More...
 
void PMIC_close (PMIC_Handle handle)
 Close PMIC driver. More...
 
void PMIC_critSecStartFn (void)
 Initiates the start of a critical section for PMIC operations. This function attempts to acquire a semaphore, which is typically used to ensure exclusive access to resources during PMIC operations. More...
 
void PMIC_critSecStopFn (void)
 Concludes a critical section for PMIC operations. This function releases the semaphore, signifying the end of a critical section initiated by a corresponding "start" function. More...