AM62Px MCU+ SDK  12.00.00

Detailed Description

Parameters passed during PMIC_open()

Data Fields

uint32_t mainDrvinstance
 
uint32_t qaWdogDrvinstance
 

Field Documentation

◆ mainDrvinstance

uint32_t PMIC_Params::mainDrvinstance

Underlying I2C/MCSPI peripheral driver instance that is used by the PMIC driver

◆ qaWdogDrvinstance

uint32_t PMIC_Params::qaWdogDrvinstance

Underlying I2C peripheral driver instance that is used by the PMIC driver. This is used only when watchdog Q&A mode is enabled via separate I2C.