AM62D FreeRTOS SDK  12.00.00
Release Notes 11.01.00

Attention
Also refer to individual module pages for more details on each feature, unsupported features, important usage guidelines.
Note
The examples will show usage of SW modules and APIs on a specific CPU instance and OS combination.
Unless explicitly noted otherwise, the SW modules would work in both FreeRTOS and no-RTOS environment.

Device and Validation Information

SOC Supported CPUs EVM Host PC
AM62Dx MCU R5F, WKUP R5F, A53, C75 AM62D-EVM EVM (referred to as am62dx-evm in code) Windows 10 64b or Ubuntu 22.04 64b

Features Added in This Release

Feature Module
SBL initiates LBSIT and PSBIST for MCU R5F core before booting MCU R5F now SBL
HS-SE boot support SBL
Hello World CPP example added for A53 and C7x examples
DDR inline ECC suppot DDR
Updated DDR configuration from DDR configuration tool v10.30 DDR
ECC Functional Test example for single bit errors is added SDL

Experimental Features

Attention
Features listed below are early versions and should be considered as "experimental".
Users can evaluate the feature, however the feature is not fully tested at TI side.
TI would not support these feature on public e2e.
Experimental features will be enabled with limited examples and SW modules.
Feature Module
FreeRTOS AMP support on A53. DPL, FreeRTOS
A53 FreeRTOS AMP examples demonstrating usage of ethernet Networking
AUDIOLIB Moudles in AUDIOLIB

Dependent Tools and Compiler Information

Attention
It is recommended to use the TIFS version provided with the release for ensuring compatibility between TIFS and device manager. Using the TIFS from different MCU+SDK release is not recomended and may cause TIFS/ DM functionality to break.
Tools Supported CPUs Version
Code Composer Studio MCU-R5F, C75 20.2.0
SysConfig MCU-R5F, DM-R5F, C75 1.24.0, build 4150
TI ARM CLANG MCU-R5F, WKUP-R5F 4.0.1.LTS
GCC AARCH64 A53 9.2-2019.12
C7000-CGT C75 5.0.0.LTS
FreeRTOS Kernel MCU-R5F, WKUP-R5F, C75, A53 11.1.0

SDK Components

SYSFW / TIFS

Version 11.01.02
Release Notes LINK
User Guide LINK

Key Features

OS Kernel

OS Supported CPUs SysConfig Support
FreeRTOS Kernel MCU-R5F, WKUP-R5F, A53, C75 NA
FreeRTOS POSIX MCU-R5F, A53 NA
FreeRTOS SMP A53 NA
No RTOS MCU-R5F, WKUP-R5F, A53 NA

Driver Porting Layer (DPL)

Module Supported CPUs SysConfig Support OS support
Address Translate MCU-R5F, WKUP-R5F Yes FreeRTOS, NORTOS
Cache MCU-R5F, WKUP-R5F, A53, C75 Yes FreeRTOS, NORTOS
Clock MCU-R5F, WKUP-R5F, A53, C75 Yes FreeRTOS, NORTOS
CycleCounter MCU-R5F, WKUP-R5F, A53, C75 NA FreeRTOS, NORTOS
Debug MCU-R5F, WKUP-R5F, A53, C75 Yes FreeRTOS, NORTOS
Heap MCU-R5F, WKUP-R5F, A53, C75 NA FreeRTOS, NORTOS
Hwi MCU-R5F, WKUP-R5F, A53, C75 Yes FreeRTOS, NORTOS
MPU MCU-R5F, WKUP-R5F, A53, C75 Yes FreeRTOS, NORTOS
Semaphore MCU-R5F, WKUP-R5F, A53, C75 NA FreeRTOS, NORTOS
Task MCU-R5F, WKUP-R5F, A53, C75 NA FreeRTOS
Timer MCU-R5F, WKUP-R5F, A53 Yes FreeRTOS, NORTOS

Secondary Bootloader (SBL)

SBL Mode Supported CPUs SysConfig Support PHY Support DMA Support OS support
OSPI NOR WKUP-R5F Yes No Yes NORTOS
EMMC WKUP-R5F Yes NA NA NORTOS
UART WKUP-R5F Yes NA No NORTOS

Networking

Module Supported CPUs SysConfig Support OS Support Key features tested Key features not tested
TSN R5F NO FreeRTOS gPTP IEEE 802.1 AS-2020 compliant gPTP stack, End Nodes and Bridge mode support, YANG data model configuration, IEEE 1722 compliant AVTP Stack Multi-Clock Domain
LwIP R5F YES FreeRTOS TCP/UDP IP networking stack with and without checksum offload enabled, TCP/UDP IP networking stack with server and client functionality, basic Socket APIs, netconn APIs and raw APIs, DHCP, ping, TCP iperf, scatter-gather, DSCP priority mapping, LwIP bridge, shared memory driver Other LwIP features
Ethernet driver (ENET) R5F YES FreeRTOS Ethernet as port using CPSW, MAC loopback and PHY loopback, Layer 2 MAC, Packet Timestamping, CPSW Switch, Policer and Classifier, MDIO Manual Mode, CBS (IEEE 802.1Qav) on CPSW, IET (IEEE 802.1Qbu) on CPSW, cut through switch on CPSW RMII mode

SOC Device Drivers

Note
See the updated MCASP usage guidelines in MCASP for changes in MCASP driver
Peripheral Domain Supported CPUs SysConfig Support
DDR Main WKUP-R5F Yes
GPIO MCU MCU-R5F Yes
Main A53, C75 Yes
Wakeup WKUP-R5F Yes
I2C MCU MCU-R5F Yes
Main A53, C75 Yes
Wakeup WKUP-R5F Yes
IPC MCU MCU-R5F Yes
Main A53, C75 Yes
Wakeup WKUP-R5F Yes
MCAN MCU MCU-R5F Yes
Maim A53 Yes
MCASP Main A53, C75 Yes
MCSPI Main A53, C75 Yes
MCU MCU-R5F Yes
MMCSD Main A53, C75 Yes
Wakeup WKUP-R5 Yes
OSPI Main A53 Yes
Wakeup WKUP-R5 Yes
Pinmux Main A53, C75 Yes
MCU MCU-R5F Yes
Wakeup WKUP-R5F Yes
SA3UL Main A53 Yes
SOC NA MCU-R5F, WKUP-R5F, A53, C75 Yes
SCIClient NA MCU-R5F, WKUP-R5F, A53, C75 Yes
UART Main A53, C75 Yes
MCU MCU-R5F Yes
Wakeup WKUP-R5F Yes
UDMA Main A53, C75 Yes
MCU MCU-R5F Yes
Wakeup WKUP-R5F Yes
WDT Main A53 Yes
MCU MCU-R5F Yes
Note
Refer Accessing main and wakeup domain peripherals from MCU domain for accessing main/wakeup peripherals from MCU Domain.

Board Device Drivers

Peripheral Supported CPUs SysConfig Support
EEPROM MCU-R5F, A53, C75 Yes
Flash WKUP-R5F, A53 Yes
LED MCU-R5F, A53, C75 Yes

SDL

SDL Module Supported CPUs SysConfig Support
MCRC MCU-R5F No
ESM MCU-R5F No
VTM MCU-R5F No
DCC MCU-R5F No
ECC MCU-R5F No
RTI MCU-R5F No
POK MCU-R5F No
STOG MCU-R5F No
MTOG MCU-R5F No
PBIST MCU-R5F No
LBIST MCU-R5F No
ROM_CHECKSUM MCU-R5F No

Fixed Issues

ID Head Line Module Applicable Releases
EXT_EP-12267 AM62D: MCRC Udma Init failure in semi cpu and auto mode configuration - MCRC semi cpu and auto mode examples fail at udma init step SDL 11.01.00
EXT_EP-12721 ECC TCM example cannot be built for AM62D SDL 11.01.00
EXT_SITMPUSW-98 Audio playback stops on applying breakpoint during CCS debugging McASP 11.00.00
EXT_SITMPUSW-101 Not able to import example projects in CCS v20 Build 11.00.00
EXT_SITMPUSW-104 Missing $Board to build HSMAppImageGen in /mcu_plus_sdk/am62dx/imports.mak Build 11.00.00
EXT_SITMPUSW-105 MMCSD driver uses snprintf function from libc MMCSD 11.00.00
EXT_SITMPUSW-77 Modify Read capture delay logic for Tap Mode OSPI 11.00.00
EXT_SITMPUSW-106 OSPI Phy Tuning Data is not written correctly in Flash_norOspiOpen() OSPI 10.01.00

Known Issues

ID Head Line Module Reported in release Workaround
EXT_SITMPUSW-108 freeRTOS/C7x - Task Size is very big FreeRTOS 11.00.00 No known workaround
EXT_SITMPUSW-109 Wrong comments on HwiP_inISR() API DPL 11.00.00 No known workaround
EXT_SITMPUSW-78 MMCSD Sysconfig provides options to configure PHY type MMCSD 11.00.00 No known workaround
EXT_SITMPUSW-84 MMCSD error recovery sequence isn't implemented correctly MMCSD 11.00.00 No known workaround
EXT_SITMPUSW-110 eMMC Init Code Missing DLL Register Settings needed for Initial Legacy SDR Mode Phase MMCSD 11.00.00 No known workaround
EXT_SITMPUSW-113 eMMC PHY I/O Calibration not getting executed during eMMC boot MMCSD 11.00.00 No known workaround
EXT_SITMPUSW-114 MMCSD_enableBootPartition implements two mutually exclusive concepts as one function MMCSD 11.00.00 No known workaround
EXT_SITMPUSW-123 MMCSD driver does not follow the SWITCH command sequence correctly MMCSD 11.00.00 No known workaround
EXT_SITMPUSW-124 EXTCSD HS_TIMING register is set incorrectly at certain places in the driver MMCSD 11.00.00 No known workaround
EXT_SITMPUSW-125 MMCSD driver uses infinite loop instead of timeout for checking fields of PRESENTSTATE register MMCSD 11.00.00 No known workaround
EXT_SITMPUSW-126 Timing issues with MMCSD host controller driver MMCSD 11.00.00 No known workaround
EXT_SITMPUSW-128 EMMC timiing parameters to be changed based on SOC and MMC instance MMCSD 11.00.00 No known workaround
EXT_SITMPUSW-120 C7x task size/alignment should be 8KB (not 16KB) FreeRTOS 11.00.00 Change the stack alignment
EXT_SITMPUSW-121 FORCE bit not book keeped properly for MCSPI DMA mode of operation MCSPI 11.00.00 No known workaround
EXT_EP-12276 ECC: Firewall related aggregators failures - ECC Aggregators SDL_SMS0_SMS_TIFS_ECC, SDL_SMS0_SMS_HSM_ECC, SDL_SA3_SS0_SA3SS_AM62A_DMSS_ECCAGGR and SDL_SA3_SS0_SA3SS_AM62A_SA_UL_ECC_AGGR fail because of firewall access issues faced by SDL SDL 10.01.00 No known workaround
EXT_EP-12283 ECC aggregators CPSW0, CSI RX are failing on AM62A and CPSW0 on AM62D. SDL 09.00.00 No known workaround
EXT_EP-12280 Running MCU LBIST on SBL causes JTAG connection issues to MCU R5F SDL 09.00.00 No known workaround

Limitations

S.No Head Line Module
1 The ROM startup model for runtime initializations in TI ARM CLANG is not supported/tested in the SDK NA

Upgrade and Compatibility Information

This section lists changes which could affect user applications developed using older SDK versions. Read this carefully to see if you need to do any changes in your existing application when migrating to this SDK version relative to previous SDK version. Also refer to older SDK version release notes to see changes in earlier SDKs.

The below table captures the list of migration document sections when migrating from one version to another. The migration for a partcluar module will be applicable, if you are migrating from older version listed to newer version listed on the table below.

Module Migration guide Older version Newer version
Bootloader Bootloader Migration Guidelines<= 10.01.00 >= 11.00.00
NETWORKING Version Updates from earlier SDKs to Latest11.00.00 >= 11.01.00

Networking

Module Affected API Change
TSN notify_linkchange notify_linkchange function is renamed to cb_lld_notify_linkchange, include path <tsn_combase/tilld/cb_lld_ethernet.h> in the file that uses cb_lld_notify_linkchange.