The Multi Channel Audio Seiral Peripheral (MCASP) driver is a generic, full-duplex driver that transmits and receives data using the MCASP interface. This is specially designed to transmit and receive the digital audio data.
Features Supported
- Interrupt mode operation
- DMA mode operation
- Internal Loopback
- Transmit and Receive in TDM format with multi-serializer, multi-slot support.
- SysConfig support for driver parameter configuration and initialization.
- Different audio buffer formats for application
SysConfig Features
- Attention
- The instances for McASP needs to be selected the same for serializers for the instance. Syscfg will automatically assign different instances for all and user will be required to assign same instance and choose to ignore the warning.
- Note
- It is strongly recommend to use SysConfig where it is available instead of using direct SW API calls. This will help simplify the SW application and also catch common mistakes early in the development cycle.
Features NOT Supported
- Transmit in DIT mode
- Burst Mode
Usage Overview
Key Careabouts in Driver Usage
- Note
- The changes pulled in for the driver starting release 10.0 requires some changes in the Driver usage from application
- All transactions submitted from the applications must be of the same size.
- The TX and RX can be of seperate size.
- The Loopjob buffer size can be configured from the sysconfig.
- Application can provide an external buffer for loopjob buffer from Sysconfig
- This enables application to provide the transaction buffer itself as loopjob
- MCASP_stopTransferRx() and MCASP_stopTransferTx() are blocking calls that should not be called from an ISR context.
API Sequence
To use the MCASP driver to send data over the MCASP interface, the application calls the following APIs:
MCASP migration guide 11.02 to 12.00
- Note
- This section highlights key features that have changed or got added from 11.02 to 12.00 SDK.
-
Different Audio Buffer Formats feature was added.
-
For multi-serializer RX/TX, you should select multi-serializer audio buffer formats only.
Supported Application Audio Buffer Formats
The McASP driver provides various buffer formats for sending the data to/from the audio device. The differences between these formats arise from the way the audio samples are collected from various serializers and their timeslots and arranged in the system’s memory. This way the application can choose to run audio processing algorithms over the data without the need for re-arranging those data every frame. This section provides an overview of the various formats . In the explanatory diagrams in each section, McASP controller recieves samples in frame intervals denoted by t1,t2..tn. The McASP driver collects these and arranges those samples in the memory in various formats in to the host’s System memory. We have chosen 32 bit samples and 32-bit word addresses throughout for simplicity.
- 1-Serializer Multi-Slot Interleaved: This is applicable if multiple slots are used with one serializer. The samples from the different timeslots are stored interleaved in the memory as below. Different timeslots’ samples are denoted by different colors and are labelled t1,t2..tn according to the time they arrive at the serializer.
mcasp_buff_format_1serMultiSlotInterleaved Block Diagram
- 1-Serializer Multi-Slot NonInterleaved: This is applicable if multiple slots are used with one serializer. The samples from the different timeslots are grouped together on the basis of the timeslot and stored in the memory as shown below. Different timeslots’ samples are denoted by different colors and are labelled t1,t2..tn according to the time they arrive at the serializer.
mcasp_buff_format_1serMultiSlotNonInterleaved Block Diagram
- Multi-Serializer Multi-Slot Interleaved Type1: This is applicable if multiple serializers are used and each serializer containing multiple timeslots. The samples are stored in the memory interleaved based on serializer and timeslots as shown below. In this example, there are 3 serializers and 2 timeslots per serializers whose samples are noted by Ln (left) and Rn (right). Different serializers’ samples are denoted by different colors.
mcasp buff format MultiSerMultiSlotType1 Block Diagram
- Multi-Serializer Multi-Slot Interleaved Type2: This is applicable if multiple serializers are used and each serializer containing multiple timeslots. The samples are grouped based on the serializer and within one serializer, the timeslots are interleaved as shown below. In this example, there are 3 serializers and 2 timeslots per serializers whose samples are noted by Ln (left) and Rn (right).Different serializers’ samples are denoted by different colors.
mcasp buff format MultiSerMultiSlotType2 Block Diagram
- Multi-Serializer Multi-Slot NonInterleaved: This is applicable if multiple serializers are used and each serializer containing multiple timeslots. The samples are grouped based on the serializer and slot within one serializer, the timeslots are interleaved as shown below. In this example, there are 3 serializers and 2 timeslots per serializers whose samples are noted by Ln (left) and Rn (right).Different serializers’ samples are denoted by different colors.
mcasp buff format NonInterleaved Block Diagram
Loopjob Configuration
Mcasp driver allows loopjob enabled/disabled configuration to handle delayed application buffer submission at run time. Loopjob is a default buffer that gets transmitted / received into if the application fails to submit the buffers in time. When loopjob is disabled the last 2 application buffers will be re programmed and re used. The application callback corresponding to the re programmed buffers is not called.
- Loopjob buffer is programmed in sys config. Sys config will define a uint8_t array and initialize it to 0.
- Application can access the buffer and optionally initialize the data.
- If the loopjob buffer is programmed, after sending the full loopjob buffer next submitted buffer is programmed.
Buffer Queuing
- The application buffers need to be programmed before starting the transfer.
- If the loopjob is enabled application can start without queuing any buffers, Driver will work with the loopjob buffers till application queues the actual buffers.
- If loopjob is disabled at least 2 buffers should be queued before starting the mcasp transfer. New buffer will be programmed in the interrupt callback corresponding to current transfer. the application is expected to submit the new buffer before that else the same buffer is re programmed, so it is recommended to start the transfer with at least 3 buffers queued.
Example Usage
Include the below file to access the APIs
Instance Open Example
mcaspParams.edmaInst = 0;
mcaspParams.edmaInst = CONFIG_EDMA0,
gMcaspHandle =
MCASP_open(CONFIG_MCASP0, &mcaspParams);
Instance Close Example
Start McASP Transfer Example
uint8_t mcaspTxBuffer[APP_MCASP_MSG_COUNT][APP_MCASP_MSGSIZE];
uint8_t mcaspRxBuffer[APP_MCASP_MSG_COUNT][APP_MCASP_MSGSIZE];
uint32_t i;
for (i = 0U; i < APP_MCASP_MSG_COUNT; i++)
{
txnTx[i].
buf = (
void*) &mcaspTxBuffer[i][0];
txnTx[i].
count = APP_MCASP_MSGSIZE/4;
}
for (i = 0U; i < APP_MCASP_MSG_COUNT; i++)
{
txnRx[i].
buf = (
void*) &mcaspRxBuffer[i][0];
txnRx[i].
count = APP_MCASP_MSGSIZE/4;
}
Stop McASP Transfer Example
{
do {
}while (transaction != NULL);
do {
}while (transaction != NULL);
}
SysConfig migration guide 11.01 to 11.02
- Note
- This section highlights key features that have changed or got added from 11.01 to 11.02 SDK
AUX clock selection
- This version of SDK (11.02) gives the configurability to choose between different sources of AUXCLK
MCASP AUX Clock selection
- The specific option for AUXCLK will vary from device to device. View long description in Syscfg view for more details on the AUXCLK options to select from.
- The frequency for the configurable AUX clock options can be choosen at a global level as this will be applicable across all instances of MCASP.
MCASP AUX Clock Frequency Configuration
- Some option in the AUX clock selections might expect the aux clock to be supplied externally to the SoC. Refer the TRM of the specific device to check if the clock is supplied externally or generated interally.
- When using an internally generated auxiliary clock source, not all frequency values are achievable due to hardware limitations. If the user-specified frequency cannot be generated, the system will throw a runtime error.
Clock Divider Configurability
- This version of SDK (11.02) gives configurability of the High Clock Divider (HCLK Divider), and the BCLK divider.
MCASP Clock Divider Configuration
- The "Re-Calculate" button can be used to calculate the divider values that would result in the closest FSYNC value required.
- The "Apply" button needs to be pressed to view the frequencies for any change in the Sysconfig GUI that have resulted in a change of frequencies.
- Press the "Apply" button to update the frequency information displayed in the Syscfg GUI for all configuration parameters that affect frequency settings.
- User have to ensure all the frequencies that is displayed is as expected in the system after pressing "Apply".
- User can adjust the Divider values and press the "Apply" button to achieve any specific clock frequencies.
API
APIs for MCASP