AM62D FreeRTOS SDK  12.00.00
Version Updates from earlier SDKs to Latest

While upgrading from 11.01 or earlier to latest SDK

Change Set

Change-1: Sysconfig generated file changes
Change-2: Enet Module interface removed

Change-1 Description

Enet-LLD sysconfig layer has been cleaned up to improve code readability by removing sysconfig API abstractions and statically initializing CPSW/ICSSG configurations and calling driver APIs directly.

The following new files are generated from sysconfig. Example makefiles have been updated to include these files:

Generated File Description
ti_enet_dma_init.h Contains DMA structures and API definitions
ti_enet_dma_init.c Contains DMA object initialization based on the DMA channel config settings in Sysconfig GUI
ti_enet_init.c Contains global CPSW config and RM resource config initialization along with helper functions:
- Global RM resource config is populated from an array defined in device specific .js files
- Global CPSW config is populated from the Sysconfig GUI settings

The following APIs have been removed from syscfg generated files:

Removed API Description
EnetApp_enablePorts() Replaced by separate host/mac functions
EnetApp_openDmaChannels() Inlined into main flow
EnetApp_openAllRxDmaChannels() Inlined into main flow
EnetApp_openAllTxDmaChannels() Inlined into main flow
EnetApp_doCpswOpen() No longer needed, replaced with direct call to Enet_open()
EnetAppUtils_initResourceConfig() Replaced with static config

The following APIs have been added in syscfg generated files:

New API Description
EnetApp_enableHostPort() Separate host port enable
EnetApp_enableMacPort() Separate MAC port enable
EnetApp_getPhyAliveStatus() Direct PHY status check
EnetApp_updateTxChInitCfg() Direct TX channel config update
EnetApp_updateRxChInitCfg() Direct RX channel config update
EnetApp_getCpswCfg() Returns static CPSW config pointer
EnetApp_cpswInitMacAddr() Static MAC address init
getAleModeFlags(), getAlePortMask() Template helper functions
getIpNxtWhitelistCount(), getIpNxtWhitelistCount() Template helper functions

Change-1 Impact

  • All networking examples now generate additional files that are included in makefiles - ti_enet_dma_init.c/h and ti_enet_init.c.
  • Enet driver initialization has been internally refactored to reduce abstraction. Users need to rebuild their projects to get the modified template changes.

Change-2 Description

Enet module abstraction layer has been removed to meet functional safety standards by replacing generic EnetMod_Handle with specific typed handles (e.g., CpswAle_Handle, Mdio_Handle), eliminating function pointers and void pointers.

  • The void *arg argument used in the function pointer of EnetPhy_Mdio structure has been changed to Mdio_Obj*
  • The EnetMod_Obj enetMod member in all module structures has been removed and its individual members have been expanded inline
  • Module APIs now use module-specific handles instead of the generic EnetMod_Handle as below:
Module Impacted APIs Old parameters New parameters
CPSW ALE CpswAle_open, CpswAle_rejoin, CpswAle_ioctl, CpswAle_close,
CpswAle_saveCtxt, CpswAle_restoreCtxt
EnetMod_Handle hMod, ... CpswAle_Handle hAle, ...
CPSW CPTS CpswCpts_open, CpswCpts_rejoin, CpswCpts_ioctl,
CpswCpts_close, CpswCpts_saveCtxt, CpswCpts_restoreCtxt
EnetMod_Handle hMod, ... CpswCpts_Handle hCpts, ...
CPSW HostPort CpswHostPort_open, CpswHostPort_rejoin, CpswHostPort_ioctl,
CpswHostPort_close, CpswHostPort_saveCtxt, CpswHostPort_restoreCtxt
EnetMod_Handle hMod, ... CpswHostPort_Handle hPort, ...
CPSW MacPort CpswMacPort_open, CpswMacPort_rejoin, CpswMacPort_ioctl,
CpswMacPort_close, CpswMacPort_saveCtxt, CpswMacPort_restoreCtxt
EnetMod_Handle hMod, ... CpswMacPort_Handle hPort, ...
CPSW Stats CpswStats_open, CpswStats_rejoin, CpswStats_ioctl,
CpswStats_close, CpswStats_saveCtxt, CpswStats_restoreCtxt
EnetMod_Handle hMod, ... CpswStats_Handle hStats, ...
MDIO Mdio_open, Mdio_rejoin, Mdio_ioctl, Mdio_close, Mdio_saveCtxt, Mdio_restoreCtxt EnetMod_Handle hMod, ... Mdio_Handle hMdio, ...
ICSSG Stats IcssgStats_open, IcssgStats_rejoin, IcssgStats_ioctl, IcssgStats_close EnetMod_Handle hMod, ... IcssgStats_Handle hStats, ...
ICSSG TAS IcssgTas_open, IcssgTas_rejoin, IcssgTas_ioctl, IcssgTas_close EnetMod_Handle hMod, ... IcssgTas_Handle hTas, ...
ICSSG TimeSync IcssgTimeSync_open, IcssgTimeSync_rejoin, IcssgTimeSync_ioctl, IcssgTimeSync_close EnetMod_Handle hMod, ... IcssgTimeSync_Handle hTimeSync, ...
NullMod NullMod_open EnetMod_Handle hMod, ... , const void *cfg NullMod_Handle hNull, ... , const NullMod_Cfg *nullModCfg
NullMod_rejoin, NullMod_ioctl, NullMod_close EnetMod_Handle hMod, ... NullMod_Handle hNull, ...
EnetPhyMdioDflt EnetPhyMdioDflt_isAlive, EnetPhyMdioDflt_isLinked, EnetPhyMdioDflt_readC22,
EnetPhyMdioDflt_writeC22, EnetPhyMdioDflt_readC45, EnetPhyMdioDflt_writeC45
..., void *args ..., Mdio_Obj *hMdio
EnetPhy EnetPhy_open ..., void *mdioArgs ..., Mdio_Obj *mdioArgs

Change-2 Impact

  1. All code using EnetMod_Handle has been replaced with module specific handle type (e.g., CpswAle_Handle, Mdio_Handle)
  2. All code using the ENET_MOD() macro has been removed
  3. All generic wrapper calls for module IOCTLs have been replaced with module-specific functions
  4. PHY code that passes void* pointers has been updated to use Mdio_Obj* instead

While upgrading from 11.00 SDK to 11.01 SDK

Change Set

Change-1 : ENET UDMA API changes

Change-1 Description

The ENET UDMA API has undergone some changes, with the primary goal of enhancing overall code quality and adhering to functional safety standards. These changes aim to minimize the use of error-prone constructs and eliminate the utilization of void pointers.

Old API Header New API Header
1. Initialize RX channel open parameters: EnetDma_initRxChParams(void *pRxChCfg) EnetUdma_initRxFlowParams(EnetUdma_OpenRxFlowPrms *pRxFlowPrms)
2. Enet DMA open RX channel: EnetDma_openRxCh(EnetDma_Handle hDma, const void *pRxChCfg) EnetUdma_openRxFlow(EnetDma_Handle hDma,const EnetUdma_OpenRxFlowPrms *pRxFlowPrms)
3. Enet DMA close RX channel: EnetDma_closeRxCh(EnetDma_RxChHandle hRxCh, EnetDma_PktQ *fq, EnetDma_PktQ *cq) EnetUdma_closeRxFlow(EnetDma_RxChHandle hRxCh,EnetDma_PktQ *fq,EnetDma_PktQ *cq)
4. Initialize TX channel open parameters: EnetDma_initTxChParams(void *pTxChCfg) EnetUdma_initTxChParams(EnetUdma_OpenTxChPrms *pTxChPrms)
5. Enet DMA open TX channel: EnetDma_openTxCh(EnetDma_Handle hDma, const void *pTxChCfg) EnetUdma_openTxCh(EnetDma_Handle hDma, const EnetUdma_OpenTxChPrms *pTxChPrms)
6. Enet DMA close TX channel: EnetDma_closeTxCh(EnetDma_TxChHandle hTxCh, EnetDma_PktQ *fq, EnetDma_PktQ *cq) EnetUdma_closeTxCh(EnetDma_TxChHandle hTxCh, EnetDma_PktQ *fq, EnetDma_PktQ *cq)

While upgrading from 10.00 SDK

Change Set

Change-1 : ENET(CPSW) and ENET(ICSS) pinmux configuration.
Change-2 : Support to configure link parameters in Sysconfig GUI tool.
Change-3 : ENET(CPSW) and ENET(ICSS) Example paths have been changed.
Change-4 : Support to add and configure Ethernet PHY module through sysconfig-GUI tool.

Change-1 Description

In MCU+ SDK version of 10.01, ENET(CPSW) and ENET(ICSS) related examples showcasing various features have been moved from ${MCU_PLUS_SDK_PATH}/examples/networking to ${MCU_PLUS_SDK_PATH}/source/networking/enet/core/examples

Change-1 Impact

The above change makes older build commands to build Networking examples no longer supported, and it has to be updated with correct path.

Change-1 Solution

Please use "make help DEVICE=<dev_name>" to get the correct location and build commands for the examples.

Note
For Windows , please use "gmake" instead of "make"

Change-2 Description

In MCU+ SDK version of 10.01, support to add custom PHY and configure it through sysconfig tool has been added, and this needs updates in corresponding example.syscfg file to be compatible with latest changes

Change-2 Impact

This will need addition of the corresponding sysconfig tool changes to add the ethernet phy module and configure it.

Change-2 Solution

While upgrading from 09.02 SDK or earlier

Change-1 Description

In MCU+ SDK version of 10.00, ENET(CPSW) and ENET(ICSS) component in Sysconfig GUI has been updated with fixes to correct MII/RMII mode for ICSSG and CPSW Resp.. Additionally support added to release unused pins based on number of ports were enabled in CPSW.

Change-1 Impact

The above described change makes any older 'example.syscfg' generated using SDK version of 09.00 or earlier not compatible with SDK version 10.00 or later. This incompatibility is seen only when either ENET(CPSW) or ENET(ICSS) is added in your application/example.If neither of the components are added, you may ignore this change and there is no impact. User will see the error in sysconfig gui tool when the old example.syscfg file is opened in updated version of mcu plus sdk.

Change-1 Solution

Option 1:

If it is possible to create an example.syscfg as per user configurations, please generate a new example.syscfg from any SDK example and change the configration as per your need. This is the safest option.

Option 2:

Sometimes, it is not easy to get a new example.syscfg that matches the older example.syscfg. In those case, please follow the below steps

  • Open example.syscfg file in any text editor (avoid notepad or word)
  • Find and replace 'enet_cpsw1.pinmux[0].$name = "ENET_CPSW_PINMUX0";' with 'enet_cpsw1.$name = "CONFIG_ENET_CPSW0";'
  • Find and replace 'enet_cpsw1.pinmux[0].' with 'enet_cpsw1.' (note '.' at the end of the strings)
  • Find and replace 'enet_cpsw1.macport1LoopbackEn = true;' with 'enet_cpsw1.macport1LoopbackMode = "LOOPBACK_MODE_MAC";'

Save the modifications. Then open sysconfig GUI tool with the modifications, save and close the tool.

Change-2 Description

In MCU+ SDK version of 10.00, parameters that configures link capabilities for auto negotiation such as speed and duplexity is added into syscfg GUI.

Change-2 Impact

'EnetApp_initLinkArgs' function that is defined in the user applicaiton code is no longer called. Instead, a new function EnetApp_initLinkArgs is defined.

Change-2 Solution

  • User shall open delete their locally defined 'EnetApp_initLinkArgs' and instead let sysconfig tool handle it via generated code.
  • For CPSW users: open sysconfig gui tool and navigate to ENET(CPSW)->MACPORT configuration-> Mac Port 1/2 . Set the link speed capbility and link duplexity capability here. Keep both as Auto to use the default settings.
  • For ICSSG user: open sysconfig gui tool and navigate to ENET(ICSSG) and configure link speed capabilities and link duplexity capabilities as your user configuration. Keep it as Auto to use the default settings.