AM275 FreeRTOS SDK  12.00.00
hyperRam.h File Reference

Introduction

This file contains structure, typedefs, functions and prototypes used for Hyperram.

Go to the source code of this file.

Data Structures

struct  HyperRam_Attrs
 HyperRam device attributes, these are filled by SysCfg based on the HyperRam device that is selected. More...
 
struct  HyperRam_Config
 HyperRam driver configuration, these are filled by SysCfg based on the HyperRam device that is selected. More...
 
struct  HyperRam_Object
 

Typedefs

typedef void * HYPERRAM_Handle
 Handle to the HYPERRAM driver returned by HyperRam_open() More...
 

Functions

void HyperRam_init (void)
 This function initializes the HYPERBUS module. More...
 
void HyperRam_deinit (void)
 This function de-initializes the HYPERBUS module. More...
 
HYPERRAM_Handle HyperRam_open (uint32_t instanceId)
 Open HyperRam driver. More...
 
void HyperRam_close (HYPERRAM_Handle handle)
 Close HyperRam driver. More...