AM275 FreeRTOS SDK  12.00.00
HyperRam_Object Struct Reference

Data Fields

HYPERRAM_Handle handle
 
HYPERBUS_Handle hyperbusHandle
 
uint32_t isOpen
 
SemaphoreP_Object lockObj
 

Field Documentation

◆ handle

HYPERRAM_Handle HyperRam_Object::handle

Instance handle

◆ hyperbusHandle

HYPERBUS_Handle HyperRam_Object::hyperbusHandle

Handle of the underlying HyperBus instance

◆ isOpen

uint32_t HyperRam_Object::isOpen

Flag to indicate if the instance is already open

◆ lockObj

SemaphoreP_Object HyperRam_Object::lockObj

Transfer Sync Semaphore object