AM275 FreeRTOS SDK  12.00.00

Introduction

This module contains APIs to program and use the HyperRAM module on the board . See HyperRam for more details.

Data Structures

struct  HyperRam_Attrs
 HyperRam device attributes, these are filled by SysCfg based on the HyperRam device that is selected. More...
 
struct  HyperRam_Config
 HyperRam driver configuration, these are filled by SysCfg based on the HyperRam device that is selected. More...
 

Functions

void HyperRam_init (void)
 This function initializes the HYPERBUS module. More...
 
void HyperRam_deinit (void)
 This function de-initializes the HYPERBUS module. More...
 
HYPERRAM_Handle HyperRam_open (uint32_t instanceId)
 Open HyperRam driver. More...
 
void HyperRam_close (HYPERRAM_Handle handle)
 Close HyperRam driver. More...
 

Typedefs

typedef void * HYPERRAM_Handle
 Handle to the HYPERRAM driver returned by HyperRam_open() More...
 

Typedef Documentation

◆ HYPERRAM_Handle

typedef void* HYPERRAM_Handle

Handle to the HYPERRAM driver returned by HyperRam_open()

Function Documentation

◆ HyperRam_init()

void HyperRam_init ( void  )

This function initializes the HYPERBUS module.

◆ HyperRam_deinit()

void HyperRam_deinit ( void  )

This function de-initializes the HYPERBUS module.

◆ HyperRam_open()

HYPERRAM_Handle HyperRam_open ( uint32_t  instanceId)

Open HyperRam driver.

Make sure the SOC peripheral driver is opened before calling this API. Drivers_open function generated by SysCfg opens the underlying SOC peripheral driver, e.g HYPERBUS.

Internally this API also reads the device and manufacture ID and checks if it matches the expected value for the HYPERRAM device, if there is mismatch then NULL is returned.

Global variables HYPERRAM_Config gHyperRamConfig[] and uint32_t gHyperRamConfigNum is instantiated by SysCfg to describe the HYPERRAM configuration based on user selection in SysCfg.

Parameters
instanceId[in] Index within HyperRam_Config gHyperRamConfig[] denoting the HyperRam driver to open
Returns
Handle to HyperRam driver which should be used in subsequent API call
NULL in case of failure

◆ HyperRam_close()

void HyperRam_close ( HYPERRAM_Handle  handle)

Close HyperRam driver.

Parameters
handle[in] HyperRam driver handle from HyperRam_open