AM275 FreeRTOS SDK  12.00.00

Introduction

AASRC transactions, transfer objects and parameters.

Go to the source code of this file.

Data Structures

struct  AASRC_Transaction
 Data structure used with transfer call. More...
 
struct  AASRC_TransferObj
 AASRC Transfer Data structure stored in Channel object. More...
 

Macros

#define AASRC_MAX_TXN_WORD_COUNT   (1024U*1024U*512U)
 
#define AASRC_WORD_SIZE_IN_BYTES   (4U)
 
#define AASRC_WORD_SIZE_IN_BITS   (32U)
 
Transfer Status Code

Status codes that are set by the AASRC driver

#define AASRC_TRANSFER_STATUS_QUEUED   (0U)
 I/O buffer queued and pending. More...
 
#define AASRC_TRANSFER_STATUS_LOADED   (1U)
 I/O buffer fetched from queue, waiting for interrupt to fire. More...
 
#define AASRC_TRANSFER_STATUS_STARTED   (2U)
 I/O started processing. More...
 
#define AASRC_TRANSFER_STATUS_COMPLETED   (3U)
 I/O completed successfully. More...
 
#define AASRC_TRANSFER_STATUS_CANCELLED   (4U)
 I/O cancelled. Returned by incomplete read or write requests. More...
 
#define AASRC_TRANSFER_STATUS_FAILED   (5U)
 Generic failure condition. More...
 
#define AASRC_TRANSFER_STATUS_ERROR   (6U)
 ASRC channel has gone into an error. More...
 
#define AASRC_TRANSFER_STATUS_TIMEOUT   (7U)
 I/O timeout occurred. More...
 
AASRC Transfer Mode

#define AASRC_TRANSFER_MODE_INTERRUPT   (0U)
 AASRC read/write APIs does not block code execution and will call a AASRC_TxnCallbackFxn This mode can be used in a Task, Swi, or Hwi context. More...
 
#define AASRC_TRANSFER_MODE_DMA   (1U)
 AASRC read/write APIs does not block code execution and will use DMA for transfers. More...
 

Typedefs

typedef void(* AASRC_TxnCallbackFxn) (AASRC_ChHandle chHandle, AASRC_Transaction *transaction)
 The definition of a callback function used by the AASRC driver when used in Callback Mode. More...
 
typedef void(* AASRC_ChErrorCallbackFxn) (AASRC_ChHandle chHandle, AASRC_Transaction *transactionRx, AASRC_Transaction *transactionTx)
 The definition of a channel error callback function used by the AASRC driver when used in Callback Mode. More...
 

Functions

int32_t AASRC_queueTransactionRx (AASRC_ChHandle chHandle, AASRC_Transaction *transaction)
 Function submit transactions to AASRC input queue. More...
 
int32_t AASRC_queueTransactionTx (AASRC_ChHandle chHandle, AASRC_Transaction *transaction)
 Function submit transactions to AASRC output queue. More...