AM275 FreeRTOS SDK  12.00.00

Detailed Description

Data structure used with transfer call.

Data Fields

QueueP_Elem qElem
 
void * buf
 
uint32_t sampleCount
 
int32_t status
 
void * args
 

Field Documentation

◆ qElem

QueueP_Elem AASRC_Transaction::qElem

[IN] This should be the first parameter. this is the queue element used by driver.

◆ buf

void* AASRC_Transaction::buf

[IN] void * to a buffer with data to be transferred . This parameter can't be NULL

◆ sampleCount

uint32_t AASRC_Transaction::sampleCount

[IN/OUT] Number of sample words for this transaction. This is input incase of read/write call and on API return this represents number of sample words actually read by the API

◆ status

int32_t AASRC_Transaction::status

◆ args

void* AASRC_Transaction::args

[IN] Argument to be passed to the callback function