Enet RM IOCTL permission table.
This structure has the information about IOCTL permissions for all IOCTL commands.
Data Fields | |
| uint32_t | defaultPermittedCoreMask |
| uint32_t | numEntries |
| EnetRm_IoctlPermissionEntry | entry [ENET_RM_NUM_IOCTL_PERM_ENTRY_MAX] |
| uint32_t EnetRm_IoctlPermissionTable::defaultPermittedCoreMask |
Permitted core mask if IOCTL command not found in explicit permission entry table
| uint32_t EnetRm_IoctlPermissionTable::numEntries |
Number of explicit permission entry
| EnetRm_IoctlPermissionEntry EnetRm_IoctlPermissionTable::entry[ENET_RM_NUM_IOCTL_PERM_ENTRY_MAX] |
Permission table entries. Must have numEntries valid entries