Enet RM IOCTL permission entry.
This structure has the information about IOCTL permissions for each IOCTL command.
Data Fields | |
| uint32_t | cmd |
| uint32_t | permittedCoreMask |
| uint32_t EnetRm_IoctlPermissionEntry::cmd |
IOCTL command
| uint32_t EnetRm_IoctlPermissionEntry::permittedCoreMask |
Cores from which this IOCTL call is allowed. This is a bitmask of allowed coreIds