Go to the source code of this file.
Macros | |
#define | SDL_ESM_INSTANCE_MSS (SDL_ESMG1_CCMR5_ST_ERR) |
#define | SDL_MSS_CCMR 0U |
#define | SDL_CCM_MAX_INSTANCE 1U |
Typedefs | |
typedef uint32_t | SDL_CCM_Inst |
CCM Instance supported. More... | |
Variables | |
static uint32_t | SDL_CCM_baseAddress [SDL_CCM_MAX_INSTANCE] |
This API is used to get the base address of the instance. More... | |