The SDL CCM module provides API for CCM Diagnostics
Sub Modules | |
CCM API | |
CCM Low-Level API | |
Typedefs | |
typedef uint32_t | SDL_CCM_Inst |
CCM Instance supported. More... | |
Macros | |
#define | SDL_ESM_INSTANCE_MSS (SDL_ESMG1_CCMR5_ST_ERR) |
#define | SDL_MSS_CCMR 0U |
#define | SDL_CCM_MAX_INSTANCE 1U |
#define SDL_ESM_INSTANCE_MSS (SDL_ESMG1_CCMR5_ST_ERR) |
#define SDL_MSS_CCMR 0U |
CCM INSTANCE
#define SDL_CCM_MAX_INSTANCE 1U |
Maximum
typedef uint32_t SDL_CCM_Inst |
CCM Instance supported.
|
static |
This API is used to get the base address of the instance.