This module contains APIs to program and use the MCASP module. The APIs can be used by other drivers to get access to MCASP and also by application to initiate data transfer operation.
|
#define | MCASP_GBLCTL_TIMEOUT (30000U) |
| The time to try (in Msec) before the GBLCTL register setting timeouts if the setting/resetting is done in a context other than a task this will be used as a retry count rather than the MSec timeout. More...
|
|
#define | MCASP_RESET ((uint32_t) 0x00U) |
| McASP macros for enable/reset. More...
|
|
#define | MCASP_ENABLE ((uint32_t) 0x01U) |
|
#define | MCASP_DISABLE ((uint32_t) 0x00U) |
|
#define | MCASP_REG_OFFSET ((uint32_t)0x4U) |
|
◆ MCASP_GBLCTL_TIMEOUT
#define MCASP_GBLCTL_TIMEOUT (30000U) |
The time to try (in Msec) before the GBLCTL register setting timeouts if the setting/resetting is done in a context other than a task this will be used as a retry count rather than the MSec timeout.
◆ MCASP_RESET
#define MCASP_RESET ((uint32_t) 0x00U) |
McASP macros for enable/reset.
◆ MCASP_ENABLE
#define MCASP_ENABLE ((uint32_t) 0x01U) |
◆ MCASP_DISABLE
#define MCASP_DISABLE ((uint32_t) 0x00U) |
◆ MCASP_REG_OFFSET
#define MCASP_REG_OFFSET ((uint32_t)0x4U) |
◆ MCASP_TRANSFER_STATUS_COMPLETED
#define MCASP_TRANSFER_STATUS_COMPLETED (0U) |
I/O completed successfully.
◆ MCASP_TRANSFER_STATUS_STARTED
#define MCASP_TRANSFER_STATUS_STARTED (1U) |
◆ MCASP_TRANSFER_STATUS_CANCELLED
#define MCASP_TRANSFER_STATUS_CANCELLED (2U) |
I/O cancelled. Returned by incomplete read or write requests.
◆ MCASP_TRANSFER_STATUS_FAILED
#define MCASP_TRANSFER_STATUS_FAILED (3U) |
Generic failure condition.
◆ MCASP_TRANSFER_STATUS_TIMEOUT
#define MCASP_TRANSFER_STATUS_TIMEOUT (4U) |
◆ MCASP_DRIVER_MODE_POLLING
#define MCASP_DRIVER_MODE_POLLING (0U) |
MCASP read/write APIs blocks execution. This mode can only be used when called within a Task context.
◆ MCASP_DRIVER_MODE_INTERRUPT
#define MCASP_DRIVER_MODE_INTERRUPT (1U) |
MCASP read/write APIs does not block code execution and will call a MCASP_CallbackFxn. This mode can be used in a Task, Swi, or Hwi context.
◆ MCASP_DRIVER_MODE_DMA
#define MCASP_DRIVER_MODE_DMA (2U) |
MCASP read/write APIs does not block code execution and will use DMA for transfers.
◆ MCASP_OPMODE_MASTER
#define MCASP_OPMODE_MASTER (0U) |
I/O completed successfully.
◆ MCASP_OPMODE_SLAVE
#define MCASP_OPMODE_SLAVE (1U) |
◆ MCASP_CHANNEL_INPUT
#define MCASP_CHANNEL_INPUT (0x0001U) |
MCASP Channel will receive data.
◆ MCASP_CHANNEL_OUTPUT
#define MCASP_CHANNEL_OUTPUT (0x0002U) |
MCASP Channel will transmit data.
◆ MCASP_CHANNEL_INOUT
McASP channel transmits & recieves data.
◆ MCASP_DRIVER_STATE_DELETED
#define MCASP_DRIVER_STATE_DELETED (0U) |
◆ MCASP_DRIVER_STATE_CREATED
#define MCASP_DRIVER_STATE_CREATED (1U) |
◆ MCASP_DRIVER_STATE_INITIALIZED
#define MCASP_DRIVER_STATE_INITIALIZED (2U) |
◆ MCASP_DRIVER_STATE_OPENED
#define MCASP_DRIVER_STATE_OPENED (3U) |
◆ MCASP_DRIVER_STATE_CLOSED
#define MCASP_DRIVER_STATE_CLOSED (4U) |
◆ MCASP_DRIVER_STATE_DEINITIALIZED
#define MCASP_DRIVER_STATE_DEINITIALIZED (5U) |
◆ MCASP_DRIVER_STATE_POWERED_DOWN
#define MCASP_DRIVER_STATE_POWERED_DOWN (6U) |
◆ MCASP_DRIVER_STATE_PWRM_SUSPEND
#define MCASP_DRIVER_STATE_PWRM_SUSPEND (7U) |
◆ MCASP_SERIALIZER_STATUS_FREE
#define MCASP_SERIALIZER_STATUS_FREE (0U) |
◆ MCASP_SERIALIZER_STATUS_XMT
#define MCASP_SERIALIZER_STATUS_XMT (1U) |
◆ MCASP_SERIALIZER_STATUS_RCV
#define MCASP_SERIALIZER_STATUS_RCV (2U) |
◆ MCASP_CHANNEL_MODE_FREE
#define MCASP_CHANNEL_MODE_FREE (0U) |
◆ MCASP_CHANNEL_MODE_XMT_DIT
#define MCASP_CHANNEL_MODE_XMT_DIT (1U) |
◆ MCASP_CHANNEL_MODE_XMT_TDM
#define MCASP_CHANNEL_MODE_XMT_TDM (2U) |
◆ MCASP_CHANNEL_MODE_RCV
#define MCASP_CHANNEL_MODE_RCV (3U) |
◆ MCASP_WORD_SELECT_LSW
#define MCASP_WORD_SELECT_LSW (0U) |
◆ MCASP_WORD_SELECT_MSW
#define MCASP_WORD_SELECT_MSW (1U) |
◆ MCASP_TRANSMIT_STATE_TX_RESET
#define MCASP_TRANSMIT_STATE_TX_RESET (0U) |
◆ MCASP_TRANSMIT_STATE_TX_FLUSH
#define MCASP_TRANSMIT_STATE_TX_FLUSH (1U) |
◆ MCASP_TRANSMIT_STATE_LOAD_INIT_BUFFER
#define MCASP_TRANSMIT_STATE_LOAD_INIT_BUFFER (2U) |
◆ MCASP_TRANSMIT_STATE_RELEASE_FROM_RESET
#define MCASP_TRANSMIT_STATE_RELEASE_FROM_RESET (3U) |
◆ MCASP_TRANSMIT_STATE_WAIT_EVENT
#define MCASP_TRANSMIT_STATE_WAIT_EVENT (4U) |
◆ MCASP_TRANSMIT_STATE_PROCESS_EVENT
#define MCASP_TRANSMIT_STATE_PROCESS_EVENT (5U) |
◆ MCASP_TRANSMIT_STATE_LOAD_ACTIVE_BUFFER
#define MCASP_TRANSMIT_STATE_LOAD_ACTIVE_BUFFER (6U) |
◆ MCASP_TRANSMIT_STATE_DONE
#define MCASP_TRANSMIT_STATE_DONE (7U) |
◆ MCASP_TRANSMIT_STATE_SPIN_IDLE
#define MCASP_TRANSMIT_STATE_SPIN_IDLE (8U) |
◆ MCASP_TRANSMIT_STATE_ERROR
#define MCASP_TRANSMIT_STATE_ERROR (9U) |
◆ MCASP_TRANSMIT_STATE_EXIT
#define MCASP_TRANSMIT_STATE_EXIT (10U) |
◆ MCASP_RECEIVE_STATE_RX_RESET
#define MCASP_RECEIVE_STATE_RX_RESET (0U) |
◆ MCASP_RECEIVE_STATE_RX_FLUSH
#define MCASP_RECEIVE_STATE_RX_FLUSH (1U) |
◆ MCASP_RECEIVE_STATE_RELEASE_FROM_RESET
#define MCASP_RECEIVE_STATE_RELEASE_FROM_RESET (2U) |
◆ MCASP_RECEIVE_STATE_WAIT_EVENT
#define MCASP_RECEIVE_STATE_WAIT_EVENT (3U) |
◆ MCASP_RECEIVE_STATE_PROCESS_EVENT
#define MCASP_RECEIVE_STATE_PROCESS_EVENT (4U) |
◆ MCASP_RECEIVE_STATE_DONE
#define MCASP_RECEIVE_STATE_DONE (5U) |
◆ MCASP_RECEIVE_STATE_SPIN_IDLE
#define MCASP_RECEIVE_STATE_SPIN_IDLE (6U) |
◆ MCASP_RECEIVE_STATE_ERROR
#define MCASP_RECEIVE_STATE_ERROR (7U) |
◆ MCASP_RECEIVE_STATE_EXIT
#define MCASP_RECEIVE_STATE_EXIT (8U) |
◆ MCASP_Handle
◆ MCASP_CallbackFxn
The definition of a callback function used by the MCASP driver when used in Callback Mode.
- Parameters
-
◆ MCASP_init()
This function initializes the MCASP module.
◆ MCASP_deinit()
void MCASP_deinit |
( |
void |
| ) |
|
This function de-initializes the MCASP module.
◆ MCASP_openParamsInit()
◆ MCASP_open()
This function opens a given MCASP peripheral.
- Precondition
- MCASP controller has been initialized using MCASP_init()
- Parameters
-
index | Index of config to use in the MCASP_Config array |
openParams | Pointer to parameters to open the driver with |
- Returns
- A MCASP_Handle on success or a NULL on an error or if it has been opened already
- See also
- MCASP_init()
-
MCASP_close()
◆ MCASP_close()
Function to close a MCASP peripheral specified by the MCASP handle.
- Precondition
- MCASP_open() has to be called first
- Parameters
-
- See also
- MCASP_open()
◆ MCASP_getHandle()
This function returns the handle of an open MCASP Instance from the instance index.
- Precondition
- MCASP controller has been opened using MCASP_open()
- Parameters
-
- Returns
- A MCASP_Handle if it has been opened already or NULL otherwise
- See also
- MCASP_init()
-
MCASP_open()
◆ MCASP_transfer()
Generic transfer function using McASP.
- Parameters
-
- Returns
- Success/Failure for configuration
◆ gMcaspConfig
Externally defined driver configuration array.
◆ gMcaspConfigNum
Externally defined driver configuration array size.