MCASP Parameters.
MCASP Parameters are used to with the MCASP_open() call. Default values for these parameters are set using MCASP_openParamsInit().
If NULL is passed for the parameters, MCASP_open() uses default parameters.
Data Fields | |
uint32_t | edmaInst |
uint32_t MCASP_OpenParams::edmaInst |
EDMA instance used for MCASP transfer