McASP Transfer Data structure stored in driver object.
Data Fields | |
uint32_t | inProgress |
uint32_t | state |
int32_t | status |
uint32_t | count |
MCASP_Transaction * | transaction |
uint32_t MCASP_TransferObj::inProgress |
Flag to indicate if the transfer is ongoing
uint32_t MCASP_TransferObj::state |
MCASP Transfer State
int32_t MCASP_TransferObj::status |
MCASP_Transfer Status
uint32_t MCASP_TransferObj::count |
MCASP Transfer count
MCASP_Transaction* MCASP_TransferObj::transaction |
Pointer to current transaction struct