Go to the source code of this file.
Data Structures | |
struct | CSIRX_DphyConfig |
DPHY configuration. More... | |
struct | CSIRX_ComplexioLaneConfig |
Lane configuration. More... | |
struct | CSIRX_ComplexioLaneIntr |
Complex IO per lane interrupt. More... | |
struct | CSIRX_ComplexioLanesIntr |
Complex IO all (logical) lanes interrupts. More... | |
struct | CSIRX_ComplexioLanesConfig |
All lanes configuration. More... | |
struct | CSIRX_ComplexioConfig |
Complex IO configuration. More... | |
struct | CSIRX_CommonIntr |
Common (across contexts) interrupts. More... | |
struct | CSIRX_CommonIntrCallbacks |
Callbacks and callback arguments for various common interrupt event. More... | |
struct | CSIRX_CommonConfig |
Common to all context configuration. More... | |
struct | CSIRX_ContextPingPongConfig |
ping-pong related configuration for each context. Note specified ping and pong addresses can be identical which will effectively disable double buffering. More... | |
struct | CSIRX_ContextCropConfig |
Cropping configuration. More... | |
struct | CSIRX_ContextTranscodeConfig |
Transcoding configuration. More... | |
struct | CSIRX_ContextIntr |
Context interrupts. More... | |
struct | CSIRX_ContextConfig |
Context configuration. More... | |
struct | CSIRX_Info |
CSIRX Instance information. More... | |
struct | CSIRX_ContextObject |
Context specific state information, not to be used by end users. More... | |
struct | CSIRX_Object |
CSIRX Instance Object. Used internally, not to be used by end users. More... | |
struct | CSIRX_HwAttrs |
CSIRX HW Attributes. Generated when using sysconfig. More... | |
struct | CSIRX_Config |
CSIRX Instance Config Object. More... | |
Macros | |
#define | CSIRX_DATA_LANES_MAX (4U) |
Max possible data lanes. More... | |
#define | CSIRX_STOP_STATE_FSM_TIMEOUT_MAX (200000U) |
Special value of CSIRX_CommonConfig::stopStateFsmTimeoutInNanoSecs for setting maximum timeout, this is also the CSIRX IP reset state. More... | |
#define | CSIRX_CONTEXTS_MAX (8U) |
Max possible CSIRX contexts. More... | |
#define | CSIRX_PING_PONG_ADDRESS_LINEOFFSET_ALIGNMENT_IN_BYTES (32U) |
Ping-pong addresses and line offset alignment. Can be used for aligning ping-pong buffers and enforcing line offset alignment in bytes. More... | |
#define | CSIRX_LINEOFFSET_CONTIGUOUS_STORAGE (0U) |
Special value for contiguous storage. More... | |
#define | CSIRX_NUM_FRAMES_TO_ACQUIRE_INFINITE (0U) |
Special value of CSIRX_ContextConfig::numFramesToAcquire for setting infinite frames, this is also the CSIRX IP reset state. More... | |
#define | CSIRX_INTERRUPT_NOT_CONNECTED_ID (0xFFFFU) |
Interrupt number ID to indicate, this interrupt line is not connected in this CPU. More... | |
Complex IO power commands | |
#define | CSIRX_COMPLEXIO_POWER_COMMAND_OFF (0U) |
Power off ComplexIO. More... | |
#define | CSIRX_COMPLEXIO_POWER_COMMAND_ON (1U) |
Power on ComplexIO. More... | |
#define | CSIRX_COMPLEXIO_POWER_COMMAND_ULP (2U) |
Put ComplexIO in ULP (Ultra Low Power) state. More... | |
Complex IO power status | |
#define | CSIRX_COMPLEXIO_POWER_STATUS_OFF (0U) |
Complex IO power status OFF. More... | |
#define | CSIRX_COMPLEXIO_POWER_STATUS_ON (1U) |
Complex IO power status ON. More... | |
#define | CSIRX_COMPLEXIO_POWER_STATUS_ULP (2U) |
Complex IO power status ULP (Ultra Low Power) More... | |
Lane polarity | |
#define | CSIRX_LANE_POLARITY_PLUS_MINUS (0U) |
Lane polarity +/-. More... | |
#define | CSIRX_LANE_POLARITY_MINUS_PLUS (1U) |
Lane polarity -/+. More... | |
Lane position | |
#define | CSIRX_LANE_POSITION_LANE_NOT_USED (0U) |
Lane not used. More... | |
#define | CSIRX_LANE_POSITION_1 (1U) |
Physical lane position #1. More... | |
#define | CSIRX_LANE_POSITION_2 (2U) |
Physical lane position #2. More... | |
#define | CSIRX_LANE_POSITION_3 (3U) |
Physical lane position #3. More... | |
#define | CSIRX_LANE_POSITION_4 (4U) |
Physical lane position #4. More... | |
#define | CSIRX_LANE_POSITION_5 (5U) |
Physical lane position #5. More... | |
Data endianess | |
#define | CSIRX_ENDIANNESS_NATIVE_MIPI_CSI2 (0U) |
All little endian except legacy YUV422 8b and YUV420, which are big endian. More... | |
#define | CSIRX_ENDIANNESS_LITTLE_ENDIAN (1U) |
All little endian. More... | |
#define | CSIRX_ENDIANNESS_MAX (1U) |
Endianness max for error checking purposes. More... | |
Burst size defines | |
#define | CSIRX_BURST_SIZE_1X64 (0U) |
Burst size 1x64 OCP writes. More... | |
#define | CSIRX_BURST_SIZE_2X64 (1U) |
Burst size 2x64 OCP writes. More... | |
#define | CSIRX_BURST_SIZE_4X64 (2U) |
Burst size 4x64 OCP writes. More... | |
#define | CSIRX_BURST_SIZE_8X64 (3U) |
Burst size 8x64 OCP writes. More... | |
#define | CSIRX_BURST_SIZE_MAX (3U) |
Burst size max. More... | |
Ping or Pong done status | |
#define | CSIRX_CONTEXT_PINGPONG_STATUS_PING_DONE (0U) |
Ping is done. More... | |
#define | CSIRX_CONTEXT_PINGPONG_STATUS_PONG_DONE (1U) |
Pong is done. More... | |
Ping pong switching mode | |
#define | CSIRX_PING_PONG_FRAME_SWITCHING (0U) |
Switch ping pong address on end of frame. More... | |
#define | CSIRX_PING_PONG_LINE_SWITCHING (1U) |
Switch ping pong address on end of line. More... | |
Transcode format | |
#define | CSIRX_TRANSCODE_FORMAT_NO_TRANSCODE (0U) |
Transcoding disabled. More... | |
#define | CSIRX_TRANSCODE_FORMAT_IN_RAW10_ALAW_OUT_RAW8 (3U) |
Compress input RAW10 using A-law. Output is regular RAW8. More... | |
#define | CSIRX_TRANSCODE_FORMAT_IN_RAW8_OUT_RAW8 (4U) |
Regular RAW8 input and regular RAW8 output. More... | |
#define | CSIRX_TRANSCODE_FORMAT_IN_RAW10_OUT_RAW10_EXP16 (5U) |
Input uncompressed RAW10, output RAW10 + EXP16. More... | |
#define | CSIRX_TRANSCODE_FORMAT_IN_RAW10_OUT_RAW10_PACKED (6U) |
Input uncompressed RAW10, output regular packed RAW10. More... | |
#define | CSIRX_TRANSCODE_FORMAT_IN_RAW12_OUT_RAW12_EXP16 (7U) |
Input uncompressed RAW12, output RAW12 + EXP16. More... | |
#define | CSIRX_TRANSCODE_FORMAT_IN_RAW12_OUT_RAW12_PACKED (8U) |
Input uncompressed RAW12, output regular packed RAW12. More... | |
#define | CSIRX_TRANSCODE_FORMAT_IN_RAW14_OUT_RAW14 (9U) |
Input uncompressed RAW14, output uncompressed RAW14. More... | |
Data format | |
#define | CSIRX_FORMAT_OTHERS_EXCEPT_NULL_AND_BLANKING (0x000U) |
Others except NULL and BLANKING. More... | |
#define | CSIRX_FORMAT_EMBEDDED_8_BIT_NON_IMAGE (0x012U) |
Embedded 8-bit non image (for example JPEG) as per MIPI spec. More... | |
#define | CSIRX_FORMAT_YUV420_8_BIT (0x018U) |
YUV420 8-bit as per MIPI spec. More... | |
#define | CSIRX_FORMAT_YUV420_10_BIT (0x019U) |
YUV420 10-bit as per MIPI spec. More... | |
#define | CSIRX_FORMAT_YUV420_8_BIT_LEGACY (0x01AU) |
YUV420 8-bit legacy as per MIPI spec. More... | |
#define | CSIRX_FORMAT_YUV420_8_BIT_CSPS (0x01CU) |
YUV420 8-bit CSPS (Chroma Shifted Pixel Sampling) as per MIPI spec. More... | |
#define | CSIRX_FORMAT_YUV420_10_BIT_CSPS (0x01DU) |
YUV420 10-bit CSPS (Chroma Shifted Pixel Sampling) as per MIPI spec. More... | |
#define | CSIRX_FORMAT_YUV422_8_BIT (0x01EU) |
YUV422 8-bit as per MIPI spec. More... | |
#define | CSIRX_FORMAT_YUV422_10_BIT (0x01FU) |
YUV422 10-bit as per MIPI spec. More... | |
#define | CSIRX_FORMAT_RGB565 (0x022U) |
RGB565 as per MIPI spec. More... | |
#define | CSIRX_FORMAT_RGB888 (0x024U) |
RGB888 as per MIPI spec. More... | |
#define | CSIRX_FORMAT_RAW6 (0x028U) |
RAW6 as per MIPI spec. More... | |
#define | CSIRX_FORMAT_RAW7 (0x029U) |
RAW7 as per MIPI spec. More... | |
#define | CSIRX_FORMAT_RAW8 (0x02AU) |
RAW8 as per MIPI spec. More... | |
#define | CSIRX_FORMAT_RAW10 (0x02BU) |
RAW19 as per MIPI spec. More... | |
#define | CSIRX_FORMAT_RAW12 (0x02CU) |
RAW12 as per MIPI spec. More... | |
#define | CSIRX_FORMAT_RAW14 (0x02DU) |
RAW14 as per MIPI spec. More... | |
#define | CSIRX_FORMAT_RGB666_EXP32_24 (0x033U) |
RGB666 EXP32_24: EXP32 = Data expansion to 32 bits, padding with CSIRX_ContextConfig::alpha. Most significant 8-bits of output 32-bit will be equal to the least significant 8-bits of CSIRX_ContextConfig::alpha. More... | |
#define | CSIRX_FORMAT_USER_DEFINED_8_BIT_DATA_TYPE_1 (0x040U) |
User Defined 8-bit data type 1. More... | |
#define | CSIRX_FORMAT_USER_DEFINED_8_BIT_DATA_TYPE_2 (0x041U) |
User Defined 8-bit data type 2. More... | |
#define | CSIRX_FORMAT_USER_DEFINED_8_BIT_DATA_TYPE_3 (0x042U) |
User Defined 8-bit data type 3. More... | |
#define | CSIRX_FORMAT_USER_DEFINED_8_BIT_DATA_TYPE_4 (0x043U) |
User Defined 8-bit data type 4. More... | |
#define | CSIRX_FORMAT_USER_DEFINED_8_BIT_DATA_TYPE_5 (0x044U) |
User Defined 8-bit data type 5. More... | |
#define | CSIRX_FORMAT_USER_DEFINED_8_BIT_DATA_TYPE_6 (0x045U) |
User Defined 8-bit data type 6. More... | |
#define | CSIRX_FORMAT_USER_DEFINED_8_BIT_DATA_TYPE_7 (0x046U) |
User Defined 8-bit data type 7. More... | |
#define | CSIRX_FORMAT_USER_DEFINED_8_BIT_DATA_TYPE_8 (0x047U) |
User Defined 8-bit data type 8. More... | |
#define | CSIRX_FORMAT_RAW6_EXP8 (0x068U) |
RAW6 with data expansion to 8-bits, padding with zeros. More... | |
#define | CSIRX_FORMAT_RAW7_EXP8 (0x069U) |
RAW7 with data expansion to 8-bits, padding with zeros. More... | |
#define | CSIRX_FORMAT_USER_DEFINED_8_BIT_DATA_TYPE_1_EXP8 (0x080U) |
User Defined 8-bit data type 1 with data expansion to 8-bits, padding with zeros. More... | |
#define | CSIRX_FORMAT_USER_DEFINED_8_BIT_DATA_TYPE_2_EXP8 (0x081U) |
User Defined 8-bit data type 2 with data expansion to 8-bits, padding with zeros. More... | |
#define | CSIRX_FORMAT_USER_DEFINED_8_BIT_DATA_TYPE_3_EXP8 (0x082U) |
User Defined 8-bit data type 3 with data expansion to 8-bits, padding with zeros. More... | |
#define | CSIRX_FORMAT_USER_DEFINED_8_BIT_DATA_TYPE_4_EXP8 (0x083U) |
User Defined 8-bit data type 4 with data expansion to 8-bits, padding with zeros. More... | |
#define | CSIRX_FORMAT_USER_DEFINED_8_BIT_DATA_TYPE_5_EXP8 (0x084U) |
User Defined 8-bit data type 5 with data expansion to 8-bits, padding with zeros. More... | |
#define | CSIRX_FORMAT_USER_DEFINED_8_BIT_DATA_TYPE_6_EXP8 (0x085U) |
User Defined 8-bit data type 6 with data expansion to 8-bits, padding with zeros. More... | |
#define | CSIRX_FORMAT_USER_DEFINED_8_BIT_DATA_TYPE_7_EXP8 (0x086U) |
User Defined 8-bit data type 7 with data expansion to 8-bits, padding with zeros. More... | |
#define | CSIRX_FORMAT_USER_DEFINED_8_BIT_DATA_TYPE_8_EXP8 (0x087U) |
User Defined 8-bit data type 8 with data expansion to 8-bits, padding with zeros. More... | |
#define | CSIRX_FORMAT_RGB444_EXP16 (0x0A0U) |
RGB444 with data expansion to 16-bits. Most significant 4-bits of 16-bit output will be equal to the least significant 4-bits of CSIRX_ContextConfig::alpha. More... | |
#define | CSIRX_FORMAT_RGB555_EXP16 (0x0A1U) |
RGB555 with data expansion to 16-bits. Most significant 1-bit of 16-bit output will be equal to the least significant 1-bit of CSIRX_ContextConfig::alpha. More... | |
#define | CSIRX_FORMAT_RAW10_EXP16 (0x0ABU) |
RAW10 with data expansion to 16-bits. Most significant 6-bits of 16-bit output will be equal to the least significant 6-bits of CSIRX_ContextConfig::alpha. More... | |
#define | CSIRX_FORMAT_RAW12_EXP16 (0x0ACU) |
RAW12 with data expansion to 16-bits. Most significant 4-bits of 16-bit output will be equal to the least significant 4-bits of CSIRX_ContextConfig::alpha. More... | |
#define | CSIRX_FORMAT_RAW14_EXP16 (0x0ADU) |
RAW14 with data expansion to 16-bits. Most significant 2-bits of 16-bit output will be equal to the least significant 2-bits of CSIRX_ContextConfig::alpha. More... | |
#define | CSIRX_FORMAT_RGB666_EXP32 (0x0E3U) |
RGB666 with data expansion to 32-bits. Most significant 14-bits of 32-bit output will be equal to the least significant 14-bits of CSIRX_ContextConfig::alpha. More... | |
#define | CSIRX_FORMAT_RGB888_EXP32 (0x0E4U) |
RGB888 with data expansion to 32-bits. Most significant 8-bits of 32-bit output will be equal to the least significant 8-bits of CSIRX_ContextConfig::alpha. More... | |
User defined data format | |
#define | CSIRX_USER_DEFINED_FORMAT_RAW6 (0U) |
RAW6. More... | |
#define | CSIRX_USER_DEFINED_FORMAT_RAW7 (1U) |
RAW8. More... | |
#define | CSIRX_USER_DEFINED_FORMAT_RAW8 (2U) |
RAW8, not valid if CSIRX_ContextConfig::format is any of the defines CSIRX_FORMAT_USER_DEFINED_8_BIT_DATA_TYPE_x_EXP8 (x=1..8) in CSIRX_DATA_FORMAT. More... | |
FIFO depth | |
#define | CSIRX_FIFODEPTH_8X68 (2U) |
FIFO depth is 8 times 68-bits. More... | |
#define | CSIRX_FIFODEPTH_16X68 (3U) |
FIFO depth is 16 times 68-bits. More... | |
#define | CSIRX_FIFODEPTH_32X68 (4U) |
FIFO depth is 32 times 68-bits. More... | |
#define | CSIRX_FIFODEPTH_64X68 (5U) |
FIFO depth is 64 times 68-bits. More... | |
#define | CSIRX_FIFODEPTH_128X68 (6U) |
FIFO depth is 128 times 68-bits. More... | |
#define | CSIRX_FIFODEPTH_256X68 (7U) |
FIFO depth is 256 times 68-bits. More... | |
Typedefs | |
typedef struct CSIRX_Config_s * | CSIRX_Handle |
CSIRX driver handle. More... | |
typedef void(* | CSIRX_CommonCallback) (CSIRX_Handle handle, void *arg, struct CSIRX_CommonIntr_s *irq) |
Common interrupt callback. More... | |
typedef void(* | CSIRX_Callback) (CSIRX_Handle handle, void *arg) |
Generic Interrupt callback. More... | |
typedef void(* | CSIRX_ContextCallback) (CSIRX_Handle handle, void *arg, uint8_t contextId) |
Context interrupt callback. More... | |
Functions | |
int32_t | CSIRX_init () |
Initialize CSIRX driver. More... | |
int32_t | CSIRX_deinit () |
De-Initialize CSIRX driver. More... | |
CSIRX_Handle | CSIRX_open (uint32_t instanceId) |
Open CSIRX driver. More... | |
int32_t | CSIRX_getInfo (CSIRX_Handle handle, CSIRX_Info *info) |
Get CSIRX instance info. More... | |
int32_t | CSIRX_reset (CSIRX_Handle handle) |
Reset CSIRX instance. More... | |
int32_t | CSIRX_close (CSIRX_Handle handle) |
Close CSIRX instance. More... | |
void | CSIRX_DphyConfig_init (CSIRX_DphyConfig *config) |
Sets default values for configuration. More... | |
int32_t | CSIRX_dphySetConfig (CSIRX_Handle handle, CSIRX_DphyConfig *config) |
Configure DPHY. More... | |
int32_t | CSIRX_dphyIsControlClockResetDone (CSIRX_Handle handle, bool *isDone) |
Check if DPHY control clock reset is done. More... | |
int32_t | CSIRX_dphyIsByteClockResetDone (CSIRX_Handle handle, bool *isDone) |
Check if DPHY byte clock reset is done. More... | |
int32_t | CSIRX_dphyIsClockMissingDetectorError (CSIRX_Handle handle, bool *isError) |
Check if DPHY clock missing detector error. More... | |
void | CSIRX_ComplexioConfig_init (CSIRX_ComplexioConfig *config) |
Sets default values for configuration. More... | |
int32_t | CSIRX_complexioSetConfig (CSIRX_Handle handle, CSIRX_ComplexioConfig *config) |
Configure Complex IO. More... | |
int32_t | CSIRX_complexioClearAllIntr (CSIRX_Handle handle) |
Celar all pending complex IO interrupts. More... | |
int32_t | CSIRX_complexioGetPendingIntr (CSIRX_Handle handle, CSIRX_ComplexioLanesIntr *intrStatus) |
Get all pending complex IO interrupts. More... | |
int32_t | CSIRX_complexioGetPowerStatus (CSIRX_Handle handle, uint8_t *powerStatus) |
Query about ComplexIO power status. More... | |
int32_t | CSIRX_complexioSetPowerCommand (CSIRX_Handle handle, uint8_t powerCommand) |
Set Complex IO power command. More... | |
int32_t | CSIRX_complexioDeassertReset (CSIRX_Handle handle) |
Deaasert complex IO reset. More... | |
int32_t | CSIRX_complexioAssertForceRxModeOn (CSIRX_Handle handle) |
Assert Force Rx Mode on complex IO. More... | |
int32_t | CSIRX_complexioDeassertForceRxModeOn (CSIRX_Handle handle) |
De-assert Force Rx Mode on complex IO. More... | |
int32_t | CSIRX_complexioIsResetDone (CSIRX_Handle handle, bool *isDone) |
Check if complex IO reset is done. More... | |
int32_t | CSIRX_complexioIsDeassertForceRxModeOn (CSIRX_Handle handle, bool *isDeasserted) |
Check if force RX mode on is deasserted. More... | |
static int32_t | CSIRX_complexioPowerOn (CSIRX_Handle handle) |
Power ON complex IO. More... | |
static int32_t | CSIRX_complexioPowerOff (CSIRX_Handle handle) |
Power OFF complex IO. More... | |
static int32_t | CSIRX_complexioUltraLowPower (CSIRX_Handle handle) |
Put complex IO in ULP (Ultra Low Power) state. More... | |
void | CSIRX_CommonConfig_init (CSIRX_CommonConfig *config) |
Sets default values for configuration. More... | |
int32_t | CSIRX_commonSetConfig (CSIRX_Handle handle, CSIRX_CommonConfig *config) |
Configure common to all context settings. More... | |
int32_t | CSIRX_commonClearAllIntr (CSIRX_Handle handle) |
Clear all pending common to all context interrupts. More... | |
int32_t | CSIRX_commonGetPendingIntr (CSIRX_Handle handle, CSIRX_CommonIntr *intrStatus) |
Get all pending common to all context interrupts. More... | |
int32_t | CSIRX_commonGetGenericShortPacket (CSIRX_Handle handle, uint32_t *shortPacket) |
Get generic short packet header. More... | |
int32_t | CSIRX_commonEnable (CSIRX_Handle handle) |
Enable CSIRX interface. More... | |
int32_t | CSIRX_commonDisable (CSIRX_Handle handle) |
Disable CSIRX interface. More... | |
void | CSIRX_ContextConfig_init (CSIRX_ContextConfig *config) |
Sets default values for configuration. More... | |
int32_t | CSIRX_contextSetConfig (CSIRX_Handle handle, uint8_t contextId, CSIRX_ContextConfig *config) |
Configure context. More... | |
int32_t | CSIRX_contextSetPingPongAddress (CSIRX_Handle handle, uint8_t contextId, uint32_t pingAddress, uint32_t pongAddress) |
Set context ping and pong address. More... | |
int32_t | CSIRX_contextSetLineOffset (CSIRX_Handle handle, uint8_t contextId, int32_t lineOffset) |
Set context line offset. More... | |
int32_t | CSIRX_contextEnable (CSIRX_Handle handle, uint8_t contextId) |
Enable context. More... | |
int32_t | CSIRX_contextDisable (CSIRX_Handle handle, uint8_t contextId) |
Disable context. More... | |
int32_t | CSIRX_contextClearAllIntr (CSIRX_Handle handle, uint8_t contextId) |
Clear all pending context interrupts. More... | |
int32_t | CSIRX_contextGetPendingIntr (CSIRX_Handle handle, uint8_t contextId, CSIRX_ContextIntr *intrStatus) |
Get all pending context interrupts. More... | |
int32_t | CSIRX_contextGetFrameNumber (CSIRX_Handle handle, uint8_t contextId, uint16_t *frameNumber) |
Get current frame number as decoded from within CSIRX long packet. More... | |
int32_t | CSIRX_contextGetRecvAddress (CSIRX_Handle handle, uint8_t contextId, uint32_t *bufAddress) |
Get current completed receive address. More... | |
int32_t | CSIRX_contextGetPingPongStatus (CSIRX_Handle handle, uint8_t contextId, uint8_t *pingPongStatus) |
Get status if ping or pong buffer write is done. More... | |
int32_t | CSIRX_debugModeSetShortPacket (CSIRX_Handle handle, uint32_t shortPacket) |
Set short packet header. More... | |
int32_t | CSIRX_debugModeSetLongPacketHeader (CSIRX_Handle handle, uint32_t longPacketHeader) |
Set long packet header. More... | |
int32_t | CSIRX_debugModeSetLongPacketPayload (CSIRX_Handle handle, uint32_t payload) |
Set long packet payload. More... | |
int32_t | CSIRX_debugModeEnable (CSIRX_Handle handle) |
Enable debug mode. More... | |
int32_t | CSIRX_debugModeDisable (CSIRX_Handle handle) |
Disable debug mode. More... | |
void | CSIRX_debugModeGenerateFrames (CSIRX_Handle handle, uint16_t txFormat, uint8_t virtualChannelId, uint32_t numOfFrames, uint32_t numLinesPerFrame, uint32_t numBytesPerLine) |
Generate frames in debug mode. More... | |
Variables | |
CSIRX_Config | gCsirxConfig [] |
Array of CSIRX instance enabled via SysConfig. More... | |
uint32_t | gCsirxConfigNum |
Number of CSIRX instances enabled via SysConfig. More... | |