See SIPC Notify for more details.
|
typedef void(* | SIPC_FxnCallback) (uint8_t remoteSecCoreId, uint8_t localClientId, uint8_t remoteClientId, uint8_t *msgValue, void *args) |
| User callback that is invoked when a message is received from a reote core for a given client ID. More...
|
|
◆ SIPC_FxnCallback
typedef void(* SIPC_FxnCallback) (uint8_t remoteSecCoreId, uint8_t localClientId, uint8_t remoteClientId,uint8_t *msgValue, void *args) |
User callback that is invoked when a message is received from a reote core for a given client ID.
Before invoking the API, the IPC module would have 'popped` the message from the HW or SW FIFO already. This callback is called frm ISR context, so all constraints of ISR should be applied by the callback, e.g. no blocking wait, quickly handle message and exit ISR.
For most applications, it is recommended to put the message value into a local SW queue and defer the message handling itself to a application task.
- Note
- This callback will process the *msgValue . Registered function should not be blocking. as this is called from isr context.
- Parameters
-
remoteSecCoreId | [in] Remote core that has sent the message |
localClientId | [in] Local client ID to which the message is sent |
remoteClientId | [in] remote client Id from which this message has been sent |
msgValue | [in] pointer to the buffer with SIPC_MSG_SIZE elements |
args | [in] Argument pointer passed by user when SIPC_registerClient is called |
◆ SIPC_fifoFlags
flags to pass with the SIPC_sendMsg Api which indicates the flow of execution when the write FIFO is full
Enumerator |
---|
ABORT_ON_FIFO_FULL | |
WAIT_IF_FIFO_FULL | |
◆ SIPC_coreId
Core Ids to identify different cores.
Enumerator |
---|
CORE_ID_R5FSS0_0 | |
CORE_ID_R5FSS0_1 | |
CORE_ID_R5FSS1_0 | |
CORE_ID_R5FSS1_1 | |
CORE_ID_HSM0_0 | |
CORE_ID_MAX | |
◆ SIPC_SecCoreId
Secure host Id to identify different secure hosts. Max number of secure host on AM263x is 2.
Enumerator |
---|
CORE_INDEX_SEC_MASTER_0 | |
CORE_INDEX_SEC_MASTER_1 | |
CORE_INDEX_HSM | |
MAX_SEC_CORES_WITH_HSM | |
◆ SIPC_Params_init()
Set default value to SIPC_Params.
- Parameters
-
params | [out] Default initialized structure |
◆ SIPC_init()
Initialize Secure IPC notify module.
This API will initialize the HW used for IPC including registering interrupts for receiving messages.
- Parameters
-
params | [in] Initializaion parameters |
◆ SIPC_deInit()
De-initialize secure IPC Notify module.
This API will de-initialize the HW used for IPC including un-registering interrupts for receiving messages.
◆ SIPC_sendMsg()
int32_t SIPC_sendMsg |
( |
uint8_t |
remoteSecCoreId, |
|
|
uint8_t |
remoteClientId, |
|
|
uint8_t |
localClientId, |
|
|
uint8_t * |
msgValue, |
|
|
SIPC_fifoFlags |
waitForFifoNotFull |
|
) |
| |
Send message to a specific remote core and specific client ID on that remote core.
- Note
- To reduce latency, error checks are avoided in this API. Users need to make sure the client ID value is < SIPC_CLIENT_ID_MAX and message value is < SIPC_CLIENT_ID_MAX
-
This API can be called from within ISRs and is also thread-safe. Internally this API disables interrupts for a short while to make the API ISR and thread safe.
-
One cannot send messages to self, i.e remoteCoreId, cannot be same as core ID of the CPU that called this API.
- Parameters
-
remoteSecCoreId | [in] Remote core to sent message to, see |
remoteClientId | [in] Remote core client ID to send message to |
localClientId | [in] self core client ID from which the meessage is being sent |
msgValue | [in] Message value to send, MUST be < IPC_NOTIFY_MSG_VALUE_MAX |
waitForFifoNotFull | [in] 1: wait for message to be inserted into HW or SW FIFO [in] 0: if FIFO is full, dont send message and return with error. |
- Returns
- SystemP_SUCCESS, message sent successfully
-
SystemP_FAILURE, message could not be sent since HW or SW FIFO for holding the message is full.
◆ SIPC_registerClient()
int32_t SIPC_registerClient |
( |
uint8_t |
localClientId, |
|
|
SIPC_FxnCallback |
msgCallback, |
|
|
void * |
args |
|
) |
| |
Register a callback to handle messages received from a specific remote core and for a specific local client ID.
- Parameters
-
localClientId | [in] Client ID to which the message has been sent |
msgCallback | [in] Callback to invoke, if callback is already registered, error will be returned. |
args | [in] User arguments, that are passed back to user when the callback is invoked |
- Returns
- SystemP_SUCCESS, callback registered sucessfully
-
SystemP_FAILURE, callback registration failed, either remoteCoreId or localClientId is invalid or callback already registered.
◆ SIPC_unregisterClient()
int32_t SIPC_unregisterClient |
( |
uint16_t |
localClientId | ) |
|
Un-register a previously registered callback.
- Parameters
-
localClientId | [in] Client ID to which the message has been sent |
- Returns
- SystemP_SUCCESS, callback un-registered sucessfully
-
SystemP_FAILURE, callback un-registration failed, either remoteCoreId or localClientId is invalid
◆ SIPC_getSelfCoreId()
uint32_t SIPC_getSelfCoreId |
( |
| ) |
|
Return current core ID.
- Returns
- Core ID, see SIPC_coreId for valid values.
◆ SIPC_getSelfSecMasterId()
uint32_t SIPC_getSelfSecMasterId |
( |
| ) |
|
Return current core sec master ID.
- Returns
- Core ID, see SIPC_SecCoreId for valid values.
◆ SIPC_isCoreEnabled()
uint32_t SIPC_isCoreEnabled |
( |
uint32_t |
coreId | ) |
|
Check if a core is enabled for SIPC.
- Parameters
-
- Returns
- 1: core is enabled for SIPC, 0: core is not enabled for SIPC