This module contains APIs for device drivers for various peripherals supported in this SDK
Sub Modules | |
APIs for ADC | |
APIs for BOOTLOADING CPUs | |
APIs for CMPSS | |
APIs for DAC | |
APIs for ECAP | |
APIs for EDMA | |
APIs for EPWM | |
APIs for EQEP | |
APIs for FSI | |
APIs for FSI RX | |
APIs for FSI TX | |
APIs for GPIO | |
APIs for HSM_CLIENT | |
This driver currently is used to load HSMRt firmware on HS-SE devices. This driver is used to leverage services from HSM on HS-FS and HS-SE devices. To use this on HS-FS devices, an encrypted HSMRt binary is needed which will be released by 8.4. For HS-SE devices, TIFS-MCU can be used for HSM which is available on mySecureSW. | |
APIs for I2C | |
APIs for IPC Notify | |
APIs for IPC RPMessage | |
APIs for LIN | |
APIs for MCAN | |
APIs for MCSPI | |
APIs for MDIO | |
APIs for MPU Firewall | |
APIs for PINMUX | |
APIs for PRUICSS | |
APIs for QSPI | |
APIs for RTI | |
APIs for SDFM | |
APIs for SOC Specific Functions | |
APIs for SPINLOCK | |
APIs for Secure IPC Notify | |
APIs for UART | |
APIs for WDT | |