AM263x MCU+ SDK  08.03.00
Hsmclient_ipcLoadHSMResult Struct Reference

Detailed Description

IPC Load HSM Result.

This is the format of the message which is sent from the HSM Boot ROM to the R5 SBL to indicate the result of the loading request.

Data Fields

Hsmclient_ipcExportHeader header
 This is header which is added to all the messages. More...
 
Hsmclient_ipcLoadHSMStatus status
 Status of the HSM Boot ROM Loading status. More...
 

Field Documentation

◆ header

Hsmclient_ipcExportHeader Hsmclient_ipcLoadHSMResult::header

This is header which is added to all the messages.

◆ status

Hsmclient_ipcLoadHSMStatus Hsmclient_ipcLoadHSMResult::status

Status of the HSM Boot ROM Loading status.