IPC Load HSM Runtime.
This is the format of the message which is sent to load the HSM runtime. The R5 SBL will populate this message and will send to the HSM Boot ROM.
Data Fields | |
uint32_t | version |
Version of the IPC Exported Interface. More... | |
Hsmclient_ipcExportMsgType | msgType |
IPC Message Type which is being sent. More... | |
uint16_t | checksum |
This is the 16bit checksum which will need to be added to ensure correctness of the data being passed. The checksum is computed on the header + payload. More... | |
uint32_t Hsmclient_ipcExportHeader::version |
Version of the IPC Exported Interface.
Hsmclient_ipcExportMsgType Hsmclient_ipcExportHeader::msgType |
IPC Message Type which is being sent.
uint16_t Hsmclient_ipcExportHeader::checksum |
This is the 16bit checksum which will need to be added to ensure correctness of the data being passed. The checksum is computed on the header + payload.