Data Structures | |
struct | Hsmclient_ipcExportHeader |
IPC Load HSM Runtime. More... | |
struct | Hsmclient_ipcLoadHSM |
IPC Load HSM Runtime. More... | |
struct | Hsmclient_ipcLoadHSMResult |
IPC Load HSM Result. More... | |
Macros | |
#define | HSMCLIENT_IPC_EXPORT_VERSION (0x1U) |
This is the version number for the IPC Export Interface. The version number should be the same between the HSM Boot ROM and the R5 SBL. In the case of a mismatch the HSM Boot ROM will generate an error. More... | |
Enumerations | |
enum | Hsmclient_ipcExportMsgType { Hsmclient_ipcExportMsgType_LOAD_HSM = 0x9980A1D4U, Hsmclient_ipcExportMsgType_LOAD_HSM_RESULT = 0xA70915DEU } |
hsmclient IPC Message Type More... | |
enum | Hsmclient_ipcLoadHSMStatus { Hsmclient_ipcLoadHSMStatus_SUCCESS = 0x4A43AB6CU, Hsmclient_ipcLoadHSMStatus_FAILURE = 0x7021AE4BU } |
IPC Load HSM Status. More... | |
Functions | |
static uint16_t | Hsmclient_computeIPCChecksum (uint8_t *ptrBuffer, uint32_t sizeMsg) |
This is a utility function which is used to compute the checksum on the provided buffer. More... | |
static void | Hsmclient_mboxRxISR (void *args) |
mailbox Rx ISR More... | |
int32_t | Hsmclient_init (uint32_t coreId) |
Initialize Hsm Client module. More... | |
int32_t | Hsmclient_loadHSMRtFirmware (const uint8_t *pHSMRt_firmware) |
Loads the HSMRt firmware. This is typically called by SBL. More... | |
Variables | |
volatile uint32_t | gHsmRtDownloadComplete = 0 |
CSL_mss_ctrlRegs * | ptrMSSCtrlRegs = (CSL_mss_ctrlRegs *)CSL_MSS_CTRL_U_BASE |
#define HSMCLIENT_IPC_EXPORT_VERSION (0x1U) |
This is the version number for the IPC Export Interface. The version number should be the same between the HSM Boot ROM and the R5 SBL. In the case of a mismatch the HSM Boot ROM will generate an error.
hsmclient IPC Message Type
The enumeration describes the messages which are supported by the IPC Module executing in the HSM Runtime state.
|
static |
This is a utility function which is used to compute the checksum on the provided buffer.
ptrBuffer | Buffer pointer. |
sizeMsg | message size in bytes. |
|
static |
mailbox Rx ISR
args | loadHSMResult passing as arument |
volatile uint32_t gHsmRtDownloadComplete = 0 |
CSL_mss_ctrlRegs* ptrMSSCtrlRegs = (CSL_mss_ctrlRegs *)CSL_MSS_CTRL_U_BASE |