AM263Px MCU+ SDK  26.00.00

Detailed Description

UART driver object.

Data Fields

UART_Params prms
 
const uint8_t * writeBuf
 
uint32_t writeCount
 
uint32_t writeSizeRemaining
 
uint8_t * readBuf
 
uint32_t readCount
 
uint32_t readSizeRemaining
 
uint32_t rxTimeoutCnt
 
uint32_t readErrorCnt
 
UART_Transaction * readTrans
 
UART_Transaction * writeTrans
 
uint32_t isOpen
 
SemaphoreP_Object * lock
 
SemaphoreP_Object lockObj
 
SemaphoreP_Object * readTransferSem
 
SemaphoreP_Object readTransferSemObj
 
SemaphoreP_Object * writeTransferSem
 
SemaphoreP_Object writeTransferSemObj
 
HwiP_Object * hwiHandle
 
HwiP_Object hwiObj
 
void * uartDmaHandle
 
UARTLLD_Object uartLld_object
 
UARTLLD_Handle uartLld_handle
 
UARTLLD_InitHandle uartLld_initHandle
 
UARTLLD_InitObject uartLld_initObject
 

Field Documentation

◆ prms

UART_Params UART_Object::prms

Open parameter as provided by user

◆ writeBuf

const uint8_t* UART_Object::writeBuf

Buffer data pointer

◆ writeCount

uint32_t UART_Object::writeCount

Number of Chars sent

◆ writeSizeRemaining

uint32_t UART_Object::writeSizeRemaining

Chars remaining in buffer

◆ readBuf

uint8_t* UART_Object::readBuf

Buffer data pointer

◆ readCount

uint32_t UART_Object::readCount

Number of Chars read

◆ readSizeRemaining

uint32_t UART_Object::readSizeRemaining

Chars remaining in buffer

◆ rxTimeoutCnt

uint32_t UART_Object::rxTimeoutCnt

Receive timeout error count

◆ readErrorCnt

uint32_t UART_Object::readErrorCnt

Line status error count

◆ readTrans

UART_Transaction* UART_Object::readTrans

Pointer to the current read transaction

◆ writeTrans

UART_Transaction* UART_Object::writeTrans

Pointer to the current write transaction

◆ isOpen

uint32_t UART_Object::isOpen

Flag to indicate whether the instance is opened already

◆ lock

SemaphoreP_Object* UART_Object::lock

Instance lock - to protect across transfers

◆ lockObj

SemaphoreP_Object UART_Object::lockObj

Driver lock object

◆ readTransferSem

SemaphoreP_Object* UART_Object::readTransferSem

Read Transfer Sync Sempahore - to sync between transfer completion ISR and task

◆ readTransferSemObj

SemaphoreP_Object UART_Object::readTransferSemObj

Read Transfer Sync Sempahore object

◆ writeTransferSem

SemaphoreP_Object* UART_Object::writeTransferSem

Write Transfer Sync Sempahore - to sync between transfer completion ISR and task

◆ writeTransferSemObj

SemaphoreP_Object UART_Object::writeTransferSemObj

Write Transfer Sync Sempahore object

◆ hwiHandle

HwiP_Object* UART_Object::hwiHandle

Interrupt handle for controller ISR

◆ hwiObj

HwiP_Object UART_Object::hwiObj

Interrupt object

◆ uartDmaHandle

void* UART_Object::uartDmaHandle

Pointer to current transaction struct

◆ uartLld_object

UARTLLD_Object UART_Object::uartLld_object

◆ uartLld_handle

UARTLLD_Handle UART_Object::uartLld_handle

[IN] Initialization parameters of UART instance

◆ uartLld_initHandle

UARTLLD_InitHandle UART_Object::uartLld_initHandle

◆ uartLld_initObject

UARTLLD_InitObject UART_Object::uartLld_initObject