AM263Px MCU+ SDK  11.01.00
UARTLLD_Handle Struct Reference

Detailed Description

UART driver object.

Data Fields

uint32_t baseAddr
 
UARTLLD_InitHandle hUartInit
 
const uint8_t * writeBuf
 
uint32_t writeCount
 
uint32_t writeSizeRemaining
 
uint8_t * readBuf
 
uint32_t readCount
 
uint32_t readSizeRemaining
 
uint32_t rxTimeoutCnt
 
uint32_t readErrorCnt
 
UART_Transaction readTrans
 
UART_Transaction writeTrans
 
uint32_t currIntMask
 
uint32_t state
 
void * readTransferMutex
 
void * writeTransferMutex
 
struct UART_Config_s * args
 
uint64_t lineStatusTimeout
 

Field Documentation

◆ baseAddr

uint32_t UARTLLD_Handle::baseAddr

Peripheral base address

◆ hUartInit

UARTLLD_InitHandle UARTLLD_Handle::hUartInit

[IN] Initialization parameters of UART instance

◆ writeBuf

const uint8_t* UARTLLD_Handle::writeBuf

Buffer data pointer

◆ writeCount

uint32_t UARTLLD_Handle::writeCount

Number of Chars sent

◆ writeSizeRemaining

uint32_t UARTLLD_Handle::writeSizeRemaining

Chars remaining in buffer

◆ readBuf

uint8_t* UARTLLD_Handle::readBuf

Buffer data pointer

◆ readCount

uint32_t UARTLLD_Handle::readCount

Number of Chars read

◆ readSizeRemaining

uint32_t UARTLLD_Handle::readSizeRemaining

Chars remaining in buffer

◆ rxTimeoutCnt

uint32_t UARTLLD_Handle::rxTimeoutCnt

Receive timeout error count

◆ readErrorCnt

uint32_t UARTLLD_Handle::readErrorCnt

Line status error count

◆ readTrans

UART_Transaction UARTLLD_Handle::readTrans

Pointer to the current read transaction

◆ writeTrans

UART_Transaction UARTLLD_Handle::writeTrans

Pointer to the current write transaction

◆ currIntMask

uint32_t UARTLLD_Handle::currIntMask

◆ state

uint32_t UARTLLD_Handle::state

Flag to indicate whether the instance is opened already

◆ readTransferMutex

void* UARTLLD_Handle::readTransferMutex

Read Transfer Sync Sempahore - to signal transfer completion

◆ writeTransferMutex

void* UARTLLD_Handle::writeTransferMutex

Write Transfer Sync Sempahore - to signal transfer completion

◆ args

struct UART_Config_s* UARTLLD_Handle::args

Pointer to be used by application to store miscellaneous data.

◆ lineStatusTimeout

uint64_t UARTLLD_Handle::lineStatusTimeout

Variable to hold the line status timeout in ticks