AM263Px MCU+ SDK  26.00.00

Introduction

This is the header file for the CANFD driver which exposes the data structures and exported API which can be used by the applications to use the CANFD driver.

The CANFD driver provides functionality of transferring data between CANFD peripherals. This driver does not interpret any of the data sent to or received from using this peripheral.

The CANFD header file should be included in an application as follows:

#include <ti/drivers/canfd/canfd.h>

Initializing the driver

The CANFD Driver needs to be initialized once across the System. This is done using the CANFD_open. None of the CANFD API's can be used without invoking this API.

Once the CANFD Driver has been initialized; the bit timing can be configured using CANFD_configBitTime. This APIs can be called multiple times to reconfigure bit timings.

Creating the message objects

Message objects are used to transmit or receive data over the CANFD peripheral. A message object is created using CANFD_createMsgObject.

Sending and receiving data

Data is transmitted using the CANFD_write. The application will be notified when the transmit is complete if it has enabled dataInterruptEnable and registered a callback function appDataCallBack when initializing the CANFD driver.

If the receive interrupts are enabled using dataInterruptEnable field and a callback function appCallBack has been registered when initializing the CANFD driver, the driver notifies the application when the data has arrived. The application needs to call the CANFD_read function to read the received data.

Error and status handling

The application can monitor the ECC error, Bus off error and Protocol Errors by enabling the error interrupts errInterruptEnable. The driver will call the registered callback function appErrCallBack to indicate which error fields caused the interrupt. It is up to the application to take appropriate action.

Get/Set Options

Helper APIs to get and set various statistics, error counters, ECC diagnostics, power down have been provided. Refer to CANFD_Option for more information.

Limitation

The CANFD driver does not support the DMA or power down.

Go to the source code of this file.

typedef struct CANFD_Config_s * CANFD_Handle
 A handle that is returned from a CANFD_open() call. More...
 
uint32_t gCANFDConfigNum
 Externally defined driver configuration array size. More...
 

CANFD ECC error type

#define CANFD_MCAN_ECC_ERR_TYPE_SEC   (0U)
 
#define CANFD_MCAN_ECC_ERR_TYPE_DED   (1U)
 
typedef uint32_t CANFD_MCANECCErrType
 This enumeration defines the MCAN ECC Error Types. More...
 

Data Structures

struct  CANFD_MCANLoopbackCfgParams
 
struct  CANFD_MCANBitTimingParams
 
struct  CANFD_MCANTdcConfig
 
struct  CANFD_MCANGlobalFiltConfig
 
struct  CANFD_MCANMsgRAMCfgParams
 
struct  CANFD_MCANECCConfigParams
 
struct  CANFD_MCANErrCntStatus
 
struct  CANFD_MCANProtocolStatus
 
struct  CANFD_MCANECCErrForceParams
 
struct  CANFD_MCANECCErrStatus
 
union  CANFD_ErrStatusResp
 
struct  CANFD_Attrs
 
struct  CANFD_OptionTLV
 
struct  CANFD_OpenParams
 
struct  CANFD_Object
 
struct  CANFD_Config
 
struct  CANFD_DmaMsgConfig
 
struct  CANFD_DmaRxBuf
 
struct  CANFD_MessageObject
 
struct  CANFD_MCANMsgObjectStats
 

Macros

Return status

Return status when the API execution was successful

#define MCAN_STATUS_SUCCESS   ((int32_t)0)
 
#define MCAN_STATUS_FAILURE   ((int32_t)-1)
 Return status when the API execution was not successful due to a failure. More...
 
Transfer Mode

This determines whether the driver operates synchronously or asynchronously

In CANFD_TRANSFER_MODE_BLOCKING mode CANFD_write() blocks code execution until the transaction has completed

In CANFD_TRANSFER_MODE_CALLBACK CANFD_write() does not block code execution and instead calls a CANFD_TransferCallbackFxn callback function when the transaction has completed

#define CANFD_TRANSFER_MODE_BLOCKING   (0U)
 CANFD_write() blocks execution. This mode can only be used when called within a Task context More...
 
#define CANFD_TRANSFER_MODE_CALLBACK   (1U)
 CANFD_write() does not block code execution and will call a CANFD_TransferCallbackFxn. This mode can be used in a Task, Swi, or Hwi context More...
 
Operating Mode

Values used to determine the CANFD driver operation.

#define CANFD_OPER_MODE_POLLED   (0U)
 
#define CANFD_OPER_MODE_INTERRUPT   (1U)
 
#define CANFD_OPER_MODE_DMA   (2U)
 
#define MCAN_MSG_RAM_STD_ELEM_SIZE   (1U)
 The section has a list of all the data structures which are exposed to the application. More...
 
#define MCAN_MSG_RAM_EXT_ELEM_SIZE   (2U)
 Extended ID Filter Element Size. More...
 
#define MCAN_MSG_HEADER_SIZE   (8U)
 MCAN Header size in Bytes. More...
 
#define MCAN_FRAME_TYPE_FD   (1U)
 MCAN Frame type FD. More...
 
#define MCAN_MSG_RAM_TX_RX_ELEM_SIZE   (18U)
 Tx/Rx Element Size. 18 words = 18 * 4 = 72 bytes: 8 bytes of header and 64 bytes of data. More...
 
#define XTD_MSGID_MASK   (0x1fffffffU)
 Message Identifier Masks. More...
 
#define STD_MSGID_MASK   (0x7ffU)
 
#define STD_MSGID_SHIFT   (18U)
 
#define MCAN_MAX_PAYLOAD_BYTES   (64U)
 Maximum payload supported by CAN-FD protocol in bytes. More...
 
#define MCAN_MAX_RX_BUFFERS   (64U)
 Maximum number of Rx buffers. More...
 
#define MCAN_MAX_TX_BUFFERS   (32U)
 Maximum number of Tx buffers. More...
 
#define CANFD_UTILS_ARRAYSIZE(x)   (sizeof(x) / sizeof(x[0]))
 Macro to get the size of an array. More...
 
#define CANFD_UTILS_GETARRAYINDEX(member, array)   (member - &array[0])
 Get the index of the given element within an array. More...
 
#define CANFD_UTILS_ARRAYISMEMBER(member, array)
 Macro to determine if a member is part of an array. More...
 
#define MCAN_INTR_MASK
 Defines all the interrupt are enabled. More...
 
#define CANFD_DMA_TX_COMPLETION_INTERMEDIATE   (1U)
 completion type for Tx in dma mode - Intermediate completion More...
 
#define CANFD_DMA_TX_COMPLETION_FINAL   (2U)
 completion type for Tx in dma mode - Final completion More...
 
#define CANFD_DMA_RX_COMPLETION_INTERMEDIATE   (1U)
 completion type for Rx in dma mode - Intermediate completion More...
 
#define CANFD_DMA_RX_COMPLETION_FINAL   (2U)
 completion type for Rx in dma mode - Final completion More...
 
#define CANFD_MAX_DLC_MAPPING   (16U)
 Maximum data to DLC mapping supported. Refer MCAN_DataLengthSize. More...
 
CANFD Driver State

This macros defines the values used to represent the CANFD driver state

#define CANFD_DRIVER_STATE_UNINIT   (0U)
 
#define CANFD_DRIVER_STATE_STARTED   (1U)
 
#define CANFD_DRIVER_STATE_STOPPED   (2U)
 
#define CCANFD_DRIVER_STATE_SLEEP   (3U)
 

Typedefs

CANFD Option TLV

Options TLV data structure

Specifies the option type, length, value.

typedef void(* CANFD_TransferCallbackFxn) (void *args, CANFD_Reason reason)
 The definition of a callback function used by the CANFD driver when used in CANFD_TRANSFER_MODE_CALLBACK. More...
 
typedef void(* CANFD_ErrorCallbackFxn) (void *args, CANFD_Reason reason, CANFD_ErrStatusResp *errStatusResp)
 The definition of a callback function used by the CANFD driver when used in CANFD_TRANSFER_MODE_CALLBACK in case of error. More...
 
CANFD Message Handle

CANFD message object handle returned by the CANFD_createMsgObject() API call.

typedef CANFD_MessageObject * CANFD_MsgObjHandle
 

Enumerations

CANFD Element Size

This enumeration defines the MCAN FIFO/Buffer element Size

enum  CANFD_MCANElemSize {
  CANFD_MCANElemSize_8BYTES = 0U, CANFD_MCANElemSize_12BYTES = 1U, CANFD_MCANElemSize_16BYTES = 2U, CANFD_MCANElemSize_20BYTES = 3U,
  CANFD_MCANElemSize_24BYTES = 4U, CANFD_MCANElemSize_32BYTES = 5U, CANFD_MCANElemSize_48BYTES = 6U, CANFD_MCANElemSize_64BYTES = 7U
}
 
CANFD Operation Mode

Enumerates the values used to represent the MCAN mode of operation

enum  CANFD_MCANOperationMode { CANFD_MCANOperationMode_NORMAL = 0U, CANFD_MCANOperationMode_SW_INIT = 1U }
 
CANFD Direction

This enumeration defines the values used to set the direction of message object

enum  CANFD_Direction { CANFD_Direction_RX, CANFD_Direction_TX }
 
CANFD Identifier Type

This enumeration defines the values used to represent the CAN Identifier Type

enum  CANFD_MCANXidType { CANFD_MCANXidType_11_BIT, CANFD_MCANXidType_29_BIT }
 
CANFD Frame Type

This enumeration defines the CAN frame type

enum  CANFD_MCANFrameType { CANFD_MCANFrameType_CLASSIC, CANFD_MCANFrameType_FD }
 
CANFD Time out select

This enumeration defines the MCAN timeout counter configuration

enum  CANFD_MCANTimeOutSelect { CANFD_MCANTimeOutSelect_CONT = 0U, CANFD_MCANTimeOutSelect_TX_EVENT_FIFO = 1U, CANFD_MCANTimeOutSelect_RX_FIFO0 = 2U, CANFD_MCANTimeOutSelect_RX_FIFO1 = 3U }
 
CANFD Loopback mode

This enumeration defines the MCAN Loopback mode

enum  CANFD_MCANLoopBackMode { CANFD_MCANLoopBackMode_INTERNAL = 0U, CANFD_MCANLoopBackMode_EXTERNAL = 1U }
 
CANFD Communication State

This enumeration defines the MCAN's communication state

enum  CANFD_MCANCommState { CANFD_MCANCommState_SYNCHRONIZING = 0U, CANFD_MCANCommState_IDLE = 1U, CANFD_MCANCommState_RECEIVER = 2U, CANFD_MCANCommState_TRANSMITTER = 3U }
 
CANFD Error Code

This enumeration defines the MCAN's Error Code

enum  CANFD_MCANErrCode {
  CANFD_MCANErrCode_NO_ERROR = 0U, CANFD_MCANErrCode_STUFF_ERROR = 1U, CANFD_MCANErrCode_FORM_ERROR = 2U, CANFD_MCANErrCode_ACK_ERROR = 3U,
  CANFD_MCANErrCode_BIT1_ERROR = 4U, CANFD_MCANErrCode_BIT0_ERROR = 5U, CANFD_MCANErrCode_CRC_ERROR = 6U, CANFD_MCANErrCode_NO_CHANGE = 7U
}
 
CANFD reason

This enumeration describes a list of all the reasons for which the driver will invoke application callback functions.

enum  CANFD_Reason {
  CANFD_Reason_RX = 0x1, CANFD_Reason_TX_COMPLETION = 0x2, CANFD_Reason_TX_CANCELED = 0x3, CANFD_Reason_ECC_ERROR = 0x4,
  CANFD_Reason_BUSOFF = 0x5, CANFD_Reason_PROTOCOL_ERR_DATA_PHASE = 0x6, CANFD_Reason_PROTOCOL_ERR_ARB_PHASE = 0x7, CANFD_Reason_SRC_RX_FIFO0_MSG_LOST = 0x8,
  CANFD_Reason_SRC_RX_FIFO1_MSG_LOST = 0x9
}
 
CANFD Option

This enumeration defines the values used to represent the GET/SET options

See also
CANFD_OptionTLV
enum  CANFD_Option {
  CANFD_Option_MCAN_ERROR_COUNTER, CANFD_Option_MCAN_PROTOCOL_STATUS, CANFD_Option_MCAN_MSG_OBJECT_STATS, CANFD_Option_MCAN_MODE,
  CANFD_Option_MCAN_LOOPBACK, CANFD_Option_MCAN_POWER_DOWN
}
 

Functions

CANFD Dma Config

CANFD DMA Configuration, these are filled by SysCfg based on the DMA driver(EDMA/UDMA) that is selected

void CANFD_init (void)
 This function initializes each driver instance object and create a driver lock. More...
 
void CANFD_deinit (void)
 This function de-initializes each driver instance object and delete a driver lock. More...
 
CANFD_Handle CANFD_open (uint32_t index, CANFD_OpenParams *openPrms)
 This function opens a given CANFD peripheral. More...
 
void CANFD_close (CANFD_Handle handle)
 Function to close a CANFD peripheral specified by the CANFD handle. More...
 
int32_t CANFD_configBitTime (CANFD_Handle handle, const CANFD_MCANBitTimingParams *bitTimeParams)
 Function configures the bit time parameters for the CANFD module. More...
 
int32_t CANFD_createMsgObject (CANFD_Handle handle, CANFD_MessageObject *ptrCanMsgObj)
 Function configures the receive or transmit message object. It also enables Tx completion and Tx cancelation interrupts. The callback function will be invoked on data transmit complete for transmit message objects OR upon receiving data for receive message objects. The application MUST then call CANFD_read() API to process the received data. More...
 
int32_t CANFD_createRxRangeMsgObject (CANFD_Handle handle, CANFD_MessageObject *ptrCanMsgObj)
 Function configures a receive message objects for a range of message identifiers. It also enables Rx interrupts. The callback function will be invoked upon receiving data for receive message objects. The application MUST then call CANFD_read() API to process the received data. More...
 
int32_t CANFD_deleteMsgObject (CANFD_MsgObjHandle handle)
 Function deletes a message object. More...
 
int32_t CANFD_write (CANFD_MsgObjHandle handle, uint32_t id, CANFD_MCANFrameType frameType, uint32_t numMsgs, const uint8_t *data)
 Function used by the application to transmit data. More...
 
int32_t CANFD_writeCancel (CANFD_MsgObjHandle handle)
 Function used by the application to cancel a pending data transmit. More...
 
int32_t CANFD_writeDma (CANFD_MsgObjHandle handle, uint32_t id, CANFD_MCANFrameType frameType, uint32_t numMsgs, const void *data)
 Function used by the application to initiate transmit data in dma mode. DMA mode is recommended to be used when multiple msgs needs to be transmitted. This will transmit first msg and configure the dma to copy subsequent msgs in message ram. Once first msg transfer is completed the CANFD_dmaTxCompletionCallback function is called. Application needs to call the API CANFD_writeDmaTriggerNext to trigger transmission of subsequent msgs. More...
 
int32_t CANFD_writeDmaTriggerNext (CANFD_MsgObjHandle handle)
 Function used by the application to start transmission of next msg in dma mode. Transfer should be initiated using the API CANFD_writeDma before calling this function. This should be called after the previous transfer is completed and CANFD_dmaTxCompletionCallback is called. More...
 
uint32_t CANFD_getFilterEventConfig (uint32_t eventNum)
 
int32_t CANFD_read (CANFD_MsgObjHandle rxMsgHandle, uint32_t numMsgs, uint8_t *data)
 Function is used by the application to get the CAN message from message RAM using a receive message object. NOTE: This API must ONLY be called from the callback context. Function is used by the application to get the CAN message from message RAM using a receive message object. More...
 
int32_t CANFD_readDmaConfig (CANFD_MsgObjHandle handle, const void *data, uint32_t numMsgs)
 Function is used by the application to configure reading the received msgs from message ram. This API will configure the DMA to copy msg from MCAN message ram to application buffer. For every message received the CANFD_dmaRxCompletionCallback will be called by driver by pointing to the latest msg in the data buffer. More...
 
int32_t CANFD_getOptions (CANFD_Handle handle, const CANFD_OptionTLV *ptrOptInfo)
 Function is used by the application to get the error and status information from the driver. More...
 
int32_t CANFD_setOptions (CANFD_Handle handle, const CANFD_OptionTLV *ptrOptInfo)
 Function is used by the application to configure the driver options. More...
 
void CANFD_int0Isr (void *args)
 The function is the registered interrupt 0 ISR for the CANFD Driver. More...
 
void CANFD_int1Isr (void *args)
 The function is the registered interrupt 1 ISR for the CANFD Driver. More...
 
void CANFD_transferCallBack (void *args, CANFD_Reason reason)
 Application specified callback function which is invoked by the CANFD driver once transmit is complete or data has been received for the specified message object. More...
 
void CANFD_errStatusCallBack (CANFD_Handle handle, CANFD_Reason reason, CANFD_ErrStatusResp *errStatusResp)
 Application specified callback function which is invoked by the CANFD driver on error or status change. More...
 
int32_t CANFD_dmaOpen (CANFD_Handle canfdHandle, CANFD_DmaChConfig dmaChCfg)
 API to open an CANFD DMA channel. More...
 
int32_t CANFD_dmaClose (CANFD_Handle canfdHandle)
 API to close an CANFD DMA channel. More...
 
int32_t CANFD_createDmaTxMsgObject (const CANFD_Object *ptrCanFdObj, CANFD_MessageObject *ptrCanMsgObj)
 API to configure dma for the Tx message object. Called from the API CANFD_createMsgObject. More...
 
int32_t CANFD_deleteDmaTxMsgObject (const CANFD_Object *ptrCanFdObj, const CANFD_MessageObject *ptrCanMsgObj)
 API to delete dma configuration for the Tx message object. Called from the API CANFD_deleteMsgObject. More...
 
int32_t CANFD_configureDmaTx (const CANFD_Object *ptrCanFdObj, CANFD_MessageObject *ptrCanMsgObj, uint32_t dataLengthPerMsg, uint32_t numMsgs, const void *data)
 API to enable dma event transfer for the Tx. Called from the API CANFD_writeDma. More...
 
int32_t CANFD_cancelDmaTx (const CANFD_Object *ptrCanFdObj, const CANFD_MessageObject *ptrCanMsgObj)
 API to disbale dma event transfer for the Tx to cancel the transfer. More...
 
void CANFD_dmaTxCompletionCallback (CANFD_MessageObject *ptrCanMsgObj, const void *data, uint32_t completionType)
 Callback function for the Tx completion. This is called for each message in the array of msgs provided in CANFD_configureDmaTx. Data will point to the current transmitted message. For intermediate message transfer completion the completionType will be set to CANFD_DMA_TX_COMPLETION_INTERMEDIATE for last message transfer completion the completionType will be set to CANFD_DMA_TX_COMPLETION_FINAL. More...
 
int32_t CANFD_createDmaRxMsgObject (const CANFD_Object *ptrCanFdObj, CANFD_MessageObject *ptrCanMsgObj)
 API to configure dma for the Rx message object. Called from the CANFD_createMsgObject. More...
 
int32_t CANFD_deleteDmaRxMsgObject (const CANFD_Object *ptrCanFdObj, const CANFD_MessageObject *ptrCanMsgObj)
 API to delete dma configuration for the Rx message object. Called from the CANFD_deleteMsgObject. More...
 
int32_t CANFD_configureDmaRx (const CANFD_Object *ptrCanFdObj, CANFD_MessageObject *ptrCanMsgObj, uint32_t dataLengthPerMsg, uint32_t numMsgs, const void *data)
 API to enable dma event transfer for the Rx. Called from the API CANFD_readDma. More...
 
void CANFD_dmaRxCompletionCallback (CANFD_MessageObject *ptrCanMsgObj, const void *data, uint32_t completionType)
 Callback function for the Rx completion. This is called for each message in the array of msgs provided in CANFD_configureDmaRx. Data will point to the current received message. For intermediate message transfer completion the completionType will be set to CANFD_DMA_RX_COMPLETION_INTERMEDIATE for last message transfer completion the completionType will be set to CANFD_DMA_RX_COMPLETION_FINAL. More...
 
int32_t CANFD_isDataSizeValid (uint32_t dataSize)
 Function to validate the data Size. More...
 
int32_t CANFD_getEndianVal (CANFD_Handle canfdHandle)
 This function return endianness value of MCAN module. More...
 
void CANFD_getRevisionId (CANFD_Handle canfdHandle)
 This API is used get the MCAN revision ID. More...
 
void CANFD_addClockStopRequest (CANFD_Handle canfdHandle, uint32_t enable)
 This API add clock stop request for MCAN module to put it in power down mode. More...
 
uint32_t CANFD_clockStopReq (CANFD_Handle canfdHandle)
 This API get clock stop acknowledgement for MCAN module. It return whether MCAN is power down mode or not. More...
 
uint32_t CANFD_getClkStopAck (CANFD_Handle canfdHandle)
 This API will return clock stop acknowledgement for MCAN module. More...
 
uint32_t CANFD_getRxPinState (CANFD_Handle canfdHandle)
 This API will return Rx pin state of MCAN module. More...
 
void CANFD_setTxPinState (CANFD_Handle canfdHandle, uint32_t state)
 This API will set Tx pin state of MCAN module. More...
 
uint32_t CANFD_getTxPinState (CANFD_Handle canfdHandle)
 This API will return Tx pin state of MCAN module. More...
 
void CANFD_getBitTime (CANFD_Handle canfdHandle)
 This API will get the configured bit timings for MCAN module. More...
 
uint32_t CANFD_getTSCounterVal (CANFD_Handle canfdHandle)
 This API will return current timestamp counter value. More...
 
void CANFD_resetTSCounter (CANFD_Handle canfdHandle)
 This API will reset timestamp counter value. More...