AM263Px MCU+ SDK  11.01.00
CANFD_MCANECCErrForceParams Struct Reference

Data Fields

uint32_t errType
 
uint32_t rowNum
 
uint32_t bit1
 
uint32_t bit2
 
uint32_t errOnce
 
uint32_t errForce
 

Field Documentation

◆ errType

uint32_t CANFD_MCANECCErrForceParams::errType

Error type to be forced Refer enum CANFD_MCANECCErrType.

◆ rowNum

uint32_t CANFD_MCANECCErrForceParams::rowNum

Row address where error needs to be applied.

◆ bit1

uint32_t CANFD_MCANECCErrForceParams::bit1

Column/Data bit that needs to be flipped when force_sec or force_ded is set

◆ bit2

uint32_t CANFD_MCANECCErrForceParams::bit2

Data bit that needs to be flipped when force_ded is set

◆ errOnce

uint32_t CANFD_MCANECCErrForceParams::errOnce

Force Error once 1: The error will inject an error to the specified row only once

◆ errForce

uint32_t CANFD_MCANECCErrForceParams::errForce

Force error on the next RAM read