MCSPI LLD Driver API/interface file.
Go to the source code of this file.
Data Structures | |
struct | MCSPI_Transaction |
Data structure used with MCSPI_transfer() More... | |
struct | MCSPI_ExtendedParams |
Data structure used with MCSPI_lld_read(), MCSPI_lld_readIntr(), MCSPI_lld_readDma(), MCSPI_lld_write(), MCSPI_lld_writeIntr, MCSPI_lld_writeDma, MCSPI_lld_readWrite(), MCSPI_lld_readWriteIntr(), MCSPI_lld_readWriteDma(). More... | |
struct | MCSPI_ChConfig |
MCSPI configuration parameters for the channel. More... | |
struct | MCSPI_ChObject |
MCSPI channel object. More... | |
struct | MCSPILLD_InitObject |
MCSPI driver initialization object. More... | |
struct | MCSPILLD_Object |
MCSPI driver object. More... | |
Macros | |
#define | MCSPI_MAX_NUM_CHANNELS (4U) |
Max number of channels/Chip Select (CS) supported. More... | |
#define | MCSPI_ERROR_TX_UNDERFLOW (0x00000001U) |
McSPI error macro's. More... | |
#define | MCSPI_ERROR_RX_OVERFLOW (0x00000002U) |
#define | MCSPI_FIFO_LENGTH (64U) |
Total length of FIFO for both TX/RX. More... | |
#define | MCSPI_RX_FIFO_ENABLE |
McSPI peripheral Rx FIFO is enabled. More... | |
#define | MCSPI_RX_FIFO_DISABLE |
McSPI peripheral Rx FIFO is disabled. More... | |
#define | MCSPI_TX_FIFO_ENABLE |
McSPI peripheral Tx FIFO is enabled. More... | |
#define | MCSPI_TX_FIFO_DISABLE |
McSPI peripheral Tx FIFO is disabled. More... | |
#define | MCSPI_REG_OFFSET (0x14U) |
McSPI Register Offset for MCSPI_CHxCONF, MCSPI_CHxSTAT, MCSPI_CHxCTRL, MCSPI_TXx and MCSPI_RXx register set. More... | |
#define | MCSPI_CHCONF(x) |
Base address of McSPI_CHCONF(x) More... | |
#define | MCSPI_CHSTAT(x) |
Base address of McSPI_CHSTAT(x) More... | |
#define | MCSPI_CHCTRL(x) |
Base address of McSPI_CHCTRL(x) More... | |
#define | MCSPI_CHTX(x) |
Base address of McSPI_CHTX(x) More... | |
#define | MCSPI_CHRX(x) |
Base address of McSPI_CHRX(x) More... | |
#define | MCSPI_CLKD_MASK (0x0FU) |
#define | MCSPI_IRQSTATUS_CLEAR_ALL |
Bit mask to clear all status bits. More... | |
Return status | |
#define | MCSPI_STATUS_SUCCESS ((int32_t)0) |
Return status when the API execution was successful. More... | |
#define | MCSPI_STATUS_FAILURE ((int32_t)-1) |
Return status when the API execution was not successful due to a failure. More... | |
#define | MCSPI_TIMEOUT ((int32_t)-2) |
Return status when the API execution was not successful due to a time out. More... | |
#define | MCSPI_INVALID_PARAM ((int32_t)-3) |
Return status when the API execution failed due invalid parameters. More... | |
#define | MCSPI_STATUS_BUSY ((int32_t)-4) |
Return status when the API execution failed due to driver busy. More... | |
#define | MCSPI_INVALID_STATE ((int32_t)-5) |
Return status when the API execution failed due to invalid state. More... | |
Timeout values | |
#define | MCSPI_NO_WAIT ((uint32_t)0) |
Value to use when needing a timeout of zero or NO timeout, return immediately on resource not available. More... | |
#define | MCSPI_WAIT_FOREVER ((uint32_t)-1) |
Value to use when needing a timeout of infinity or wait forver until resource is available. More... | |
MCSPI Driver states | |
#define | MCSPI_STATE_RESET ((uint32_t)0U) |
MCSPI driver is in Reset State prior to driver init and post driver deinit. More... | |
#define | MCSPI_STATE_READY ((uint32_t)1U) |
MCSPI driver accepts runtime APIs only Ready State, otherwise return error. More... | |
#define | MCSPI_STATE_BUSY ((uint32_t)2U) |
MCSPI driver is busy performing operation with peripherals, return error when APIs are invoked. More... | |
#define | MCSPI_STATE_ERROR ((uint32_t)3U) |
MCSPI driver ran into error, returns error for all APIs other than deinit in this state. More... | |
Channel Id | |
#define | MCSPI_CHANNEL_0 (0U) |
#define | MCSPI_CHANNEL_1 (1U) |
#define | MCSPI_CHANNEL_2 (2U) |
#define | MCSPI_CHANNEL_3 (3U) |
Operating Mode | |
#define | MCSPI_OPER_MODE_POLLED (0U) |
#define | MCSPI_OPER_MODE_INTERRUPT (1U) |
#define | MCSPI_OPER_MODE_DMA (2U) |
Transfer Status Code | |
#define | MCSPI_TRANSFER_COMPLETED ((int32_t)0U) |
#define | MCSPI_TRANSFER_STARTED ((int32_t)1U) |
#define | MCSPI_TRANSFER_CANCELLED ((int32_t)2U) |
#define | MCSPI_TRANSFER_FAILED ((int32_t)3U) |
#define | MCSPI_TRANSFER_CSN_DEASSERT ((int32_t)4U) |
#define | MCSPI_TRANSFER_TIMEOUT ((int32_t)5U) |
Modes of Operation | |
Definitions for various MCSPI modes of operation The MCSPI driver operates in both controller and SPI peripheral modes. Logically, the implementation is identical, however the difference between these two modes is driven by hardware. The default mode is MCSPI_MS_MODE_CONTROLLER, but can be set to peripheral mode by setting MCSPI_OpenParams.msMode to MCSPI_MS_MODE_PERIPHERAL in the parameters passed to MCSPI_open(). | |
#define | MCSPI_MS_MODE_CONTROLLER (CSL_MCSPI_MODULCTRL_MS_MASTER) |
The module generates the clock and CS. More... | |
#define | MCSPI_MS_MODE_PERIPHERAL (CSL_MCSPI_MODULCTRL_MS_SLAVE) |
The module receives the clock and CS. More... | |
Frame Format | |
#define | MCSPI_FF_POL0_PHA0 (0U) |
#define | MCSPI_FF_POL0_PHA1 (1U) |
#define | MCSPI_FF_POL1_PHA0 (2U) |
#define | MCSPI_FF_POL1_PHA1 (3U) |
Chip-select Polarity | |
#define | MCSPI_CS_POL_HIGH (CSL_MCSPI_CH0CONF_EPOL_ACTIVEHIGH) |
SPIEN (CS) is held high during the ACTIVE state. More... | |
#define | MCSPI_CS_POL_LOW (CSL_MCSPI_CH0CONF_EPOL_ACTIVELOW) |
SPIEN (CS) is held low during the ACTIVE state. More... | |
Transmit-Receive Modes | |
#define | MCSPI_TR_MODE_TX_RX (CSL_MCSPI_CH0CONF_TRM_TRANSRECEI) |
#define | MCSPI_TR_MODE_RX_ONLY (CSL_MCSPI_CH0CONF_TRM_RECEIVONLY) |
#define | MCSPI_TR_MODE_TX_ONLY (CSL_MCSPI_CH0CONF_TRM_TRANSONLY) |
Input Select | |
#define | MCSPI_IS_D0 (CSL_MCSPI_CH0CONF_IS_LINE0) |
Data line 0 (SPIDAT[0]) selected for reception. More... | |
#define | MCSPI_IS_D1 (CSL_MCSPI_CH0CONF_IS_LINE1) |
Data line 1 (SPIDAT[1]) selected for reception. More... | |
Transmission Enable for Data Line | |
#define | MCSPI_DPE_ENABLE (CSL_MCSPI_CH0CONF_DPE0_ENABLED) |
Data line selected for transmission. More... | |
#define | MCSPI_DPE_DISABLE (CSL_MCSPI_CH0CONF_DPE0_DISABLED) |
No transmission on Data Line. More... | |
Peripheral Chip-select Signal Select | |
#define | MCSPI_SLV_CS_SELECT_0 (CSL_MCSPI_CH0CONF_SPIENSLV_SPIEN0) |
#define | MCSPI_SLV_CS_SELECT_1 (CSL_MCSPI_CH0CONF_SPIENSLV_SPIEN1) |
#define | MCSPI_SLV_CS_SELECT_2 (CSL_MCSPI_CH0CONF_SPIENSLV_SPIEN2) |
#define | MCSPI_SLV_CS_SELECT_3 (CSL_MCSPI_CH0CONF_SPIENSLV_SPIEN3) |
Start-bit Polarity | |
#define | MCSPI_SB_POL_HIGH (CSL_MCSPI_CH0CONF_SBPOL_HIGHLEVEL) |
SStart-bit polarity is held to 1 during MCSPI transfer. More... | |
#define | MCSPI_SB_POL_LOW (CSL_MCSPI_CH0CONF_SBPOL_LOWLEVEL) |
Start-bit polarity is held to 0 during MCSPI transfer. More... | |
Chip-select Idle Time | |
#define | MCSPI_TCS0_0_CLK (CSL_MCSPI_CH0CONF_TCS0_ZEROCYCLEDLY) |
0.5 clock cycles delay More... | |
#define | MCSPI_TCS0_1_CLK (CSL_MCSPI_CH0CONF_TCS0_ONECYCLEDLY) |
1.5 clock cycles delay More... | |
#define | MCSPI_TCS0_2_CLK (CSL_MCSPI_CH0CONF_TCS0_TWOCYCLEDLY) |
2.5 clock cycles delay More... | |
#define | MCSPI_TCS0_3_CLK (CSL_MCSPI_CH0CONF_TCS0_THREECYCLEDLY) |
3.5 clock cycles delay More... | |
Channel Mode | |
#define | MCSPI_CH_MODE_SINGLE (CSL_MCSPI_MODULCTRL_SINGLE_SINGLE) |
Only one channel will be used in controller mode. This should be used when CS is used in forced enable mode. More... | |
#define | MCSPI_CH_MODE_MULTI (CSL_MCSPI_MODULCTRL_SINGLE_MULTI) |
More than one channel will be used in controller mode. More... | |
Pin Mode | |
#define | MCSPI_PINMODE_3PIN (CSL_MCSPI_MODULCTRL_PIN34_3PINMODE) |
SPIEN (CS) is not used. In this mode all related options to chip-select have no meaning. More... | |
#define | MCSPI_PINMODE_4PIN (CSL_MCSPI_MODULCTRL_PIN34_4PINMODE) |
Init Delay | |
#define | MCSPI_INITDLY_0 (CSL_MCSPI_MODULCTRL_INITDLY_NODELAY) |
No delay. More... | |
#define | MCSPI_INITDLY_4 (CSL_MCSPI_MODULCTRL_INITDLY_4CLKDLY) |
4 SPI bus clock delays More... | |
#define | MCSPI_INITDLY_8 (CSL_MCSPI_MODULCTRL_INITDLY_8CLKDLY) |
8 SPI bus clock delays More... | |
#define | MCSPI_INITDLY_16 (CSL_MCSPI_MODULCTRL_INITDLY_16CLKDLY) |
16 SPI bus clock delays More... | |
#define | MCSPI_INITDLY_32 (CSL_MCSPI_MODULCTRL_INITDLY_32CLKDLY) |
32 SPI bus clock delays More... | |
Typedefs | |
typedef void * | MCSPI_DmaHandle |
typedef void * | MCSPI_DmaChConfig |
typedef uint32_t(* | MCSPI_clockGet) (void) |
typedef void(* | MCSPI_transferCallbackFxn) (void *args, uint32_t tansferStatus) |
The definition of a transfer completion callback function used by the SPI driver when used in MCSPI_TRANSFER_MODE_CALLBACK. More... | |
typedef void(* | MCSPI_errorCallbackFxn) (void *args) |
The definition of a error callback function used by the SPI driver when used in MCSPI_TRANSFER_MODE_CALLBACK. More... | |
typedef struct MCSPILLD_InitObject * | MCSPILLD_InitHandle |
typedef struct MCSPILLD_Object * | MCSPILLD_Handle |
Functions | |
void | MCSPI_reset (uint32_t baseAddr) |
void | MCSPI_clearAllIrqStatus (uint32_t baseAddr) |
void | MCSPI_stop (MCSPILLD_Handle hMcspi, MCSPI_ChObject *chObj, uint32_t chNum) |
void | MCSPI_setChDataSize (uint32_t baseAddr, MCSPI_ChObject *chObj, uint32_t dataSize, uint32_t csDisable) |
static void | MCSPI_intrStatusClear (const MCSPI_ChObject *chObj, uint32_t baseAddr, uint32_t intFlags) |
int32_t | MCSPI_lld_init (MCSPILLD_Handle hMcspi) |
This API Initializes the McSPI instance. More... | |
int32_t | MCSPI_lld_initDma (MCSPILLD_Handle hMcspi) |
This API Initializes the McSPI instance in DMA Mode. More... | |
int32_t | MCSPI_lld_deInit (MCSPILLD_Handle hMcspi) |
This API De-Initializes the McSPI instance. More... | |
int32_t | MCSPI_lld_deInitDma (MCSPILLD_Handle hMcspi) |
This API De-Initializes the McSPI instance in DMA mode. More... | |
int32_t | MCSPI_lld_write (MCSPILLD_Handle hMcspi, void *txBuf, uint32_t count, uint32_t timeout, const MCSPI_ExtendedParams *extendedParams) |
This API writes data to the McSPI instance in Polling mode. More... | |
int32_t | MCSPI_lld_writeIntr (MCSPILLD_Handle hMcspi, void *txBuf, uint32_t count, uint32_t timeout, const MCSPI_ExtendedParams *extendedParams) |
This API writes data to the McSPI instance in Interrupt mode. More... | |
int32_t | MCSPI_lld_writeDma (MCSPILLD_Handle hMcspi, void *txBuf, uint32_t count, uint32_t timeout, const MCSPI_ExtendedParams *extendedParams) |
This API writes data to the McSPI instance in DMA mode. More... | |
int32_t | MCSPI_lld_read (MCSPILLD_Handle hMcspi, void *rxBuf, uint32_t count, uint32_t timeout, const MCSPI_ExtendedParams *extendedParams) |
This API reads data from the McSPI instance in Polling mode. More... | |
int32_t | MCSPI_lld_readIntr (MCSPILLD_Handle hMcspi, void *rxBuf, uint32_t count, uint32_t timeout, const MCSPI_ExtendedParams *extendedParams) |
This API reads data from the McSPI instance in Interrupt mode. More... | |
int32_t | MCSPI_lld_readDma (MCSPILLD_Handle hMcspi, void *rxBuf, uint32_t count, uint32_t timeout, const MCSPI_ExtendedParams *extendedParams) |
This API reads data from the McSPI instance in DMA mode. More... | |
int32_t | MCSPI_lld_readWrite (MCSPILLD_Handle hMcspi, void *txBuf, void *rxBuf, uint32_t count, uint32_t timeout, const MCSPI_ExtendedParams *extendedParams) |
This API reads writes data from the McSPI instance in polling mode. More... | |
int32_t | MCSPI_lld_readWriteIntr (MCSPILLD_Handle hMcspi, void *txBuf, void *rxBuf, uint32_t count, uint32_t timeout, const MCSPI_ExtendedParams *extendedParams) |
This API reads writes data from the McSPI instance in Interrupt mode. More... | |
int32_t | MCSPI_lld_readWriteDma (MCSPILLD_Handle hMcspi, void *txBuf, void *rxBuf, uint32_t count, uint32_t timeout, const MCSPI_ExtendedParams *extendedParams) |
This API reads writes data from the McSPI instance in DMA mode. More... | |
int32_t | MCSPI_lld_readWriteCancel (MCSPILLD_Handle hMcspi) |
This API cancels current McSPI transfer. More... | |
int32_t | MCSPI_lld_readWriteDmaCancel (MCSPILLD_Handle hMcspi) |
This API cancels current McSPI transfer in DMA mode. More... | |
int32_t | MCSPI_lld_transfer (MCSPILLD_Handle hMcspi, MCSPI_Transaction *transaction) |
This API transfers data from the McSPI instance in Polling mode. More... | |
int32_t | MCSPI_lld_transferIntr (MCSPILLD_Handle hMcspi, MCSPI_Transaction *transaction) |
This API reads data from the McSPI instance in Interrupt mode. More... | |
int32_t | MCSPI_lld_transferDma (MCSPILLD_Handle hMcspi, MCSPI_Transaction *transaction) |
This API reads data from the McSPI instance in DMA mode. More... | |
void | MCSPI_lld_controllerIsr (void *args) |
This is the McSPI Controller ISR and can be used as IRQ handler in Controller mode. More... | |
void | MCSPI_lld_peripheralIsr (void *args) |
This is the McSPI Peripheral ISR and can be used as IRQ handler in Peripheral mode. More... | |
int32_t | MCSPI_lld_getState (MCSPILLD_Handle hMcspi) |
This API returns the driver state. More... | |
int32_t | MCSPI_lld_transferCancel (MCSPILLD_Handle hMcspi) |
This API cancels current McSPI transfer. More... | |
int32_t | MCSPI_lld_transferDmaCancel (MCSPILLD_Handle hMcspi) |
This API cancels current McSPI transfer in DMA mode. More... | |
static void | MCSPI_lld_ChConfig_init (MCSPI_ChConfig *chConfig) |
Function to initialize the MCSPI_ChConfig struct to its defaults. More... | |
static void | MCSPI_lld_Transaction_init (MCSPI_Transaction *trans) |
Function to initialize the MCSPI_Transaction struct to its defaults. More... | |
uint32_t | MCSPI_lld_getBaseAddr (MCSPILLD_Handle handle) |
Function to get base address of MCSPI instance of a particular handle. More... | |
int32_t | MCSPI_lld_reConfigFifo (MCSPILLD_Handle handle, uint32_t chNum, uint32_t numWordsRxTx) |
Function to re-configure Effective FIFO Words. More... | |
static uint8_t | MCSPI_getBufWidthShift (uint32_t dataSize) |
This API will return the buffer width in bytes based on dataSize. More... | |
static uint32_t | MCSPI_readChStatusReg (uint32_t baseAddr, uint32_t chNum) |
This API will return the status of the McSPI channel currently in use. More... | |
static uint32_t | MCSPI_readChCtrlReg (uint32_t baseAddr, uint32_t chNum) |
This API returns Channel control register value. More... | |
static void | MCSPI_writeChCtrlReg (uint32_t baseAddr, uint32_t chNum, uint32_t regVal) |
This API sets Channel control register value. More... | |
static uint32_t | MCSPI_readChConf (uint32_t baseAddr, uint32_t chNum) |
This API returns Channel Config register value. More... | |
static void | MCSPI_writeChConfReg (uint32_t baseAddr, uint32_t chNum, uint32_t regVal) |
This API sets Channel Config register value. More... | |
static void | MCSPI_writeTxDataReg (uint32_t baseAddr, uint32_t txData, uint32_t chNum) |
This API will put the data on to the McSPI Channel transmit register. More... | |
static void | MCSPI_enableTxFIFO (uint32_t baseAddr, uint32_t chNum, uint32_t enableFlag) |
This API will enable/disable the Tx FIFOs of McSPI peripheral. More... | |
static void | MCSPI_enableRxFIFO (uint32_t baseAddr, uint32_t chNum, uint32_t enableFlag) |
This API will enable/disable the Rx FIFOs of McSPI peripheral. More... | |
static uint32_t | MCSPI_readRxDataReg (uint32_t baseAddr, uint32_t chNum) |
This API will return the data present in the MCSPI_RX register. More... | |
static void | MCSPI_setDataWidth (uint32_t baseAddr, uint32_t chNum, uint32_t dataWidth) |
This API will set the data width in the channel config register. More... | |