This module contains APIs to program and use the MCSPI module. The APIs can be used by other drivers to get access to MCSPI and also by application to initiate data transfer operation.
Files | |
file | mcspi/v0/mcspi.h |
MCSPI Driver API/interface file. | |
Data Structures | |
struct | MCSPI_OpenParams |
MCSPI Parameters. More... | |
struct | MCSPI_Attrs |
MCSPI instance attributes - used during init time. More... | |
struct | MCSPI_Object |
MCSPI driver object. More... | |
struct | MCSPI_Config |
MCSPI global configuration array. More... | |
Typedefs | |
typedef void * | MCSPI_Handle |
A handle that is returned from a MCSPI_open() call. More... | |
Transfer Mode | |
This determines whether the driver operates synchronously or asynchronously In MCSPI_TRANSFER_MODE_BLOCKING mode MCSPI_transfer() blocks code execution until the transaction has completed In MCSPI_TRANSFER_MODE_CALLBACK MCSPI_transfer() does not block code execution and instead calls a MCSPI_CallbackFxn callback function when the transaction has completed | |
typedef void(* | MCSPI_CallbackFxn) (MCSPI_Handle handle, MCSPI_Transaction *transaction) |
The definition of a callback function used by the SPI driver when used in MCSPI_TRANSFER_MODE_CALLBACK. More... | |
void | MCSPI_init (void) |
This function initializes the MCSPI module. More... | |
void | MCSPI_deinit (void) |
This function de-initializes the MCSPI module. More... | |
MCSPI_Handle | MCSPI_open (uint32_t index, const MCSPI_OpenParams *openPrms) |
This function opens a given MCSPI peripheral. More... | |
void | MCSPI_close (MCSPI_Handle handle) |
Function to close a MCSPI peripheral specified by the MCSPI handle. More... | |
MCSPI_Handle | MCSPI_getHandle (uint32_t index) |
Function to return a open'ed MCSPI handle given a MCSPI instance index. More... | |
int32_t | MCSPI_chConfig (MCSPI_Handle handle, const MCSPI_ChConfig *chCfg) |
Function to configure a MCSPI channel. More... | |
int32_t | MCSPI_dmaChConfig (MCSPI_Handle handle, const MCSPI_ChConfig *chCfg, const MCSPI_DmaChConfig *dmaChCfg) |
Function to configure a DMA of a channel. More... | |
int32_t | MCSPI_transfer (MCSPI_Handle handle, MCSPI_Transaction *transaction) |
Function to perform MCSPI transactions. More... | |
int32_t | MCSPI_transferCancel (MCSPI_Handle handle) |
Function to cancel MCSPI transactions on channel of a SPI peripheral specified by the MCSPI handle. More... | |
static void | MCSPI_OpenParams_init (MCSPI_OpenParams *openPrms) |
Function to initialize the MCSPI_OpenParams struct to its defaults. More... | |
static void | MCSPI_ChConfig_init (MCSPI_ChConfig *chConfig) |
Function to initialize the MCSPI_ChConfig struct to its defaults. More... | |
static void | MCSPI_Transaction_init (MCSPI_Transaction *trans) |
Function to initialize the MCSPI_Transaction struct to its defaults. More... | |
int32_t | MCSPI_reConfigFifo (MCSPI_Handle handle, uint32_t chNum, uint32_t numWordsRxTx) |
Function to re-configure Effective FIFO Words. More... | |
uint32_t | MCSPI_getBaseAddr (MCSPI_Handle handle) |
Function to get base address of MCSPI instance of a particular handle. More... | |
#define | MCSPI_TRANSFER_MODE_BLOCKING (0U) |
MCSPI_transfer() blocks execution. This mode can only be used when called within a Task context More... | |
#define | MCSPI_TRANSFER_MODE_CALLBACK (1U) |
MCSPI_transfer() does not block code execution and will call a MCSPI_CallbackFxn. This mode can be used in a Task, Swi, or Hwi context More... | |
#define MCSPI_TRANSFER_MODE_BLOCKING (0U) |
MCSPI_transfer() blocks execution. This mode can only be used when called within a Task context
#define MCSPI_TRANSFER_MODE_CALLBACK (1U) |
MCSPI_transfer() does not block code execution and will call a MCSPI_CallbackFxn. This mode can be used in a Task, Swi, or Hwi context
typedef void* MCSPI_Handle |
A handle that is returned from a MCSPI_open() call.
typedef void(* MCSPI_CallbackFxn) (MCSPI_Handle handle, MCSPI_Transaction *transaction) |
The definition of a callback function used by the SPI driver when used in MCSPI_TRANSFER_MODE_CALLBACK.
MCSPI_Handle | MCSPI_Handle |
MCSPI_Transaction* | Pointer to a MCSPI_Transaction |
void MCSPI_init | ( | void | ) |
This function initializes the MCSPI module.
void MCSPI_deinit | ( | void | ) |
This function de-initializes the MCSPI module.
MCSPI_Handle MCSPI_open | ( | uint32_t | index, |
const MCSPI_OpenParams * | openPrms | ||
) |
This function opens a given MCSPI peripheral.
index | Index of config to use in the MCSPI_Config array |
openPrms | Pointer to open parameters. If NULL is passed, then default values will be used |
void MCSPI_close | ( | MCSPI_Handle | handle | ) |
Function to close a MCSPI peripheral specified by the MCSPI handle.
handle | MCSPI_Handle returned from MCSPI_open() |
MCSPI_Handle MCSPI_getHandle | ( | uint32_t | index | ) |
Function to return a open'ed MCSPI handle given a MCSPI instance index.
index | Index of config to use in the MCSPI_Config array |
int32_t MCSPI_chConfig | ( | MCSPI_Handle | handle, |
const MCSPI_ChConfig * | chCfg | ||
) |
Function to configure a MCSPI channel.
handle | MCSPI_Handle returned from MCSPI_open() |
chCfg | Pointer to MCSPI_ChConfig. This parameter can't be NULL |
int32_t MCSPI_dmaChConfig | ( | MCSPI_Handle | handle, |
const MCSPI_ChConfig * | chCfg, | ||
const MCSPI_DmaChConfig * | dmaChCfg | ||
) |
Function to configure a DMA of a channel.
handle | MCSPI_Handle returned from MCSPI_open() |
chCfg | Pointer to MCSPI_ChConfig. This parameter can't be NULL |
dmaChCfg | Pointer to MCSPI_DmaChConfig. This parameter can't be NULL |
int32_t MCSPI_transfer | ( | MCSPI_Handle | handle, |
MCSPI_Transaction * | transaction | ||
) |
Function to perform MCSPI transactions.
If the MCSPI is in MCSPI_MS_MODE_CONTROLLER mode, it will immediately start the transaction. If the MCSPI is in MCSPI_MS_MODE_PERIPHERAL mode, it prepares the driver for a transaction with a MCSPI controller device. The device will then wait until the controller begins the transfer.
In MCSPI_TRANSFER_MODE_BLOCKING, MCSPI_transfer() will block task execution until the transaction has completed or a timeout has occurred.
In MCSPI_TRANSFER_MODE_CALLBACK, MCSPI_transfer() does not block task execution, but calls a MCSPI_CallbackFxn once the transfer has finished. This makes MCSPI_transfer() safe to be used within a Task, software or hardware interrupt context.
From calling MCSPI_transfer() until transfer completion, the MCSPI_Transaction structure must stay persistent and must not be altered by application code. It is also forbidden to modify the content of the MCSPI_Transaction.txBuf during a transaction, even though the physical transfer might not have started yet. Doing this can result in data corruption. This is especially important for peripheral operations where MCSPI_transfer() might be called a long time before the actual data transfer begins.
handle | MCSPI_Handle returned from MCSPI_open() |
transaction | Pointer to a MCSPI_Transaction. All of the fields within transaction except MCSPI_Transaction.count and MCSPI_Transaction.status are WO (write-only) unless otherwise noted in the driver implementations. If a transaction timeout has occurred, MCSPI_Transaction.count will contain the number of frames that were transferred. Neither is it allowed to modify the transaction object nor the content of MCSPI_Transaction.txBuf until the transfer has completed |
int32_t MCSPI_transferCancel | ( | MCSPI_Handle | handle | ) |
Function to cancel MCSPI transactions on channel of a SPI peripheral specified by the MCSPI handle.
In MCSPI_TRANSFER_MODE_BLOCKING, MCSPI_transferCancel has no effect.
In MCSPI_TRANSFER_MODE_CALLBACK, MCSPI_transferCancel() will stop an MCSPI transfer if one is in progress. If a transaction was in progress, its callback function will be called in context from which this API is called from. The MCSPI_CallbackFxn function can determine if the transaction was successful or not by reading the MCSPI_TransferStatus status value in the MCSPI_Transaction structure.
handle | MCSPI_Handle returned from MCSPI_open() |
|
inlinestatic |
Function to initialize the MCSPI_OpenParams struct to its defaults.
openPrms | Pointer to MCSPI_OpenParams structure for initialization |
|
inlinestatic |
Function to initialize the MCSPI_ChConfig struct to its defaults.
chConfig | Pointer to MCSPI_ChConfig structure for initialization |
|
inlinestatic |
Function to initialize the MCSPI_Transaction struct to its defaults.
trans | Pointer to MCSPI_Transaction structure for initialization |
int32_t MCSPI_reConfigFifo | ( | MCSPI_Handle | handle, |
uint32_t | chNum, | ||
uint32_t | numWordsRxTx | ||
) |
Function to re-configure Effective FIFO Words.
handle | MCSPI_Handle returned from MCSPI_open() |
chNum | Channel used for communication. |
numWordsRxTx | Number of words to transfer |
uint32_t MCSPI_getBaseAddr | ( | MCSPI_Handle | handle | ) |
Function to get base address of MCSPI instance of a particular handle.
handle | MCSPI_Handle returned from MCSPI_open() |