AM261x MCU+ SDK  26.00.00
USB NCM Example

Introduction

  • This examples demonstrates the use of TinyUSB NCM DEV Class driver. Its implements all the necessary callbacks that are required by TinyUSB NCM DEV class driver.
  • Network Control Model (NCM) is a USB standard protocol that facilitates the transfer of Ethernet frames over a USB connection, enabling devices to function as network adapters. For more details, refer to the NCM Specification.

    NCM Example Block diagram
  • This example integrates LWIP HTTPD webserver running on r5fss0-0 core with TinyUSB NCM class dirver. The class driver's job is to collect the ethernet frames comming over USB and forward it to the Lwip web server and vice versa.
Note
In this example we receive one ethernet packet at a time from NCM class driver and forward it to Lwip webeserver. This is a simplified design to demonstrate the use of NCM net class driver thus to achive better throughput, further optimizations are required.
  • This example also implements a DHCP server which will provide a static ip address to HTTPD web server.Moreover it allocates ip address to the NCM Host PC as well.
  • Refer Enet LwIP HTTP Server On Bare Metal (No-RTOS) to know more about http web server using lwip( TCP/IP) stack.
  • Once NCM device enumearation is successful, AM261x-LP will be recognised as a separate network interface. The Network interface driver on the Host side will convert and transfer the ethernet traffic Via USB bus as per NCM protocol specification.
  • To enable USB Logging for this example refer USB CDC Echo Example

Supported Combinations

Parameter Value
CPU + OS r5fss0-0_nortos
r5fss0-0_freertos
Toolchain ti-arm-clang
iar-arm
Boards am261x-som, am261x-lp
Example folder examples/usb/device/ncm

Steps to Run the Example

Build the example

HW Setup

AM261x-LP

  • To test the application, one can use a Windows/Linux PC as a USB host.
  • Connect the J10 on AM261x-LP to the USB host.

USB Micro B Device Connector

AM261X-SOM

  • To test the application, one can use a Windows/Linux PC as a USB host
  • Connect the J7 on AM261x SOM to the USB host

USB Micro B Device Connector

Run the example

  • Launch a CCS or IAR EW debug session and run the executable, see CCS Launch, Load and Run or IAR Launch, Load and Run
  • When application is running observe that ncm network device is detected by HOST PC ( Windows/linux)
  • If the enumeration is successful the following should be displayed on console.

Windows

  • Open command prompt and execute ipconfig. User should see a new network interface detected.

NCM Device Enumeration log
Note
  • NCM Windows driver might be readily available. Follow link to download and install the NCM host class driver for windows.

Linux

  • Open terminal and execute dmesg command. User should see a new network interface over USB detected.

NCM Device Enumeration log.

NCM Download

Note
  • Note that this IP address to host PC and device running lwip webserver will be provided by the dhcp server running along with lwip httpd. Refer Introduction

When the http get request will be successful, following HTML page will be display.

HTTP Get request via USB( NCM ) successful

See Also

USB