AM261x MCU+ SDK  26.00.00
CCS Launch, Load and Run

Note
The steps on this page should be done each time EVM is power cycled or when a new CCS session is started.
The screenshots shown are for AM263PX but can be similarly used for AM261X.

Prerequisites

A quick recap of the steps that need to have been done before you proceed

Launch CCS

Launch Target Configuration
Note
When debugging an application with SBL NULL, ensure the Target configuration is created without an Initialization script.
  • You will see the AM261X target configuration in the "Debug" window as shown below

Target Configuration After Launch

Load and run example binaries in CCS

  • POWER-ON the EVM
  • If you dont see the expected SOC initialization logs on UART or CCS console, then recheck your EVM Setup
  • Connect the target CPU of interest if not already connected. For the "hello world" example this is MAIN_Cortex_R5_0_0

Connect CPU
  • This should initialize the device and initialize R5 to be able to connect
    GEL Output
  • Reset the CPU

Reset CPU
  • Load program on the CPU


Load Program
  • When using makefiles to build,
    • In the "Load Program" dialog, select "Browse" and select the program from examples/{example folder}/{board}/{cpu}_{os}/{compiler} as shown below for the "hello world" program.

Select Program for Makefile Build
  • When using CCS projects,
    • In the "Load Program" dialog, select "Workspace", select the project and then select the program as shown below,


Select Program for CCS Projects Build


Select the Program from CCS Project
  • After the program is loaded, you will see the program is halted at "main" as shown below

Program at main()
  • Depending on the example you are running, you may need to load more programs on other CPUs for the example to work as expected. Typically, this is needed for multi-core interprocessor communication (IPC) examples. For the "hello world" program shown above, no more programs need to be loaded.
  • Select "Resume" to run the program and debug using the various CCS debug options
    \htmlonly <style>div.image img[src="ccs_load_run_07_am26.png"]{width:30%}</style>\endhtmlonly
    \image html ccs_load_run_07_am26.png "Load Program"
    
  • The program output will be seen on CCS console, and/or UART terminal, if enabled. Below shows a sample output on both CCS console and UART console, after running the "hello world" program.

Run the Program

Re-load and run example binaries

  • Here simply repeat the steps shows in Load and run example binaries in CCS
  • It is especially important to "reset the CPU" before reloading the program.
  • In most cases, you dont need to power-cycle the EVM to reload the program or load a new program.
  • In some cases, depending on whether the previous program execution was successful or not, the CPU or some SOC peripheral may be in a exception or hang state. In this case program reload may not work.
    • SOLUTION: Power cycle the EVM and repeat all steps shown on this page.