AM261x MCU+ SDK  26.00.00
USB CDC Echo Example

Introduction

This example is a USB device CDC-ACM (Communication Device Class - Abstract Control Model) application based on USB CDC class from TinyUSB.

The example does the below

  • Initializes the TinyUSB USB core driver and CDC class.
  • Create two virtual COM ports visible to a USB host.
  • Any alphabetic input from the USB host will be echo-ed back in lower case on one COM port and in upper case in the other COM port.

USB Logging Template Example

  • This example also demonstrates how to enable logging for USB using shared memory log feature.
    • The R5FSS0_0_freertos/nortos core will write logs in the shared memory and R5FSS0_1_freertos/nortos core will read and print it on UART0.
  • see USB for more information on how to enable USB logs.
  • see Debug for more information on how to enable shared memory log feature.
Note
  • Enabling logs in debug build may lead to unwanted behaviour as the application code is build with -O0 flag.
  • It is recommended to use release build when USB logging is enabled.

Supported Combinations

Parameter Value
CPU + OS r5fss0-0_nortos
Toolchain ti-arm-clang
iar-arm
Board am261x-lp, am261x-som
Example folder examples/usb/device/cdc_echo

Steps to Run the Example

Build the example

HW Setup

AM261x-LP

  • To test the application, one can use a Windows/Linux PC as a USB host.
  • Connect the J10 on AM261x-LP to the USB host.

USB Micro B Device Connector

AM261X-SOM

  • To test the application, one can use a Windows/Linux PC as a USB host
  • Connect the J7 on AM261x SOM to the USB host

USB Micro B Device Connector

Run the example

For Window 10

  • The two enumerated COM ports can be displayed using the Device Manager on Windows 10,

COM ports (COM3 and COM4) displayed using Device Manager
  • On USB host, use any serial port communication program, like Tera-Term, to connect to those two COM ports

Using Tera Term to connect to port 1

Using Tera Term to connect to port 2
  • Type in any alphabetic characters, the lower case of the input will be displayed on one COM port and the upper case of the input will be displayed on the other COM port

Lower Case Input Echo-ed

Upper Case Input Echo-ed

For Linux

  • The two enumerated serial ports can be enumerated as "/dev/ttyACM0" and "/dev/ttyACM1"
  • On Linux, one has to change the access right for those two serial ports as shown below.
  • Then use any serial port communication program, like putty, to connect to those two serial ports

Using putty to connect to port 1

Using putty to connect to port 2
  • Type in any alphabetic characters, the lower case of the input will be displayed on one COM port and the upper case of the input will be displayed on the other COM port

Lower Case Input Echo-ed

Upper Case Input Echo-ed

See Also

USB