AM243x MCU+ SDK  12.01.00

Introduction

MMCSD Driver API/interface file.

Go to the source code of this file.

Data Structures

struct  MMCSD_Params
 MMCSD instance attributes - used during initialization. More...
 
struct  MMCSD_Attrs
 MMCSD instance attributes - used during init time. More...
 
struct  MMCSD_Object
 MMCSD driver object. More...
 
struct  MMCSD_Config
 MMCSD Global configuration. More...
 

Macros

MACROS used to select the transfer mode

MMCSD_MODE_BLOCKING block task execution while a Transfer is in progress MMCSD_MODE_CALLBACK does not block task execution; but calls a callback function when the MMCSD transfer has completed

#define MMCSD_MODE_BLOCKING   ((uint32_t) 0U)
 
#define MMCSD_MODE_CALLBACK   ((uint32_t) 1U)
 

Typedefs

typedef struct MMCSD_Config_s * MMCSD_Handle
 
typedef void(* MMCSD_txnCallbackFxn) (MMCSD_Handle mmcsdHandle, int32_t transferStatus)
 MMCSD callback function. More...
 

Functions

void MMCSD_init (void)
 This function initializes the MMCSD module. More...
 
void MMCSD_deinit (void)
 This function de-initializes the MMCSD module. More...
 
void MMCSD_Params_init (MMCSD_Params *mmcsdParams)
 Initialize data structure with defaults. More...
 
MMCSD_Handle MMCSD_open (uint32_t index, const MMCSD_Params *openParams)
 This function opens a given MMCSD peripheral. More...
 
void MMCSD_close (MMCSD_Handle handle)
 Function to close a MMCSD peripheral specified by the MMCSD handle. More...
 
MMCSD_Handle MMCSD_getHandle (uint32_t index)
 This function returns the handle of an open MMCSD Instance from the instance index. More...
 
int32_t MMCSD_read (MMCSD_Handle handle, uint8_t *buf, uint32_t startBlk, uint32_t numBlks)
 Function to perform block reads from the MMC/SD media. More...
 
int32_t MMCSD_write (MMCSD_Handle handle, uint8_t *buf, uint32_t startBlk, uint32_t numBlks)
 Function to perform block writes to the MMC/SD media. More...
 
uint32_t MMCSD_getBlockSize (MMCSD_Handle handle)
 This function returns the block size of the MMC/SD media connected to the MMCSD controller. More...
 
uint32_t MMCSD_getBlockCount (MMCSD_Handle handle)
 This function returns the block count of User Data Area of the MMC/SD media connected to the MMCSD controller. More...
 
uint32_t MMCSD_isHC (MMCSD_Handle handle)
 This function returns if the media connected is High Capacity (> 2GB in size) or not. More...
 
int32_t MMCSD_change_Bus_Config (MMCSD_Handle handle, uint32_t busSpeed, uint32_t busWidth)
 This function reconfigures the bus Configuration. More...
 
int32_t MMCSD_change_Tuning_Type (MMCSD_Handle handle, uint32_t tuningType)
 This function reconfigures the bus Configuration. More...
 
int32_t MMCSD_enableBootPartition (MMCSD_Handle handle, uint32_t partitionNum)
 This function enables the boot partition if the connected media is eMMC. More...
 
int32_t MMCSD_disableBootPartition (MMCSD_Handle handle)
 This function disables the boot partition if the connected media is eMMC. More...
 

Variables

MMCSD_Config gMmcsdConfig []
 Externally defined driver configuration array. More...
 
uint32_t gMmcsdConfigNum
 Externally defined driver configuration array size. More...