Go to the source code of this file.
Data Structures | |
struct | exceptionList |
List of MAC ID's which are exempted from Learning, this is for DLR implementation. More... | |
struct | dlrStateMachineVar |
State machine variables, part of DLR Object and L2 implementation. More... | |
struct | superConfig |
Supervisor configuration. Attribute ID 4. More... | |
struct | activeSuperAddr |
Supervisor address, part of DLR Object. Attribute ID 10. More... | |
struct | lastActiveNode |
Last active node at the end of the chain Class for Attributes 6 and 7. More... | |
struct | protocolParticipants |
IP and MAC of the Ring devices. Attribute ID 9. More... | |
struct | dlrStruct |
DLR parent structure through which all other structures can be accessed. More... | |
struct | dlr_Config |
Typedefs | |
typedef struct dlr_Config_s * | EIP_DLRHandle |
Enumerations | |
enum | nodeState { NODE_IDLE = 0, NODE_FAULT = 1, NODE_NORMAL = 2 } |
node state machine states More... | |
enum | ringState { RING_NORMAL = 1, RING_FAULT = 2 } |
ring state values More... | |
enum | nwTopology { LINEAR_TOP = 0, RING_TOP = 1 } |
network topology : possible values for Attribute ID 1 More... | |
enum | nwStatus { NORMAL_STAT = 0, RING_FAULT_STAT = 1, UNEXPECTED_LOOP = 2, PARTIAL_FAULT = 3, RAPID_FAULT = 4 } |
network status : possible values for Attribute ID 2 More... | |
enum | supervisorStatus { BACKUP_NODE = 0, ACTIVE_RING_SUPERVISOR = 1, RING_NODE = 2, NON_DLR = 3, FEATURE_UNSUPPORTED = 4 } |
device role: possible values for Attribute ID 3 More... | |
Functions | |
void | EIP_DLR_init (EIP_DLRHandle dlrHandle) |
API to initialize the DLR driver. More... | |
void | EIP_DLR_deinit (EIP_DLRHandle dlrHandle) |
API to de-initialize the DLR driver. More... | |
void | EIP_DLR_start (EIP_DLRHandle dlrHandle) |
API to start the DLR driver Calling this enables DLR on the device. More... | |
void | EIP_DLR_stop (EIP_DLRHandle dlrHandle) |
API to stop the DLR driver Halt DLR. Calling this disables DLR on the device. More... | |
void | EIP_DLR_port0ISR (uintptr_t arg) |
Fast ISR for Port 0, bypasses the buffer copy and NDK. More... | |
void | EIP_DLR_port1ISR (uintptr_t arg) |
Fast ISR for Port 1, bypasses the buffer copy and NDK. More... | |
void | EIP_DLR_beaconTimeoutISR_P0 (uintptr_t arg) |
ISR for beacon timeout for Port 0. More... | |
void | EIP_DLR_beaconTimeoutISR_P1 (uintptr_t arg) |
ISR for beacon timeout for Port 1. More... | |
void | EIP_DLR_port0ProcessLinkBrk (uint8_t linkStatus, void *arg2) |
Process DLR state machine in the event of a link break on Port0. More... | |
void | EIP_DLR_port1ProcessLinkBrk (uint8_t linkStatus, void *arg2) |
Process DLR state machine in the event of a link break on Port1. More... | |
void | EIP_DLR_neighborTimeoutISR0 (ClockP_Object *obj, void *arg) |
ISR for Neighbor timeout timer for port 0. More... | |
void | EIP_DLR_neighborTimeoutISR1 (ClockP_Object *obj, void *arg) |
ISR for Neighbor timeout timer for port 1. More... | |
void | EIP_DLR_addVlanID (uint8_t *src, uint16_t vlanID) |
void | EIP_DLR_genNCReqFrame (EIP_DLRHandle dlrHandle, uint8_t *src, uint8_t sourcePort) |
void | EIP_DLR_genNCResFrame (uint8_t *src, uint8_t sourcePort, uint8_t reqSrcPort, uint32_t sequenceId) |
void | EIP_DLR_genNeighborLinkStatFrame (EIP_DLRHandle dlrHandle, uint8_t *src, uint8_t sourcePort, uint8_t linkOrNeighbor, uint8_t linkStatus) |
void | EIP_DLR_initDLRFrameHeader (uint8_t *src, uint8_t *header) |
void | EIP_DLR_addSignOnNumNodes (uint8_t *src, uint16_t numNodes) |
void | EIP_DLR_processDLRFrame (EIP_DLRHandle dlrHandle, uint8_t *pktBuffer, uint8_t portNum, uint16_t size) |
Processes a sign on and Neighbor check request frame. More... | |
void | EIP_DLR_dRAMInit (EIP_DLRHandle dlrHandle) |
void | EIP_DLR_resetStateMachine (EIP_DLRHandle dlrHandle) |
Initialize the state machine when it goes back to idle state. More... | |
void | EIP_DLR_setDefaultValue (EIP_DLRHandle dlrHandle) |
void | EIP_DLR_switchToFault (EIP_DLRHandle dlrHandle) |
void | EIP_DLR_switchToNormal (EIP_DLRHandle dlrHandle) |
int32_t | EIP_DLR_isrInit (EIP_DLRHandle dlrHandle) |
void | EIP_DLR_periodicProcessing (ClockP_Object *obj, void *userArg) |
void | EIP_DLR_addToExceptionList (EIP_DLRHandle dlrHandle, uint8_t *macId) |
void | EIP_DLR_clearExceptionList (EIP_DLRHandle dlrHandle) |
uint8_t | EIP_DLR_checkSupervisorException (uint8_t *macId, EIP_DLRHandle dlrHandle) |
void | EIP_DLR_addModuleIPAddress (EIP_DLRHandle dlrHandle, uint32_t newIP) |
void | EIP_DLR_setDivider_WD_IEP (EIP_DLRHandle dlrHandle) |
Sets the clock divider to 1us for IEP watch dog timers. More... | |
void | EIP_DLR_enable_WD_IEP (EIP_DLRHandle dlrHandle, uint8_t id) |
Enable the IEP Watch dog timers. More... | |
void | EIP_DLR_disable_WD_IEP (EIP_DLRHandle dlrHandle, uint8_t id) |
Disable the IEP Watch dog timers. More... | |
void | EIP_DLR_setTimeout_WD_IEP (EIP_DLRHandle dlrHandle, uint16_t periodInMicroSec, uint8_t id) |
Set the timeout value in watchdog. More... | |
void | EIP_DLR_set_pdi_wd_trigger_mode (EIP_DLRHandle dlrHandle, uint32_t mode) |
Set the PDI WD trigger mode. More... | |
#define DEFAULT_DLR_PACKET_SIZE 60 |
For future use when Ring Supervisor is implemented
#define ETHERNET_FRAME_SIZE_60 60 |
#define IEP_WD_PRE_DIV_10US 2000 |
Value written to IEP WD Predivider register to configure 1us increment
#define PORT0_WATCH_DOG_ID 0 /*PD_WD*/ |
ID for PD Watchdog in IEP
#define PORT1_WATCH_DOG_ID 1 /*PDI_WD*/ |
ID for PDI Watchdog in IEP
#define IS_A_LINK_STATUS_FRAME DLR_TRUE |
#define IS_A_NEIGHBOR_STAT_FRAME DLR_FALSE |
#define BOTH_LINKS_UP 0x0 |
#define PORT0_IS_DOWN 0x2 |
#define PORT1_IS_DOWN 0x1 |
#define BOTH_LINKS_DOWN 0x3 |
#define PORT0_WD_ISR_MASK 0x2000000 |
#define PORT1_WD_ISR_MASK 0x4000000 |
#define PDI_WD_TRIGGER_RX_SOF (0 << 4) |
Watchdog RX Start of Frame Trigger
#define PDI_WD_TRIGGER_LATCH_IN (1 << 4) |
Watchdog LATCH IN Trigger
#define PDI_WD_TRIGGER_SYNC0_OUT (2 << 4) |
Watchdog SYNC0 Trigger
#define PDI_WD_TRIGGER_SYNC1_OUT (3 << 4) |
Watchdog SYNC1 Trigger
#define DEFAULT_BEACON_INTERVAL_VARIABLE 400 /*in microseconds*/ |
DLR Timer default values, this is redundant since values are eventually read from supervisor
#define DEFAULT_BEACON_TIMEOUT_VARIABLE (DEFAULT_BEACON_INTERVAL_VARIABLE * 4) /*in microseconds*/ |
#define DEFAULT_NEIGHBOR_TIMEOUT_INTERVAL 100 /*in milliseconds*/ |
#define DEFAULT_DLR_PERIODIC_INTERVAL 100 /*in milliseconds*/ |
#define MAX_NUM_RETRIES 2 |
Number of neighbor retries before a neighbor status message is sent
#define BEACON_CPU_STALL_THRESHOLD 4 |
Number of times beacon timer is triggered before it is disabled
#define DLR_DEFAULT_CAPABILITIES (1 << 7) | (1 << 1) |
the value 1 indicates that this is only a ring node capable device, for other values see below
#define DLR_SIGNON_FRAME_SIZE (ICSS_EMAC_MAXMTU - 10U) |
If size of packet is greater than DLR_SIGNON_FRAME_SIZE in EIP_DLR_processDLRFrame, then the frame is sent directly to host. Value pf "ICSS_EMAC_MAXMTU - 10U" is used because 10 bytes space in the frame is needed so that the own MAC and IP addresses can be added.
#define DLR_COMMON_FRAME_HEADER_SIZE 18 |
#define DLR_COMMON_FRAME_OFFSET 12 |
#define ICSS_DLR_PORT0_INT_FLAG 0x200000 |
DLR port 0 Interrupt Flag for ICSS INTC
#define ICSS_DLR_PORT1_INT_FLAG 0x400000 |
DLR port 1 Interrupt Flag for ICSS INTC
typedef struct dlr_Config_s* EIP_DLRHandle |
enum nodeState |
enum ringState |
enum nwTopology |
enum nwStatus |
enum supervisorStatus |