State machine variables, part of DLR Object and L2 implementation.
Data Fields | |
uint8_t | node_state |
uint8_t | ring_state |
uint8_t | topology |
uint8_t | status |
uint8_t | superStatus |
uint8_t dlrStateMachineVar::node_state |
device state. Internal
uint8_t dlrStateMachineVar::ring_state |
ring state. Internal
uint8_t dlrStateMachineVar::topology |
network topology. Attribute ID 1
uint8_t dlrStateMachineVar::status |
network status. Attribute ID 2
uint8_t dlrStateMachineVar::superStatus |
supervisor status. Attribute ID 3