Set of optional user callbacks used by the Stack.
Typedefs | |
typedef void(* | EC_API_SLV_CBUsrApplicationMainLoop_t) (void *pAppMainLoopCtxt_p) |
User defined function. Called as application MainLoop in MainLoop. More... | |
typedef void(* | EC_API_SLV_CBUsrApplicationRun_t) (void *pAppRunCtxt_p) |
User defined function. Called as "application run" in MainLoop. More... | |
typedef void(* | EC_API_SLV_CBStackError_t) (void *pAppRunCtxt_p, uint32_t errorCode_p, uint8_t fatal_p, uint8_t numOfParam_p, va_list arg_p) |
Called on severe Stack error (OSAL_error) More... | |
typedef EC_API_SLV_EUserRetCodes_t(* | EC_API_SLV_CBStartMbxHandler_t) (void *pContext_p) |
User defined function. Called when mailbox handler is started. More... | |
typedef void(* | EC_API_SLV_CBStopMbxHandler_t) (void *pContext_p) |
User defined function. Called when mailbox handler is stopped. More... | |
typedef EC_API_SLV_EUserRetCodes_t(* | EC_API_SLV_CBStartInputHandler_t) (void *pContext_p, uint16_t *pIntMask_p) |
User defined function. Called when input handler is started. More... | |
typedef void(* | EC_API_SLV_CBStopInputHandler_t) (void *pContext_p) |
User defined function. Called when input handler is stopped. More... | |
typedef EC_API_SLV_EUserRetCodes_t(* | EC_API_SLV_CBStartOutputHandler_t) (void *pContext_p) |
User defined function. Called when output handler is started. More... | |
typedef void(* | EC_API_SLV_CBStopOutputHandler_t) (void *pContext_p) |
User defined function. Called when ouput handler is stopped. More... | |
typedef void *(* | EC_API_SLV_CBPreSeqInputPD_t) (void *pContext_p, uint32_t length_p) |
Register external Input Process Data Buffer. More... | |
typedef void *(* | EC_API_SLV_CBPreSeqOutputPD_t) (void *pContext_p, uint32_t length_p) |
Register external Output Process Data Buffer. More... | |
typedef void(* | EC_API_SLV_CBPostSeqInputPD_t) (void *pContext_p, void *pData_p, uint32_t length_p) |
Register external Release Input Process Data Buffer Function. More... | |
typedef void(* | EC_API_SLV_CBPostSeqOutputPD_t) (void *pContext_p, void *pData_p, uint32_t length_p) |
Register external Release Output Process Data Buffer Function. More... | |
typedef uint8_t(* | EC_API_SLV_CBObjRead_t) (void *pContext_p, uint16_t index_p, uint8_t subindex_p, uint32_t length_p, uint16_t *pData_p, uint8_t completeAccess_p) |
Callback trigered by a SDO Upload operation. More... | |
typedef uint8_t(* | EC_API_SLV_CBObjWrite_t) (void *pContext_p, uint16_t index_p, uint8_t subindex_p, uint32_t length_p, uint16_t *pData_p, uint8_t completeAccess_p) |
Callback trigered by a SDO Download operation. More... | |
typedef bool(* | EC_API_SLV_EoE_CBReceiveHandler_t) (void *pContext_p, uint16_t *pData_p, uint16_t length_p) |
User defined EoE receive function. Called when an EoE frame is received. More... | |
typedef bool(* | EC_API_SLV_EoE_CBSettingIndHandler_t) (void *pContext_p, uint16_t *pMac_p, uint16_t *pIp_p, uint16_t *pSubNet_p, uint16_t *pDefaultGateway_p, uint16_t *pDnsIp_p) |
EoE Settings Indication callback proxy. More... | |
typedef uint32_t(* | EC_API_SLV_FoE_CBOpenFileHandler_t) (void *pContext_p, const char *pName_p, uint16_t nameLen_p, bool isRead_p, uint32_t password_p) |
User defined FoE receive function. Called when an FoE frame is received. More... | |
typedef uint32_t(* | EC_API_SLV_FoE_CBReadFileHandler_t) (void *pContext_p, uint16_t *pData_p, uint16_t foeMaxSendBlockSize_p, uint32_t offset_p) |
Read FoE File callback. More... | |
typedef uint32_t(* | EC_API_SLV_FoE_CBWriteFileHandler_t) (void *pContext_p, uint16_t *pData_p, uint16_t size_p) |
Write FoE File callback. More... | |
typedef uint32_t(* | EC_API_SLV_FoE_CBCloseFileHandler_t) (void *pContext_p, uint32_t errorCode_p) |
Close FoE File callback. More... | |
typedef EC_API_EError_t(* | EC_API_SLV_FoE_CBFwUpdateHandler_t) (void *pContext_p) |
FoE Handle Firmware update callback. More... | |
typedef void(* | EC_API_SLV_CBSystemRebootHandler_t) (void *pContext_p) |
Handle System Reboot. More... | |
typedef void(* | EC_API_SLV_SoE_CBSend_t) (void *pContext_p, uint16_t *pSoEService_p, uint16_t *pSoEFlags_p, void **pData_p, uint16_t *pLen_p) |
Send SoE message to master. More... | |
typedef void(* | EC_API_SLV_SoE_CBRecv_t) (void *pContext_p, uint16_t soEService_p, uint16_t soEFlags_p, void *pData_p, uint16_t *pLen_p) |
Recevice SoE message from Master. More... | |
typedef uint8_t(* | EC_API_SLV_SoE_CBNofReq_t) (void *pContext_p) |
Master requests a notification. Application should send an Emergency message. More... | |
typedef bool(* | EC_API_SLV_CiA402_CBUsrApplSM_t) (void *pAppRunCtxt_p) |
User defined function. Called as "application Cia402 StateMachine" in MainLoop. More... | |
typedef uint16_t(* | EC_API_SLV_CiA402_CBUsrApplSetDict_t) (void *pContext_p) |
Configure CiA402 Object Dictionary. More... | |
typedef void(* | EC_API_SLV_CiA402_CBUsrApplSetDictValues_t) (void *pContext_p) |
Set default values for the CiA402 Objects. More... | |
typedef void(* | EC_API_SLV_CiA402_CBUsrApplApplication_t) (void *pContext_p) |
User application slot (control) More... | |
typedef void(* | EC_API_SLV_CiA402_CBUsrApplLocalError_t) (void *pContext_p, uint16_t errorCode_p) |
User application local error. More... | |
typedef bool(* | EC_API_SLV_CBEepromLoad_t) (void *pContext_p, void *pEeprom_p, uint32_t *pLength_p) |
Load EEPROM from memory. More... | |
typedef void(* | EC_API_SLV_CBEepromWrite_t) (void *pContext_p, void *pEeprom_p, uint32_t length_p) |
Write EEPROM to memory. More... | |
typedef void(* | EC_API_SLV_CBInitFlash_t) (void *pContext_p) |
Init flash memory block to load and store eeprom content. More... | |