typedef uint32_t(* EC_API_SLV_FoE_CBOpenFileHandler_t) (void *pContext_p, const char *pName_p, uint16_t nameLen_p, bool isRead_p, uint32_t password_p) |
User defined FoE receive function. Called when an FoE frame is received.
[in] | pContext_p | call context |
[in] | pName_p | FoE file name |
[in] | nameLen_p | Length of file name |
[in] | isRead_p | true: readAccess, false: writeAccess |
[in] | password_p | password |