typedef EC_API_SLV_EUserRetCodes_t(* EC_API_SLV_CBStartInputHandler_t) (void *pContext_p, uint16_t *pIntMask_p) |
User defined function. Called when input handler is started.
[in] | pContext_p | Function context. |
[in] | pIntMask_p | Value which will be written to the 0x204 register (AL event mask) during the state transition PreOP to SafeOP. |