#include <api/EI_API.h>
EI_API_ADP_T* pEI_API_ADP = NULL;
uint32_t errCode;
uint8_t numInterfaces = 1;
uint16_t vendorId = 1168;
uint16_t deviceType = 0x000c;
uint16_t productCode = 8;
uint32_t serialNumber = 0x00000065;
const char productName[] = "KUNBUS-DTK EtherNet/IP(tm)";
ETHIP_API T * EI_API_ADP_new(uint8_t numInterfaces_p)
Create a new EtherNet/IP adapter.
Definition: EI_API_ADP_main.c:195
ETHIP_API uint32_t EI_API_ADP_init(T *pAdp_p)
Apply parameters.
Definition: EI_API_ADP_main.c:390
ETHIP_API uint32_t EI_API_ADP_setSerialNumber(T *pAdp_p, uint32_t serialNumber_p)
Set the adapter's unique serial number (Instance Attribute ID: 6).
Definition: EI_API_ADP_main.c:1487
ETHIP_API uint32_t EI_API_ADP_setRevision(T *pAdp_p, EI_API_ADP_SRevision_t revison_p)
Set the adapter revision (Instance Attribute ID: 4).
Definition: EI_API_ADP_main.c:1350
ETHIP_API uint32_t EI_API_ADP_setProductCode(T *pAdp_p, uint16_t productCode_p)
Set the adapter product code (Instance Attribute ID: 3).
Definition: EI_API_ADP_main.c:1212
ETHIP_API uint32_t EI_API_ADP_setProductName(T *pAdp_p, const char *pProductName_p)
Set the adapter product name (Instance Attribute ID: 7).
Definition: EI_API_ADP_main.c:1622
ETHIP_API uint32_t EI_API_ADP_setVendorId(T *pAdp_p, uint16_t vendorId_p)
Set the adapter vendor identifier (Instance Attribute ID: 1).
Definition: EI_API_ADP_main.c:946
ETHIP_API uint32_t EI_API_ADP_setDeviceType(T *pAdp_p, uint16_t deviceType_p)
Set the adapter device type (Instance Attribute ID: 2).
Definition: EI_API_ADP_main.c:1080
uint8_t major
Definition: EI_API_ADP.h:127
uint8_t minor
Definition: EI_API_ADP.h:129
Definition: EI_API_ADP.h:126