uint32_t EI_API_ADP_setProductName | ( | T * | pAdp_p, |
const char * | pProductName_p | ||
) |
Set the adapter product name (Instance Attribute ID: 7).
Function to set the product name of the adapter selected by parameter pAdp_p
.
productName
exceeds 32 characters it will be truncated before being written to the internal adapter structures and a warning EI_API_ADP_eERR_LENGTH is returned.[in] | pAdp_p | Pointer to the adapter. |
[in] | pProductName_p | New product name as NULL (\0) terminated cstring. |
EI_API_ADP_eERR_OK | Success. |
EI_API_ADP_eERR_GENERAL | General error. |
EI_API_ADP_eERR_LENGTH | Illegal parameter length, parameter pProductName_p is truncated. |