#include <api/EI_API.h>
EI_API_ADP_T* pEI_API_ADP = NULL;
uint32_t errCode;
uint8_t numInterfaces = 1;
ETHIP_API T * EI_API_ADP_new(uint8_t numInterfaces_p)
Create a new EtherNet/IP adapter.
Definition: EI_API_ADP_main.c:195
ETHIP_API uint32_t EI_API_ADP_setRevision(T *pAdp_p, EI_API_ADP_SRevision_t revison_p)
Set the adapter revision (Instance Attribute ID: 4).
Definition: EI_API_ADP_main.c:1350
uint8_t major
Definition: EI_API_ADP.h:127
uint8_t minor
Definition: EI_API_ADP.h:129
Definition: EI_API_ADP.h:126