![]() |
0.01.00
|
This file defines the OpenThread Operational Dataset API (FTD only). More...
#include <openthread/types.h>Go to the source code of this file.
Functions | |
| OTAPI otError OTCALL | otDatasetSetActive (otInstance *aInstance, const otOperationalDataset *aDataset) |
| This function sets the Active Operational Dataset. More... | |
| OTAPI otError OTCALL | otDatasetSetPending (otInstance *aInstance, const otOperationalDataset *aDataset) |
| This function sets the Pending Operational Dataset. More... | |
| OTAPI otError OTCALL | otDatasetSendMgmtActiveGet (otInstance *aInstance, const uint8_t *aTlvTypes, uint8_t aLength, const otIp6Address *aAddress) |
| This function sends MGMT_ACTIVE_GET. More... | |
| OTAPI otError OTCALL | otDatasetSendMgmtActiveSet (otInstance *aInstance, const otOperationalDataset *aDataset, const uint8_t *aTlvs, uint8_t aLength) |
| This function sends MGMT_ACTIVE_SET. More... | |
| OTAPI otError OTCALL | otDatasetSendMgmtPendingGet (otInstance *aInstance, const uint8_t *aTlvTypes, uint8_t aLength, const otIp6Address *aAddress) |
| This function sends MGMT_PENDING_GET. More... | |
| OTAPI otError OTCALL | otDatasetSendMgmtPendingSet (otInstance *aInstance, const otOperationalDataset *aDataset, const uint8_t *aTlvs, uint8_t aLength) |
| This function sends MGMT_PENDING_SET. More... | |
| OTAPI uint32_t OTCALL | otDatasetGetDelayTimerMinimal (otInstance *aInstance) |
| Get minimal delay timer. More... | |
| OTAPI otError OTCALL | otDatasetSetDelayTimerMinimal (otInstance *aInstance, uint32_t aDelayTimerMinimal) |
| Set minimal delay timer. More... | |
This file defines the OpenThread Operational Dataset API (FTD only).