![]() |
0.01.00
|
This file includes functions for the Thread Commissioner role. More...
Go to the source code of this file.
Typedefs | |
| typedef enum otCommissionerState | otCommissionerState |
| This enumeration defines the Commissioner State. | |
| typedef void(OTCALL * | otCommissionerEnergyReportCallback) (uint32_t aChannelMask, const uint8_t *aEnergyList, uint8_t aEnergyListLength, void *aContext) |
| This function pointer is called when the Commissioner receives an Energy Report. More... | |
| typedef void(OTCALL * | otCommissionerPanIdConflictCallback) (uint16_t aPanId, uint32_t aChannelMask, void *aContext) |
| This function pointer is called when the Commissioner receives a PAN ID Conflict message. More... | |
Enumerations | |
| enum | otCommissionerState { OT_COMMISSIONER_STATE_DISABLED = 0, OT_COMMISSIONER_STATE_PETITION = 1, OT_COMMISSIONER_STATE_ACTIVE = 2 } |
| This enumeration defines the Commissioner State. More... | |
Functions | |
| OTAPI otError OTCALL | otCommissionerStart (otInstance *aInstance) |
| This function enables the Thread Commissioner role. More... | |
| OTAPI otError OTCALL | otCommissionerStop (otInstance *aInstance) |
| This function disables the Thread Commissioner role. More... | |
| OTAPI otError OTCALL | otCommissionerAddJoiner (otInstance *aInstance, const otExtAddress *aEui64, const char *aPSKd, uint32_t aTimeout) |
| This function adds a Joiner entry. More... | |
| OTAPI otError OTCALL | otCommissionerRemoveJoiner (otInstance *aInstance, const otExtAddress *aEui64) |
| This function removes a Joiner entry. More... | |
| OTAPI otError OTCALL | otCommissionerSetProvisioningUrl (otInstance *aInstance, const char *aProvisioningUrl) |
| This function sets the Provisioning URL. More... | |
| OTAPI otError OTCALL | otCommissionerAnnounceBegin (otInstance *aInstance, uint32_t aChannelMask, uint8_t aCount, uint16_t aPeriod, const otIp6Address *aAddress) |
| This function sends an Announce Begin message. More... | |
| OTAPI otError OTCALL | otCommissionerEnergyScan (otInstance *aInstance, uint32_t aChannelMask, uint8_t aCount, uint16_t aPeriod, uint16_t aScanDuration, const otIp6Address *aAddress, otCommissionerEnergyReportCallback aCallback, void *aContext) |
| This function sends an Energy Scan Query message. More... | |
| OTAPI otError OTCALL | otCommissionerPanIdQuery (otInstance *aInstance, uint16_t aPanId, uint32_t aChannelMask, const otIp6Address *aAddress, otCommissionerPanIdConflictCallback aCallback, void *aContext) |
| This function sends a PAN ID Query message. More... | |
| OTAPI otError OTCALL | otCommissionerSendMgmtGet (otInstance *aInstance, const uint8_t *aTlvs, uint8_t aLength) |
| This function sends MGMT_COMMISSIONER_GET. More... | |
| OTAPI otError OTCALL | otCommissionerSendMgmtSet (otInstance *aInstance, const otCommissioningDataset *aDataset, const uint8_t *aTlvs, uint8_t aLength) |
| This function sends MGMT_COMMISSIONER_SET. More... | |
| OTAPI uint16_t OTCALL | otCommissionerGetSessionId (otInstance *aInstance) |
| This function returns the Commissioner Session ID. More... | |
| OTAPI otCommissionerState OTCALL | otCommissionerGetState (otInstance *aInstance) |
| This function returns the Commissioner State. More... | |
| OTAPI otError OTCALL | otCommissionerGeneratePSKc (otInstance *aInstance, const char *aPassPhrase, const char *aNetworkName, const uint8_t *aExtPanId, uint8_t *aPSKc) |
| This method generates PSKc. More... | |
This file includes functions for the Thread Commissioner role.