![]() |
0.01.00
|
This structure represents a Commissioning Dataset. More...
#include <include/openthread/types.h>
Public Attributes | |
| uint16_t | mLocator |
| Border Router RLOC16. | |
| uint16_t | mSessionId |
| Commissioner Session Id. | |
| otSteeringData | mSteeringData |
| Steering Data. | |
| uint16_t | mJoinerUdpPort |
| Joiner UDP Port. | |
| bool | mIsLocatorSet: 1 |
| TRUE if Border Router RLOC16 is set, FALSE otherwise. | |
| bool | mIsSessionIdSet: 1 |
| TRUE if Commissioner Session Id is set, FALSE otherwise. | |
| bool | mIsSteeringDataSet: 1 |
| TRUE if Steering Data is set, FALSE otherwise. | |
| bool | mIsJoinerUdpPortSet: 1 |
| TRUE if Joiner UDP Port is set, FALSE otherwise. | |
This structure represents a Commissioning Dataset.