![]() |
0.01.00
|
This file implements the OpenThread Network Data API. More...
#include "openthread-core-config.h"#include <openthread/netdata.h>#include "openthread-instance.h"Functions | |
| otError | otNetDataGet (otInstance *aInstance, bool aStable, uint8_t *aData, uint8_t *aDataLength) |
| This method provides a full or stable copy of the Leader's Thread Network Data. More... | |
| otError | otNetDataGetNextOnMeshPrefix (otInstance *aInstance, otNetworkDataIterator *aIterator, otBorderRouterConfig *aConfig) |
| This function gets the next On Mesh Prefix in the partition's Network Data. More... | |
| otError | otNetDataGetNextRoute (otInstance *aInstance, otNetworkDataIterator *aIterator, otExternalRouteConfig *aConfig) |
| This function gets the next external route in the partition's Network Data. More... | |
| uint8_t | otNetDataGetVersion (otInstance *aInstance) |
| Get the Network Data Version. More... | |
| uint8_t | otNetDataGetStableVersion (otInstance *aInstance) |
| Get the Stable Network Data Version. More... | |
This file implements the OpenThread Network Data API.