![]() |
0.01.00
|
This file defines the top-level icmp6 functions for the OpenThread library. More...
Go to the source code of this file.
Classes | |
| struct | otIcmp6Header |
| This structure represents an ICMPv6 header. More... | |
| union | otIcmp6Header::OT_TOOL_PACKED_FIELD |
| struct | otIcmp6Handler |
| This structure implements ICMPv6 message handler. More... | |
Macros | |
| #define | OT_ICMP6_HEADER_DATA_SIZE 4 |
| Size of an message specific data of ICMPv6 Header. | |
Typedefs | |
| typedef enum otIcmp6Type | otIcmp6Type |
| ICMPv6 Message Types. More... | |
| typedef enum otIcmp6Code | otIcmp6Code |
| ICMPv6 Message Codes. More... | |
| typedef struct otIcmp6Header | otIcmp6Header |
| This type represents an ICMPv6 header. | |
| typedef void(* | otIcmp6ReceiveCallback) (void *aContext, otMessage *aMessage, const otMessageInfo *aMessageInfo, const otIcmp6Header *aIcmpHeader) |
| This callback allows OpenThread to inform the application of a received ICMPv6 message. More... | |
| typedef struct otIcmp6Handler | otIcmp6Handler |
| This structure implements ICMPv6 message handler. | |
Enumerations | |
| enum | otIcmp6Type { OT_ICMP6_TYPE_DST_UNREACH = 1, OT_ICMP6_TYPE_ECHO_REQUEST = 128, OT_ICMP6_TYPE_ECHO_REPLY = 129 } |
| ICMPv6 Message Types. More... | |
| enum | otIcmp6Code { OT_ICMP6_CODE_DST_UNREACH_NO_ROUTE = 0 } |
| ICMPv6 Message Codes. More... | |
Functions | |
| bool | otIcmp6IsEchoEnabled (otInstance *aInstance) |
| This function indicates whether or not ICMPv6 Echo processing is enabled. More... | |
| void | otIcmp6SetEchoEnabled (otInstance *aInstance, bool aEnabled) |
| This function sets whether or not ICMPv6 Echo processing is enabled. More... | |
| otError | otIcmp6RegisterHandler (otInstance *aInstance, otIcmp6Handler *aHandler) |
| This function registers a handler to provide received ICMPv6 messages. More... | |
| otError | otIcmp6SendEchoRequest (otInstance *aInstance, otMessage *aMessage, const otMessageInfo *aMessageInfo, uint16_t aIdentifier) |
| This function sends an ICMPv6 Echo Request via the Thread interface. More... | |
Variables | |
| OT_TOOL_PACKED_BEGIN struct otIcmp6Header | OT_TOOL_PACKED_END |
This file defines the top-level icmp6 functions for the OpenThread library.